Terasic P0082 DE0-Nano FPGA Development Kit

View table of contents ...  

image

 

{tabbedtable} Tab LabelTab Content
About

The P0082 is a DE0-Nano Development board is a compact-sized FPGA development platform suited for prototyping circuit designs such as robots and "portable" projects. The board is designed to be used in the simplest possible implementation targeting the Cyclone IV device up to 22,320 logic elements (LEs).

 

It allows user to extend designs beyond the DE0-Nano board with two external general-purpose I/O (GPIO) headers. It allows users to handle larger data storage and frame buffering with on-board memory devices including SDRAM and EEPROM. It provides enhanced user peripheral with LEDs and push buttons.

 

Other Features

  • Cyclone IV EP4CE22F17C6N FPGA
  • Configuration & set-up elements: On-Board USB Blaster ckt, serial configuration device EPCS16
  • Memory devices:32MB SDRAM,2Kb I2C EEPROM
  • G-sensor includes ADI ADXL345, 3-axis accelerometer with high resolution (13bits)
  • 8-channel, 12bit Analogue to digital converter
  • On-Board 50MHz clock oscillator
  • Altera complete design suite
  • Features DE0-Nano quick start guide
  • USB Mini-B cable
  • Reconfigurable without requiring superfluous hardware,
  • Suitable for mobile designs where portable power is crucial
  • Provides three power scheme options including a USB Mini-AB port, 2 pin external power header and two DC 5-V pins.

 

image

Important Dates

Enrollment Begins: June 2 2017

Enrollment Ends: July 19 2017

RoadTesters Selected: July 19 2017

Product Shipped: July 20 2017

RoadTesting Begins: July 27 2017

Reminder/Update Email: TBD*

Submit Reviews By: Sept 25 2017**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants were selected as official RoadTesters:

 

Terms & Conditions

Terasic P0082 DE0-Nano FPGA Development Kit – RoadTest

Terms and Conditions

These are the terms and conditions which govern theTerasic P0082 DE0-Nano FPGA Development Kit RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Terasic P0082 DE0-Nano FPGA Development Kit

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on July 19  2017

Announcement of Winner (estimated): July 26 2017

 

Prize:  Terasic P0082 DE0-Nano FPGA Development Kit

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:   
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly. 

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest; 

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7 

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned. 

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comments
Anonymous
  • Same here. Let's put this board to work and demo it. As stated in my application, all functional outputs (HDL code and software support) will be published under an open-source license.

     

    Let's hope more people get involved in FPGA development and testing.

     

    Alvaro

    ZPUino project http://www.alvie.com/zpuino/

  • I will inform you if something prevents me doing the project. As I stated my proposal, this is my first time with AES and I will do my best. In case things go worse, I have a backup project too.

    Thanks,

    Mehmet

  • Congrads on the selection. I hope there will be some information useful to those not selected but wanting to get involved with FPGAs. Possibly some Altera tutorials that we can benefit from or other educational material.

     

    Kas

  • e14 Contributor
    e14 Contributor in reply to rscasny

    Awesome! I cant wait to get started! Relaxed

  • Note About Roadtesting, Summer Vacation and Students

     

     

    Believe it or not, I was once a student. I remember those days when the semester finals were over and I had the summer to kickback and enjoy life.

     

    A few students were selected for this roadtest. Summer vacation is here. I understand the need to relax and be with family and friends.

     

    But if your summer travels will prevent you from completing this roadtest, kindly notify me. thanks.

     

    Randall Scasny

    RoadTest Program Manager

  • Enrollment Begins: June 2 2017

    Enrollment Ends: July 19 2017

    RoadTesters Selected: July 19 2017

    Product Shipped: July 20 2017

    RoadTesting Begins: July 27 2017

    Reminder/Update Email: TBD*

    Submit Reviews By: Sept 25 2017**

     

  • The following applicants were selected as official RoadTesters:

     

  • Here goes nothing, throwing my hat in the ring and we'll see how the chips land.

     

    Kas

  • Yuri, the Road Test is still open for application. If you haven't done this yet, you can click on the Enroll button and submit your proposal.

  • Looks interesting,

    I will give some heads up regarding this board.

  • Jon,

     

    I have now replaced the missing content from the blog post on the PSoC 4 entry.

    It is available here: PIC18F vs PSoC 4:  A tale of two embedded project platforms .

  • Jon,

     

    My solution was developed through a combination of drag and drop of PSoC functional blocks and schematic entry of glue logic. This approach proved to be a best fit with my way of thinking about digital design, which in turn is largely a product of the era in which I learned digital design (late 70's and early 80's).

     

    I wrote an Element 14 blog about the PSoC Creator design development where I compared the PSoC approach with a similar approach using a PIC18F4520 microcontroller.  Unfortunately when I went to look at that blog post just now I discovered that some of the key elements (schematics and some video clips) have disappeared.  I will have to spend a few minutes to re-upload the missing content.  Once I do that you will be able to get a good idea of the level of complexity in the PSoC hardware solution.   It isn't very complex, just some counters, comparators and multiplexers really.  My hope is that it will not be too challenging to port the PSoC design it over to the TerASIC FPGA platform.  I used Altera Quartus II schematic capture when I was playing with a previous TerASIC evaluation board, so I hope to use Quartus II again on this new development kit.

  • Hi Hendrik,

     

    I agree.

    Pure FPGA technology provides a developer to work with intricate circuits to handle a wide range of conditions.

    You mentioned a few, but the device itself can be used for a wide range of applications.

     

    I also agree that the PSOC is a hybrid device.  It provides the user with a limit set of programmable Analog and Digital devices for bridging normal MCU applications with a level of custom circuit implementation capability.

    There are obvious limitations with the PSOC product, but it represents a very useful tool.

     

    The NEO device introduces a lot of flexibility in a single package.

    I am very interested to see if it can be adequately exploited in the maker arena.

    In some ways it has a tremendous potential.

    On the other hand, the skills and tools may be lacking to fully use the device at this level.

     

    I hope that the road testers can better define where and who can or should consider this type of product.

     

    DAB

  • Hi Kas,

     

    FPGA's are very interesting devices.

    They are also not for the feint of heart.

    Working at the gate level can require a very detailed knowledge of data and control flow tied in with a very well crafted timing sequence.

     

    You can do both synchronous and asynchronous projects.

     

    We used these types of devices for handing high speed decoding projects.

    We also used them to replace legacy components that were no longer commercially available.

     

    So on the whole, FPGA technology is a very useful tool to have.

     

    DAB

  • Hi Lucie,

     

    That was my impression, so I would be really interested to see if the marketing claims are true.

     

    It looks like we have a good range of tester applying, so the test reports on this device should provide the community with some great experiences.

     

    DAB

  • Are you a "most novice user," Kas? My impression from your posts is that you already know a fair bit about circuit design and I suspect you can already do logic design much better than many of the people who are going to be applying for this roadtest. Building a very simple peripheral in the FPGA would be quite realisable in the time you have for doing the roadtest. Maybe take SPI from an Arduino (or whatever prototyping board you happen to have handy and like using) to the FPGA and have the FPGA decode the data and display it on a couple of 7-segment LED displays, or something like that.

  • Out of curiousity, how did you do your design for the PSoC (I'm not familiar with the PSoC parts or the Cypress design tools)? Did you synthesise it from a schematic, use a HDL [hardware discription language] like VHDL or Verilog, or was it something else (like, maybe, dragging and dropping circuit blocks)? Just wondering what you're going to have to do to get it into the FPGA.

  • I did, maybe, step over the 'a roadtest isn't a design challenge' line there a little, so you're probably right. But there are going to be a lot of people pitching for the 'board as an educational tool' approach, so this is a way to differentiate yourself from that and help TerASIC who will want a balance of the different kinds of roadtest that you might do with it. What you've already proposed is probably enough and I'm just getting enthusiastic and egging the cake a bit.

  • FPGAs shine when you are talking about a) (massive) parallel computation b) anything where reliable (and fast) timing is critical. Think of oscilloscopes, digital video cameras, high-speed bus systems. a MCU only has limited computational bandwidth, and it cannot guarantee stable timing (apart from interrupts, but using them reduces the available computation bandwidth). FPGAs can handle many things in parallel, and sometimes you need just that.

    As already mentioned, PSoC falls somewhere in the middle. They don't have as much resources as a FPGA (they are more like a CPLD), but with their programmable hardware they can handle timing-critical functions directly in hardware. This leaves the MCU core free to either go to sleep (and save power) or to take care of the more complex and not-timing-critical stuff.

  • Jon,

     

    I like your suggestions.

    May as well throttle up the project to take advantage of the FPGA platform.

     

    Just not sure I could get it all done in a two month window of working evenings and weekends.

     

    Perhaps a reasonable scope of work can be devised that highlights FPGA advantages without consuming every waking hour.  The ease of using the platform tools will determine how much can get done.

     

    You have inspired me to think more on how to structure a good (likely to be selected) road test application.

     

    Thanks!

     

    Mark A