RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Documents What Would Be Your Favorite Project Build with the Cypress PSoC 6 Pioneer Kit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 1 Aug 2017 9:24 PM Date Created
  • Last Updated Last Updated: 3 Aug 2017 4:00 PM
  • Views 6558 views
  • Likes 5 likes
  • Comments 38 comments
Related
Recommended

What Would Be Your Favorite Project Build with the Cypress PSoC 6 Pioneer Kit?

Hi RoadTesters!

 

I recently met with Cypress concerning their new PSoc 6 MCU product line. The company believes the PSoc 6 is a real winner for engineers developing IoT products. In conjunction with the PSoc 6, they've produced a BLE Pioneer Dev Kit, based on its new PSoC 6 dual-core MCU architecture,

 

Here's an Unboxing Video of the dev kit:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here's a quick overview of the PSoc 6 MCU architecture:

What's unique about the PSoc 6 is that it bridges the gap between application processors and standard microcontrollers. It features:

  •     Dual-core ARMRegistered CortexRegistered-M4 and ARM CortexRegistered-M0+, running at 150-MHz and 100-MHz, ultra-low-power 40nm architecture
  •     Ultra-low-power design that consumes as little as 22-μA/MHz in active power mode1 and 4.5-μA in deep sleep modes
  •     Flexibility with wired and wireless connectivity options, software defined peripherals, and CapSenseRegistered
  •     Integrated, hardware-based Trusted Execution Environment (TEE) with secure data storage

 

Power

The PSoC 6 MCU architecture reduces energy consumption with:

  •     Dynamic voltage and frequency scaling enabling both performance- and power-critical processing
  •     Auxiliary core which can be used as an offload engine for power efficiency, allowing the main core to sleep
  •     Ultra-low-power system: 22-µA/MHz active (CortexRegistered-M4) and 15-µA/MHz active (CortexRegistered-M0+)

 

Dual-Core Architecture

The PSoC 6 has a flexible dual-core architecture to optimize system power consumption and performance. This architecture has two processors CM0+ and CM4 on the same die, with all the memory and peripherals available for use by both the cores. This adds a lot of value to the user who wants to set up a system where the processing load is shared by the two cores.

image

Security

The PSoC 6 provides secure, internal storage for firmware, applications and secure assets, including:

  •     Scalable secure memory for multiple, independent user-defined security policies,
  •     Cryptographic algorithms including elliptical-curve cryptography (ECC) and advanced encryption standard (AES) with integrated hardware coprocessors
  •     A specialized hardware block designed to offload compute-intensive tasks from the main processor

 

Are you Looking for a Device That's Built for the Internet of Things? Then Check out the PSoc 6!

Cypress believes that the PSoC 6 will serve as the catalyst for differentiated IoT devices because:

  •     Software-defined peripherals can be used to create custom analog front-ends (AFEs) or digital interfaces for innovative system components such as electronic-ink displays.
  •     Flexible wireless connectivity options, including fully integrated Bluetooth Low Energy (BLE) 5.0.
  •     CapSenseRegistered capacitive-sensing technology, enabling modern touch and gesture-based interfaces
  •     Support by Cypress's PSoC CreatorTm Integrated Design Environment (IDE) and the expansive ARM ecosystem.

 

Click here for some application examples.

 

If you are new to Cypress PSoC MCUs, click here for a glossary of key PSoC terms.

 

Before I offer a RoadTest on this product, I'm curious to learn what would be your favorite project builds with this kit? And why the PSoc 6 is a great fit for your idea. Thanks.

 

Please leave any comments below.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • scasny
  • iot_design
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +7
    Hi Randall, I am a big fan of the PSOC and this latest product would be very useful in helping me upgrade my controller for an old CNC kit I have. I am looking to do a computer controlled scanning microscope…
  • rscasny
    rscasny over 9 years ago +7
    Overall lots of great ideas: upgrade controller for CNC kit a high end 3D printer a vehicle nanny that monitors, analyzes, diagnoses and reminds you of vehicle performance, health and maintenance schedules…
  • BigG
    BigG over 9 years ago in reply to dougw +6
    I agree that to fully test capability will involve some complexity. For me it's important to test the unique features of dual core. How exactly does this work and what can you get out of this package that…
  • Workshopshed
    Workshopshed over 9 years ago in reply to ipv1

    I love the capsense technology it works really well. CapSense MBR3 Evaluation Kit - Review

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 9 years ago

    The PSOC platform allows for quick development and with BLE 5, it can be used with a larger range. Given it's e Ink display package and onboard cap sense dashboard, it would make a great little IoT Dashboard Widget. That can run on a battery. That would serve as template for a number of applications such as:

    * Agile Sprint Display

    * Personal Productivity manager

    * Email and Weather Display

    * Industrial Process Summary

     

    On the other hand the I2S interface hints at the creation of voice enabled devices.

    * IoT Voice Capture and Communications system

    * Media Player and Internet Radio(There is a USB interface as well)

    * Google AIY?

     

    Lots of possibilities.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 9 years ago in reply to DAB

    Great ideas. A CNC machine and the knowledge to use one can be very helpful. To build your own is even better.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 9 years ago in reply to dougw

    I like your suggestions. Especially the sonar.

     

    A DIY precious metal detector project would be very interesting. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago

    I really like this kit - it has great capability and the infrastructure to implement complex designs quickly.

    However, making good use of the extensive capabilities of this kit implies a pretty complex application that will require a large effort.

    I would use it for applications like:

    • a high end 3D printer
    • a vehicle nanny that monitors, analyzes, diagnoses and reminds you of vehicle performance, health and maintenance schedules
    • an autonomous robot to mow lawns, clean beaches, plow driveways, clean pools, vacuum clean a house or groom a baseball pitch.
    • a controller for a self-balancing 2-wheeler personal transporter
    • a front end controller for a sonar system that can map a river bed or a lake bed or use a second one to autonomously control a boat to automatically map a lake bed (at night)

    (I have a long "bucket list" of project ideas lurking in my head, slowly gathering justification momentum)  image

    But for projects like this set, I would strongly consider using this PSoC6 kit because it would shorten development time.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to rscasny

    Cheers

    It seems the kit is listed for Preorder on the Aus/NZ site, but t doesn't mention the dongle.

    CY8CKIT-062-BLE - CYPRESS SEMICONDUCTOR - PSOC 6 PIONEER KIT | element14 New Zealand

     

    I'll find out when it arrives.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 9 years ago

    I created this doc to provide more info on the PSoC 6.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Hi Randall,

     

    I am a big fan of the PSOC and this latest product would be very useful in helping me upgrade my controller for an old CNC kit I have.

     

    I am looking to do a computer controlled scanning microscope to look at very small features of various materials and plants.

     

    The BLE capability would enable me to connect remotely.

    The display would enable me to follow position values locally.

    The programmable digital components would enable me to interface with the motors.

     

    I am also planning to connect an old joystick game controller to the device for manual positioning control.

     

    So if they are looking for a really different type of project, I think I have one.

     

    DAB

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
<