RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Polls Poll: Are You Interested in Roadtesting a PoE-to-USB-C Power and Data Adapter?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 1 Apr 2021 10:00 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 2799 views
  • Likes 2 likes
  • Comments 14 comments
Related
Recommended

Poll: Are You Interested in Roadtesting a PoE-to-USB-C Power and Data Adapter?

I wanted to get your opinion about roadtesting a PoE-to-USB-C Power and Data Adapter

 

Made by Microchip, the PoE to USB-CRegistered Power and Data Adapter connects Internet of Things (IoT) devices with a USB-C connector to Power over Ethernet (PoE) networks, enabling you to leverage the advantages of PoE and USB-C technologies. It provides both power and data to USB-C hosts.

POE to USCB-C Power and Data Adapter

Here are some more facts about this product:

 

The PD-USB-DP60 adapter enables flexible installation of USB-C devices, removes the need for a close power outlet and resolves the issue of limited USB cable length. The PoE source can be up to 328 ft/100m from the location of the USB-C device. A single Ethernet cable is needed while delivering up to 60W of USB power at the output of the adapter.

 

The PD-USB-DP60 connects with small PCs/Next Unit of Computing (NUC), interactive information kiosks, smart monitors, tablets, laptops, cellphones, cameras and other USB-C powered devices consuming up to 60W. The adapter is compatible with USB2.0 and 3.1 and will automatically provide to the end device the exact amount of power it needs.

 

  • Up to 60W output power
  • Enables powering of small PCs/Next Unit of Computing (NUC), interactive information kiosks, smart monitors, tablets, laptops, cameras and other USB-C devices
  • Provides power and data to USB-C Hosts
  • Allows 328 ft/100m installation range
  • Supports PoE Switches and Injectors from 15.4W and up to 90W
  • Plug and play USB-C Power, no configuration is needed, simple to use

 

Here's the datasheet:

https://ww1.microchip.com/downloads/en/DeviceDoc/PoE_to_USB-C_Adapter_Datasheet_00003813C.pdf

 

Here's the quick start guide:

https://ww1.microchip.com/downloads/en/DeviceDoc/00003800.pdf

 

Here's a short video:

https://www.microchip.com/wwwproducts/en/PD-USB

  • microchip
  • roadtest survey
  • poe to usb-c power and data adapter
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 5 years ago in reply to DAB +6
    "...I did not think that much power was available from a standard ethernet port..." The wonderful thing about standards is that there are so many of them to choose from... The PoE++ standard can output…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to obones +5
    Once the drivers are installed, it becomes a "common" ethernet adapter.
  • shabaz
    shabaz over 5 years ago +4
    For anyone who is interested in getting PoE for home, a very low-cost way is to pick up from ebay a 'SD208P' switch, they are only 100Mbit/sec, but are cheap, about $20-£30 (only worth getting if it comes…
  • DAB
    DAB over 5 years ago

    I was surprised to see it offer 60W of power at the end of an ethernet cable.

    I did not think that much power was available from a standard ethernet port.

     

    I am not sure that all ethernet ports could support such a power push.

     

    Using one of these to power a modest device would be an interesting device to test.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • obones
    obones over 5 years ago in reply to Jan Cumps

    Ah thanks, it's behaving like the docking station for a laptop then, except that the power comes from the POE part, not an AC adapter plugged to mains.

    I now see the use case with NUCs and information kiosks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to obones

    Once the drivers are installed, it becomes a "common" ethernet adapter.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • obones
    obones over 5 years ago

    The description above and the datasheet both say this:

    Converts both power and data to a single USB-C output

     

    But I have a hard time understanding how the "data" part would work with a single RJ45 plug on the input side of things. Where is the data coming from?

    I mean, look at the schematic from the datasheet:

     

    image

     

    There is nothing on there that is providing USB datagrams to the tablet. Well, sure, the adapter appears to be "USB PD" compatible and will provide those datagrams for power delivery, but if I wanted to "talk" to that tablet from afar, I don't see how this could be happening with some sort of software installed on a host in the RJ45 side of things.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<