Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Analogue Design Nice new AD Parts
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 525 subscribers
  • Views 2660 views
  • Users 0 members are here
  • analog_electronics
Related

Nice new AD Parts

michaelkellett
michaelkellett over 2 years ago

I was going to post this in the Analogue Forum - but there isn't one, or maybe Audio (nope), or even "Instrumentation "  - no.

So it has to be a blog here.

Just had a note from ADI about a few rather neat parts:

ADA4510-2 Op Amp with DigiTrimTm

Analog Devices' ADA4510-2 precision, 40 V, ±70 nV/°C, rail-to-rail input and output op amp features DigiTrim

A very nice low noise, low offset dual op amp remarkably similar to the TO OPA2192.

Currently only available in 8 pin SOIC.

ADL5960 Analyzer Front End

Analog Devices' ADL5960 10 MHz to 20 GHz integrated vector network analyzer front end supports various LO interface configurations

It looks interesting but of course it isn't a complete VNA - I don't know enough about the design of such things to tell if its would make a good VNA or just a cheapish one.

The chip is £133 and the eval board is about £800.

ADG6412/ADG2412 Switches

Analog Devices' ADG6412 and ADG2412 0.5 Ω RON quad SPST switches provide high continuous current carrying capability

These are nice (if pricey at £6.94 each) quad SPST solid state switches capable of switching serious current and a wide voltage range.

and finally the:

MAX17614 Ideal Diodes/Power Source Selector Device

Analog Devices' MAX17614 4.5 V to 60 V, 3 A, ideal diode and power source selector has current limit, UV, and OV protection

These look quit nice - I rather wish I had fitted them to my laser controller - it has four buck regulators capable of about 20W each but no easy way to current limit them. If I'd known about these parts I could have used them both for isolation and protection.

MK

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 2 years ago in reply to cstanton +1
    Thanks Chris, Extending Embedded and Microcontrollers by the addition of Analogue Design would work fine for me. It has sub fora of Embedded, DSP and PIC Microcontrollers so adding an Analogue Design…
  • cstanton
    0 cstanton over 2 years ago in reply to michaelkellett

    Done!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 2 years ago

    Interesting list of products.

    Analog Devices has always had a lot of very useful products.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<