Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum DC power jack design decision: 2.1mm ID or 2.5mm ID?????
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 340 subscribers
  • Views 37875 views
  • Users 0 members are here
  • jack
  • pcb
  • barrel
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

DC power jack design decision: 2.1mm ID or 2.5mm ID?????

e14 Contributor
e14 Contributor over 16 years ago

Hello there!

We are designing a family of consumer devices that will require an input DC power barrel connector on our PCB.  It will be for +12vdc of various power levels.  We will be able to purchase "off the shelf" UL-listed wall warts depending on the application.  My question is, as I design our PCB to work with a PCB mount DC barrel jack, which is more common?  2.1mm ID or 2.5mm ID for DC power jacks with 5.5mm OD???  So far it looks like they both are "standards".  So, which do I design for if I want to be most forward compatible?  Does one of the options work with both plug types, but not vice-versa?

 

Switchcraft 2.1mm ID, 5.5mm OD $1.61 @ qty=1k

http://search.digikey.com/scripts/DkSearch/dksus.dll?Detail&name=SC1330-ND

 

CUI 2.1mm ID, 5.5mm OD $0.19 @ qty=1k

http://search.digikey.com/scripts/DkSearch/dksus.dll?Detail&name=CP-102A-ND

 

CUI 2.5mm ID, 5.5mm OD $0.19 @ qty=1k

http://search.digikey.com/scripts/DkSearch/dksus.dll?Detail&name=CP-202B-ND

 

Thank you for any suggestions!!.... changing after we make several thousand will be much more difficult!

Respectfully,
Steve  French
814.584.1220.office
814.730.0003.cell
 
President, Volt  Vision
www.voltvision.com
  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 5 years ago in reply to Gough Lui +1
    Yep, more choice in PCB mount but not that many. I wanted a 3-pin, panel mount one that would give me more flexibility in positioning a PCB inside a case and given I already have a 2.1mm 15V wall wart…
  • Gough Lui
    Gough Lui over 5 years ago in reply to Andrew J +1
    I'm sure it will be fine, as long as you're not connecting/disconnecting under load too frequently - the arcs could damage the contacts and increase the contact resistance before the connector reaches…
  • Gough Lui
    0 Gough Lui over 5 years ago in reply to Andrew J

    That's an interesting observation @andrewj - I wouldn't have thought the size different to be significant to voltage but the thicker pin should enable higher currents.

     

    Speaking of which, a 2.1mm jack capable of more than 12V isn't entirely unknown of -

    • https://au.mouser.com/ProductDetail/Kobiconn/163-179PH-EX/?qs=Xb8IjHhkxj5l2UOaIqcGCw%3D%3D - a 18V/1.5A rated PCB-mount 2.1mm/5.5mm socket
    • https://au.mouser.com/ProductDetail/CUI-Devices/PR-2155/?qs=%252BEew9%252B0nqrDXc8k%2FA8GUUQ%3D%3D - a 20V/7A rated cable-mounted 2.1mm/5.5mm socket

     

    But you're right - there's not many choices out there.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 5 years ago in reply to Gough Lui

    Yep, more choice in PCB mount but not that many.  I wanted a 3-pin, panel mount one that would give me more flexibility in positioning a PCB inside a case and given I already have a 2.1mm 15V wall wart which I've designed around, I've decided to risk a 12V 5A panel connector rather than paying through the nose for a 15V 2.5mm jack and a replacement wall wart or, more likely, a 2.1mm to 2.5mm adapter.  If it does breakdown in the future at least I only have easy-to-change parts to deal with!  Assuming the house doesn't burn down of course image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 5 years ago in reply to Andrew J

    I'm sure it will be fine, as long as you're not connecting/disconnecting under load too frequently - the arcs could damage the contacts and increase the contact resistance before the connector reaches its "rated" contact cycles. Perhaps the rating is conservative for that reason. I'd be much more suspect using a plug adapter ... as sometimes you don't know what parts are used to make them!

     

    It should be remembered that connectors as small and fine-pitched as USB-C are rated to carry 20V at up to 5A ... and the barrel jack is likely to have quite a bit more metal and plastic.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<