Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Banksy’s “Girl with Red Balloon” Painting Gets Shredded at Auction, but Was it all Just a Stunt?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 9 Oct 2018 7:36 PM Date Created
  • Views 3332 views
  • Likes 8 likes
  • Comments 21 comments
  • prank
  • robotics
  • robot
  • cabeatwell
  • auction
  • art
  • banksy
Related
Recommended

Banksy’s “Girl with Red Balloon” Painting Gets Shredded at Auction, but Was it all Just a Stunt?

Catwell
Catwell
9 Oct 2018

image

The $1.4-million painting was seemingly cut to ribbons using a homemade shredder built into the frame. (Image credit: Sotheby’s)

 

Love him or hate him, Banksy’s art has fetched a high price over the last decade, with artworks such as “Space Girl and Bird” netting $479, 926, “Monkey Detonator” earning $587, 544, and “Keep it Spotless” netting an incredible $1.7-million. The latest auction from Sotheby’s for his “Girl with Red Balloon” brought in $1.4-million, the second highest price paid for one of his works, but that’s not what makes it astounding, as the masterpiece was shredded as soon as the auction gavel hit its base.

 

Hidden inside the frame was a homemade shredder that chewed through the canvas after sounding an alarm. Banksy claimed that if this piece ever went to auction, it would be destroyed, and destroyed it was, but was it all an elaborate trick by the 21st-century artist? The video below provides little insight on how Banksy was able to pull it off, but after looking at whatever tech he used, it seems more suspect that someone in the crowd at the auction was part of the ruse.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The video shows a row of X-ACTO blades positioned close to the base of the frame, along with a brief view of the electronics that make up the internal shredder, which looks like a pair of motors to pull the canvas through the blades and maybe some white battery enclosures at the top. It’s hard to tell what exactly is used when he designed the shredder.

 

Here’s where the speculation comes in- Banksy built that frame for the painting back in 2006, and it has apparently remained closed since that time. Shredders, even the homemade versions, require a steady amount of power to work, so it’s hard to imagine any commercial battery retaining enough power to engage the motors after 12-years. Couple that with a receiver circuit in standby mode waiting to engage the shredder, and the prospect of working drops even lower.

 

Some have suggested that a switch hidden somewhere on the frame was engaged by an accomplice at the show, as there was a report a person was escorted out of the auction after the winning bid was announced. There are too many anomalies floating around the auction, as well as unanswered questions- Why didn’t anybody notice the weight of the frame, or open up the back to see the condition of the canvas or to confirm it was an actual Banksy? After the painting self-shredded, it was immediately taken away. Did those workers know it was safe to move it, what if there were more traps that were yet to be sprung?

 

We may never know what the truth is unless the private owner who purchased the artwork reveals what exactly is inside that frame.

 

I am considering making a shedding picture frame as a project. The utility comes in when you're tired of whatever is in it - shred it. image

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

 

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +4
    Nice puzzle. It's a shame not everything is shown : ) but that keeps the value of the "art" high : ) This is my theory: (orange=motor+belt, blue=rubber rollers, brown=wood sheet fitted during the video…
  • balearicdynamics
    balearicdynamics over 7 years ago +4
    99% it's a stunt but Cabe, I am considering making a shedding picture frame as a project. The utility comes in when you're tired of whatever is in it - shred it. You have suggested me a great project,…
  • mp2100
    mp2100 over 7 years ago +4
    A great stunt. It will make the shredded painting worth even more. It’s not a cross-cut shredder. Straight line cut. I wish I’d been the bidder with $1.4mm. Cha-ching! Sell the shreddedpainting for $14…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to balearicdynamics

    balearicdynamics  wrote:

     

    ...

    About the girl with the red balloon instead, accomplishing the irony of Banksy, I embedded a video image

     

    Enrico

     

     

    I have the single image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to mcb1

    Yes, the knives are wrong in the video. They can't cut the canvas like that. There's a dedicated thread on eevblog on this, where several people suggested that:

    There are two paintings in the frame, and two rolls, and no shredder.

    One roll rolls up the intact canvas.

    The second roll, in (bad) sync unrolls a pre-cut version of the same painting.

     

    The moon landing never happened. Chem trails from jet airliners, etc ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 7 years ago

    I'm calling this a hoax.

    The video seems to be of the rear of the frame, and this makes it even weirder.

     

    The pictures showing the blades is wrong, as they are at 90 degrees to the cut marks , and the fastening down doesn't seem enough to hold them.

    The blades are not centered, and there are more than the number of cuts.

     

    The image either side of the frame is about right distance but the shredded portion is exiting the frame closer to the wall, and this extra distance means the picture has stretched somewhat.

    I suspect the original is safely inside, and the shredded copy was pre-loaded behind it and ejected out the bottom.

     

    It seems strange that a picture of that magnitude was being auctioned with the picture behind the audience, most auctions I've seen have the auctioneer in front of the piece watching the audience to gauge a reaction or entice the bidding.

    So why it was not in front of them I'm puzzled.

     

    It has now increased in value, so who knows if it was planned or not.

    Personally I do find it strange that no-one bothered checking the painting for authenticity which would have shown the inside of the frame was rigged.

     

    Mark

     

     

     

     

     

    https://www.nzherald.co.nz/entertainment/news/article.cfm?c_id=1501119&objectid=11139925

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago in reply to shabaz

    You may find the start of this documentary interesting:

     

    What makes us human ? Copycats

    https://www.youtube.com/watch?v=JHoS4W0leuQ&list=PL4CF86B15C5479B68

     

    Especially the bit where the art critic initially values the painting at half a million dollars...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to neilk

    I wish I knew : ) A wise friend once told me the only culture I had was agriculture : )

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>