Products
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
Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Try out OpenPLC on a Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 9 Aug 2019 1:01 PM Date Created
  • Views 11279 views
  • Likes 10 likes
  • Comments 8 comments
  • openplc
  • raspberry pi
  • ladder logic
Related
Recommended

Try out OpenPLC on a Raspberry Pi

Jan Cumps
Jan Cumps
9 Aug 2019

I'm checking if I can use OpenPLC on small Linux devices.

The software is known to work on a Raspberry Pi. I'll try it out on that first.

I can focus on the functionality instead of installation and dependency resolution.

It 'll also give me a chance to measure how much compute resources the application needs.

image

 

Open PLC is a combination of 3 modules:

  • a runtime, executes PLC programs you made in  ...
  • ... the editor, where you can write programs in ladder logic and other PLC languages.
  • a monitoring application (SCADA) for shop floor data collection and dashboarding

 

Install Runtime and Editor

 

I installed the runtime on my Rasperri Pi, using these instructions. I had to use sudo to install the software. Maybe because I installed it in /usr/local.

Once installed, you get a web application where you can configure the Open PLC runtime, install and monitor programs.

image

 

I started the runtime in the console, changed the settings to switch autostart and persistence storage on.

In the Hardware menu, I selected Raspberry Pi and saved the setting.

After rebooting the Pi, the OpenPLC application was up and running and I could connect via http://raspberrypi:8080

 

I installed the editor on my windows laptop, using the download available here.

Unzipping it and clicking the shortcut brought up the program.

 

Hello, world!

I started with the example application, available from the Getting Started with Raspberry Pi page.

The example waits for a key to be pressed, then enables an output for 2 seconds (oddly enough 4 - 11 seconds when I tried it).

Because the input used in this example (pin 3, named %IX0.0 in OpenPLC) is pulled high on the Pi, I added an invert block (NOT) between switch and Off Timer (TOF).

image

I then generated a .st file that can be uploaded via the OpenPLC console.

 

I connected a push button between %IX0.0 and ground, a LED and resistor (I used 660 Ohm, good enough for modern day LEDs) between %QX0.0 and ground.

image

I then used the console to upload the program to the OpenPLC runtime, then pushed the start button.

 

 

image

When the button is pushed, the led will light for a given time. Although the example sets that time to 2000 ms, mine lit up for 4-11 seconds.

The odd thing is that the monitor shows that the output pin goes low after 2 seconds, but the led stays on 6 more seconds...

 

There's a monitoring page where you can see the state of inputs and outputs.

This OpenPLC monitor is simple and just displays the pins. In theory you should be able to click on them to get more details (and manipulate them). This doesn't work on my installation. I get a 404.

 

Below you can see the monitor during the 3 possible states:

 

  • in rest: button not pressed (inverted by the NOT operation I put in between), LED off

image

  • during button press: button pressed (inverted by the NOT operation I put in between), LED on

image

  • in rest: button released (inverted by the NOT operation I put in between), LED on for a few seconds

image

  • Sign in to reply

Top Comments

  • jomoenginer
    jomoenginer over 7 years ago +4
    Very cool Jan. I had seen OpenPLC awhile back and was looking to give it go but have not been able to fit into to my schedule. There is Arduino support with OpenPLC which I thought would be interesting…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to jomoenginer +3
    The Arduino can be used as a slave device (an I/O expander). I haven't seen it listed as an embedded platform that can run OpenPLC itself. You'd still need a Pi, one of the other embedded platforms or…
  • jomoenginer
    jomoenginer over 7 years ago in reply to Jan Cumps +3
    Understood. It would still be interesting to test it out.
  • bernhardtjosef
    bernhardtjosef over 6 years ago

    Modbus TCP WIFI Modul for 24V E/A !
    Here is an example circuit for Modbus TCP with the ESP8266 module. The circuit offers 4pcs. 24V inputs, 4pcs. 24V outputs with the BSP76 Infineon HITFET as well as an analog input / output with 0.10V. The module can be used as a Modbus module but also for controls based on Arduino. You can use it for openplcproject too.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bernhardtjosef
    bernhardtjosef over 6 years ago

    Here an Example with Raspberry PI 4

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bernhardtjosef
    bernhardtjosef over 6 years ago

    I have been working with openplcproject for some time and find it very successful. So that I can test the example well, I have developed a simple I / O board with LED and buttons.
    If you are interested in examples or the test board, please feel free to contact me by email.
    Address:
    josef@bernhardt.de
    or

    image

    openplcproject.de

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 7 years ago

    PLC on a Raspberry Pi. That is a novel Idea.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to Jan Cumps

    Understood.  It would still be interesting to test it out.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>