• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56291 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
  • fmilburn
    fmilburn over 6 years ago in reply to phoenixcomm

    I started putting in shelving today :-)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to fmilburn

    fmilburn Good luck, frank I'm still putting up shelving! Lots of Elfa top mounting rails, and standards. Rubbermaid etc (Home Depot) for the brackets (cheaper price). And sometimes I buy them from my Goodwill outlet store where it's only $1.50 a pound. image I also have some Metro wire shelves, and some HomeDeopt plastic shelves. In my garage, I put together a bunch blue of 2x4x6 used shelves with nuts and bolts ( image pain in the ass!) so have about 20 feet of that stuff. And I still need to put together a workbench down there as well. for a drill press and other things. Currently building a 12' long clothes rack, from 2x4s and two uprights from the blue shelves. Not quite a 3-foot base but all the way to the ceiling made like two right triangles. And its bolted together, with a cross brace near the top to rest the steel on. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to phoenixcomm

    phoenixcomm Yep, I'm started with some metal wire shelving that is quick to put up in the garage and then building some 2x4 made to fit next.  I almost spent more time opening boxes to find the necessary tools than putting up shelves.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to fmilburn

    fmilburn " I almost spent more time opening boxes to find the necessary tools than putting up shelves." sounds very familiar!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago

    I fear this project has died. It will be a shame if it has after all the hard work that has been put in. I know I haven’t contributed very much personally, mainly because I find it all a bit beyond my analog capabilities.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davemartin
    davemartin over 6 years ago in reply to kltm

    Hi Ken,

     

    I certainly hope it hasn't died - both because of the need and potential, and because of the work Michael Kellett and others have already put in.

    I am afraid that my daytime work has been interfering with projects like this; but I have been working on a data set to provide some information to help with background for the design. To illustrate the injection aspect C1C2 and range of readings P1P2  I have, along a fixed 50 metre traverse, taken readings at 1,2,3,4,5, 10, 15, 20 ..50m using conventional square-wave excitation, capturing injection voltage V1 and current I C1C2, and the independent differential signal voltage V2 between P1P2 using 4-channel scope and then deriving injection resistance R1 and P1P2 resistance R2 with waveforms at each point both single-sweep to capture peaks and using modest filtering. I've then also got some control plots (e.g. no injection with, and without, mains on nearby) to capture background noise P1P2, and plots with the leads but using an appropriate dummy load. I've then run a series of tests using various excitation waveforms - conventional square wave, sine wave, triangle / symmetrical sawtooth, and an arbitrary trapezoid. Much of that is done and partly written up; problem has been the day-job and also getting time when it hasn't been driving rain outside! I hope to get time and opportunity to complete that within the next few days. Its looking so long that I may need to publish it in a couple of parts, or as blog posts (as Michael did for the input amp.), or as PDFs.

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago in reply to kltm

    Ken,

     

    There is still work going on for this project.  The discussions have been moved to another area and split into separate topics.  If you use the search bar at the top of the screen and enter ARMP (for Archaeology Resistivity Meter Project) you will see multiple discussions that are focused on various parts/functions of the project.

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kltm

    Hello Ken,

     

    I'm sorry you are saying that:

    I've posted blogs and comments and schematics for the input amp and the ADC/DAC/FPGA, and inital design notes about the processor and display section.

    The schematic of that last part is nearly done.

     

    Maybe it's time for show of hands as to who is interested enough to think they would actually like to try and build one or be jointly involved in the building of several.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to michaelkellett

    I'm up for it but my interest is in a LCR meter.  Even if it isn't suited for that I would be willing to build one and donate it to someone with a need if there is an archaeological interest from someone without the electronic skills to build one.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Me too, I'd like to build one although mine will be more likely spread out over perspex or something, to work on development, rather than a complete outdoor-capable unit.

    I'm tied up for a couple of weeks but much free-er after that.

    I can also help with building several.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>