Power & Energy
  • Technologies
  • More
Power & Energy
Forum Combining DC and AC signals to one
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 286 subscribers
  • Views 1423 views
  • Users 0 members are here
  • ac-dc
  • power_management
  • circuit
  • Design
  • power
Related

Combining DC and AC signals to one

Eavesdropper
Eavesdropper over 14 years ago
What are some strategies in combining two low voltage DC & AC signals on a single transmission line? IE: 5VDC @ 20A + a small AC signal 0.5VAC 
 
E
  • Sign in to reply
  • Cancel
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 14 years ago in reply to Eavesdropper

    That depends on the length of the cable and the size of the wire.

    In a 5V circuit you cannot afford much voltage drop. For a very short cable this could be done.

    The inductors to separate the AC and DC signal must also have a low resistance to minimize the voltage drop.

    At a higher voltage the current will be lower and you can afford a higher voltage drop.

    At 50V input voltage you could have a voltage drop of 5V over the cable and the inductors and you can still make a stable 5V from the remeining 45V.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Eavesdropper
    0 Eavesdropper over 14 years ago in reply to jvdberg@ieee.org

    JV,

     

    Thank you for the reply and answer. It is very clever. What would you suggest if the DC signal was at 5V@3A?

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 14 years ago
    Powering devices over the signal cable is a technique that is often used.
    For instance to power low noise converters in satellite dishes.
    However I would not recommend using 5 Volt @ 20 A over a  signal cable.
    20 A is too much for most cables.
    A better way is to apply a higher voltage, like 50 Volt, on the signal cable and place a DC-DC converter close to the load to make a stable  5 Volt.
    To separate the DC and the AC-signal an inductor should be used in the DC path and a capacitor in the AC-path at both ends.
     
    To power devices over twisted pairs, you can use the phantom or the superphantom circuit.
    This way more wires are used in parallel for the DC-current.
    See schematic.