Arduino Forum Voltage regulator question (Buck) LM2574 5V 0.5A DIP8
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
  • Replies 48 replies
  • Subscribers 408 subscribers
  • Views 4207 views
  • Users 0 members are here
  • lm2574
  • attiny85
  • power
  • regulator
  • arduino
  • inductor
Related

Voltage regulator question (Buck) LM2574 5V 0.5A DIP8

funinalaska
funinalaska over 11 years ago

So I have a few LM2574 voltage step down regulators.

I would like to use them as the regulator for an ATtiny85 project.

The project is simple, just the tiny and a shift register controlling 8 LEDs for decoration purpose.

I want to run the project off a 9v battery or 12v power supply if I can plug it in where it is being used.

The question I have is in the schematic on the second page of the data sheet it shows hot to use for the fixed voltage output version of the chip (that is what I have it is 5V 0.5A)

It calls for an inductor to be placed on the output before the load.

How critical is that inductor?

I ask because I do not have any yet. I have some on order but who knows when they will arrive.

I am also waiting on the diode as well.

I have the capacitors.

The question is if I were to hook up this regulator to my ATtiny and 595 without the inductor and diode am I going to damage any of the three components or just have it not be reliable?

Sorry, I am not exactly sure what role the diode and the inductor play in this setup.

Thanks for any help

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    The answer is yes you will damage your circuit, If you look on page 11 of the data sheet you will see that there is only one transistor between the input and the output, normally this acts as a switch…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to funinalaska +1
    that kit looks like a good start and the last diode on the list (1N5822) should work great for your D1 on the buck regulator too, it is very close to the specs of the one in the circuit it covers the basic…
  • funinalaska
    funinalaska over 11 years ago in reply to Robert Peter Oakes +1
    Oh, I have definitely earned this: https://www.adafruit.com/products/691 a time or two. I enjoy trying to make things. Most of the components I "play" with are salvage so I don't really care too much if…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    When replying before to your question of measuring caps and inductors, I was not under the impression you where thinking of using them for the buck regulator, Michaels points are all very valid and to make an efficient and reliable module need to be followed.

     

    I was simply providing some basic info on how you could determine their values and perhaps create a fun project along the way with a measurement tool for yourself at the end of it.

     

    it is also fun to experiment with inductors and capacitors while you learn their properties, there is something very satisfying in buildin an LC oscillator, doing the math and finding it running at the calculated frequency image

     

    a thing to note with the buck regulators btw is that you can get the complete unit from ebay for about 4$ or less, not sure what your paying for the inductor, diode and cap but it is worth considering and is much simpler, unless your wanting to learn how to build buck regulators of course, I always keep a few on hand for projects and when i get low, i simply get a pack of 5-10 from ebay to re-stock

     

    never had an issue with them so far except having to wait a few weeks for them to arrive.

    check out http://www.ebay.com/sch/i.html?_trksid=p2053587.m570.l1313.TR3.TRC2.A0.H0.XDC-DC+Buck+Converter+Step+Down&_nkw=DC-DC+Buck+Converter+Step+Down&_sacat=0&_from=R40

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • funinalaska
    funinalaska over 11 years ago in reply to Robert Peter Oakes

    I do have some complete units on order

    I have some of these coming:

    http://www.ebay.com/itm/141255711343?ssPageName=STRK:MEWNX:IT&_trksid=p3984.m1439.l2649

     

    The questions were more related to using the ICs I have, even if it is just experimental

    I really enjoy being a hardware experimenter but I don't know a lot of things about electronics.

    I figure the more I do and the more I ask the more I will learn.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • funinalaska
    funinalaska over 11 years ago in reply to Robert Peter Oakes

    So that Boost regulator says it is a 2A max continuous

    for 10 350mA LEDs would I not need something that can handle 3.5A continuous?

    I am looking to see if I can find a more powerful one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • funinalaska
    funinalaska over 11 years ago in reply to Robert Peter Oakes

    I suppose I could get 4 of those and run 2 per fixture that is 5 350mA LEDs per boost module.

    Just run the 5v power to the fixture and split it out to the 2 boards there.

    I am not interested in dimming these, so I do not need any other control

    The question is do I run all 5 LEDs in series then?

    I am still foggy as to how to use a constant current regulator when running LEDs in series.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to funinalaska

    if you had the LEDs in parallel, yes, the whole idea of this is they can be in series and therefore if you had 5 in series on one sconce and 5 in series in the other, that will only be 700mA but at 5* the LED voltage which would be about 15V

     

    up the boost to 30V and you can have all in series and only have to drive 350mA on the output, the input would consume the same power but at the 5V * 3.5 amp instead of 30V * .350A approximately

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to funinalaska

    boost at t he power supply, not the sconce and then you distribute 15 or 30V instead at way less current, put the LEDS in series

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Robert Peter Oakes

    The other option is to use 4.7 ohm resistors and figure the voltage is less than 5v.

    The reality is the drop over 40 ft of 1.5A rated mains cable is not going to be that great, but you could always measure the resistance and adjust accordingly.

     

    note sure what cable ratings you guys use, but this might help

    Voltage Drop Calculator

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • funinalaska
    funinalaska over 11 years ago in reply to mcb1

    The reality is one sconce is right on the other side of the wall from the power supply and control enclosure, so in a poor execution of cable running that sconce will have at most 5 feet of wire running to it.

    The other one is on the other side of the door.

    So I need to drop down under the floor or up through the ceiling, but I will say that either way probably less than 12 feet.

    I will probably go through the ceiling since there is already a chase there from running wire for the strip lights.

    I am not thinking I am going to have much to worry about in the way of voltage drop.

    There is a whole mess of 16ga stranded wire there that I think I am going to use for the run, probably ridiculously overkill, but at least then I don't have anything to worry about.

     

    I was looking for boost modules for this and ran across someone's spec of a LM2577 module and they stated that:

    An input of 5V and an output of 12V will be stable up to 800mA

     

    That worried me about having to boost all the way to 30V

     

    So I think simplicity is my answer, it is easy and cheap to replace a resistor if something stops working I only lose one LED, if I lose one of those boost modules I lose an entire fixture.

     

    Just my thought.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to funinalaska

    So I think simplicity is my answer

    An often overlooked quantity.

     

    If it doesn't work out, you can always go with plan B and try 5 in series at 350mA. which is about 20v give or take.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to mcb1

    totally agree, if those are the distances and your using 16AWG wire and can deal with the heat of the resistors... why not.

     

    I have to remind myself your using commonly available parts you have around too so my suggestion while viable and more efficient is perhaps over kill in this situation

     

    btw, would be great to see some pictures or even better a video once your done

     

    Good luck, if you need more help, you know where we are

     

    peter

     

    Oh, the buck regulator I linked to was to show you an example, to show an idea of what could be done to mitigate the power drops if it proved to be an issue, it was not necessarily the best one for your situation

     

    it looks like your good to go

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • funinalaska
    funinalaska over 11 years ago in reply to Robert Peter Oakes

    So do you think 16ga is heavy enough or should I go to 12ga?

    I do have both in ample quantity.

    The other question is how can you figure out the rated heat dissipation of a heatsink?

    I know there is some function of mass and surface area, but I have no idea how that works.

    I am hoping that the ones that I have will be sufficient for the 1 or so watt per resistor of heat that will be generated. I don't mind having a small space heater and since it is open both above and below it there is plenty of opportunity for convection, I am just curious.

    It may be a couple weeks before I get to actually implementing this project, I will be leaving Alaska for the summer in a couple days to go visit for the summer and at some point complete this job which was started last summer. LOL I will try to get back here and at least report on the success of the on the plan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to funinalaska

    Andrew

    The link I gave was in guage size, so plug some figures in.

     

    Heatsinks are rated in deg C/W, however finding out what you have is nearly impossible.

    Video cards produce lots of heat, so its likely they are pretty efficient, but usually they have forced air as well.

    Google it and you might find http://www.sm0vpo.com/begin/heat-0.htm

     

     

    You could do an experiment .... or use the imperically derived method  ... ie try it and see.

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 11 years ago in reply to funinalaska

    Andrew

    The link I gave was in guage size, so plug some figures in.

     

    Heatsinks are rated in deg C/W, however finding out what you have is nearly impossible.

    Video cards produce lots of heat, so its likely they are pretty efficient, but usually they have forced air as well.

    Google it and you might find http://www.sm0vpo.com/begin/heat-0.htm

     

     

    You could do an experiment .... or use the imperically derived method  ... ie try it and see.

    Mark