Tech Connection
  • Learn
  • Learning Center
  • Tech Connection
  • More
  • Cancel
Tech Connection
Documents How Do Light Convergent Reflective Sensors Work?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Tech Connection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 18 Oct 2021 4:03 PM Date Created
  • Last Updated Last Updated: 4 Nov 2021 6:07 PM
  • Views 4863 views
  • Likes 0 likes
  • Comments 2 comments
Related
Recommended

How Do Light Convergent Reflective Sensors Work?

Take the Poll | Join our Discussion

sponsored by

logo

Have You Ever Wondered How Sensors Detect Objects of All Colors and Textures?

Sensors are essential to enhancing productivity and safety in several industries, including factories, where automation has become increasingly commonplace. Photoelectric (optical) sensors are ubiquitous nowadays, safely controlling elevators, opening grocery store doors, and even detecting winners at racing events.

 

The continuous evolution of automated industrial equipment requires that sensors discover objects with exacting precision, while being immune to container and package design variations. Conventional diffuse reflective sensors function well with objects of certain material and color combinations, but can become unstable and inaccurate when specifications differ. In contrast, sensors based on convergent reflective technology are able to detect objects having a much wider variation in material, color, or reflectiveness.

 

This Tech Spotlight article focuses on light convergent reflective sensors, including how they work, their advantages and disadvantages, and example applications.

 

What is a Light Convergent Reflective Sensor? A light convergent reflective sensor works based on a convergent beam principle. The convergent reflective sensor uses a lens system that focuses the emitter and receiver elements to a point in front of the sensor. The sensor is able to detect objects in the area (sensing area) where the emitting beam and the light-receiving area overlap. Because the light energy is focused on a smaller area, gain is increased, allowing the sensor to more easily detect narrow or low reflectivity targets, and making it color and texture agnostic (black, white, or shiny).

 

What Is the Difference Between Diffuse and Convergent Reflective Sensors?

A photoelectric or optical sensor works through the transmission and reception of light. A common method of target detection is by the use of diffuse reflective sensors. Another approach of target detection is with convergent reflective sensors. Let's learn how these two types of sensors work.

 

  • How Do Light Diffuse Reflective Sensors Work?

In a diffuse reflective sensor, objects are detected based on the light that they reflect. A transmitter sends a beam of light in a specific direction. If there is an object present in the beam, it will reflect some or all of the light. A receiver, sharing the same housing as the transmitter, senses the reflected light, successfully detecting the object. Although it depends on the sensor size and power, diffuse reflective sensors typically have shorter detection ranges than other designs, generally less than one meter. Additionally, an object's color, finish, size, and shape directly impact the amount of light that is reflected back to the sensor.

 

  • How Do Light Convergent Reflective Sensors Work?

A light convergent reflective sensor works based on a convergent beam principle. Unlike diffuse sensors, the convergent reflective sensor uses a lens system that focuses the emitter and receiver elements to a point in front of the sensor. The sensor is able to detect objects in the area (sensing area) where the emitting beam and the light-receiving area overlap, as shown in Figure 1. Because the light energy is focused on a smaller area, gain is increased, allowing the sensor to more easily detect narrow or low reflectivity targets, and making it color and texture agnostic (black, white, or shiny).

image

Figure 1: Light diffuse reflective type (left) and convergent reflective type (right) sensors

Image Source: Omron Light Convergent Reflective Type Sensor B5W-LB Series Manual.pdf

 

Let's Dig a Little Deeper Into the Light Convergent Reflective Sensor

A light convergent reflective sensor consists of an integrated light source (LED), a receiver (phototransistor), and an optical system (lens), as illustrated in Figure 2. Optical lens structures focus the beam from the light source, as well as the detection path of the receiver, limiting the detection range to the area in which the beam and detection path converge. If an object is present in the detection range, it will reflect light back to the receiver. Because both the LED and receiver are focused rather than spread out, sensitivity is much higher, increasing the range of textures and colors that can be detected. The sensor is unable to detect outside this sensing range.

image

Figure 2: Structure and Working of a Light Convergent Reflective Sensor

 

Let's Take a Look at The Advantages and Disadvantages of Light Convergent Reflective Sensors

The primary advantage of light convergent sensors is their more accurate detection of difficult materials, such as shiny textures or dark colors. Their other advantages over traditional diffuse reflective sensors include:

 

Advantages

 

  • Greater Accuracy: Figure 3 shows one scenario where a convergent reflective sensor yields more accurate results when compared to a traditional diffuse reflective sensor. Because the beam of a diffuse reflective sensor might sense objects from farther away, it may confuse backgrounds for objects. A convergent reflective sensor limits detection range to a small area in front of the sensor, so objects just outside of this area are not detected. Additionally, a convergent reflective sensor can more accurately detect dark colors because of its increased sensitivity.

image

Figure 3: Background Effect with Traditional Reflective (left) and Convergent Reflective (right) Sensors

Image source: Omron

 

  • More Stability: Convergent reflective sensors have more stable and accurate detection across the color spectrum, and for a larger variety of textures.

 

 

image

Figure 4: Object Shifting with Convergent Sensor

Image Source: Omron

 

  • Ability to Detect Shifting Objects: A convergent reflective sensor is capable of detecting shifting objects, due to its increased sensitivity and wider sensing range. In the Omron B5W-LB, the enhanced sensing range is made possible by the use of four toroidal lenses, which help ensure a robust signal even at times when the distance of the object is not static.

 

Sensors

Shop our wide variety of sensors and transducers by Omron electronic components.

Shop Now


Don't forget to take our poll.

  • Ability to Detect Objects of Specific Shapes: Because the multiple lenses of a convergent sensor are focused on a small detection range, they have additional flexibility when used to detect objects of specific shapes. One example is a radiused object (cylinder or circle). A convergent sensor can focus on the nearest point (tangent point) of a radiused object, making it useful for applications like counting stacked cans or bottles.

 

Disadvantages

 

  • Limited Detection Range: The primary disadvantage of a convergent sensor is its limited detection range. Objects that that are too close or too far will not be detected. Additionally, objects that are too far above, below, or to the left or right of the focal point of the sensor’s lens will not be detected.

 

  • Object Detection at Predictable Distances: Convergent sensors are only suited to applications where detection targets appear at predictable distances from the sensor.

 

Omron's Light Convergent Reflective Sensors

Omron offers a range of light convergent sensors, including the B5W-LB series, which consists of a proprietary lens structure (with visible cutting filter), an infrared LED, a light receiver, and an analog circuit. The B5W-LB series is available in miniature and super-miniature form factors, with sensing range from 2-10 and 10-55mm, and digital and analog output models. Table 1 shows the product line of the B5W-LB series.

 

B5W-LB11 SeriesB5W-LB21 SeriesB5W-LB21 Series
Output MethodDigitalDigitalAnalog
TypeSuper MiniatureMiniatureMiniature

Sensing Distance

(White Paper)

2 to 10 mm10 to 55 mm10 to 55 mm
Supply Voltage24VDC +/- 10%24VDC +/- 10%5VDC +/- 10%
Output ConfigurationLight ON | Dark ONLight ON | Dark ON--

Table 1: The B5W-LB Series

Image Source: Omron Light Convergent Reflective Type Sensor B5W-LB Series Manual.pdf

 

What Can You Use Light Convergent Reflective Sensors For?

Light convergent sensors are ideal for detecting objects at predictable distances, as well as objects made from materials which are typically difficult to detect. They are used in a wide variety of equipment, including:

  • Analytical Instruments
  • Food Manufacturing Automation
  • Sanitation
  • Coffee Machines
  • Vending Machines
  • Dental Equipment
  • Medical Packaging Machines
  • Printers
  • Robot Material Handling
  • Automated Test Equipment

 

1. Cup Detection for a Coffee Machine: While a traditional diffuse reflective sensor can be used to detect the presence of cups in a coffee machine, the problems inherent in their design make them less than ideal. Coffee mugs come in a wide variety of colors and textures, many of which a traditional diffuse reflective sensor has trouble detecting. On the other hand, light convergent reflective sensors can successfully detect a much wider variety of colors and textures. A cup’s position is also important. The coffee maker should run only when the cup is in the correct position. Because of the small area created by the converging beams, light convergent sensors are much more accurate at detecting a cup’s position.

 

2. Touchless Sensors on a Vending Machine: Touchless buttons enable a user to "press" a button without physically pressing a button, providing better hygiene and decreasing the potential for mechanical failure. Touchless buttons can be created using light convergent reflective sensors. Because each “press” only occurs when the user’s finger comes in close proximity with the button, detection range is predictable. Light convergent reflective sensors will also not be confused by objects in the background, such as another person standing close by. They are able to detect a wide variety of colors and materials, making detection accurate whether the user is wearing gloves or using bare hands.

image

Figur-e 5: Vending Machine with Convergent Reflective Sensor

Image Source: Omron

 

Vending machines often have doors that open for users to retrieve products. Because vending machines have varying graphics and design, their doors may not always be the same color, making it difficult to use a traditional reflective sensor to detect if a door is open or closed. Light convergent sensors are better suited, because of their higher accuracy in detecting objects of different colors.

 

Multiple applications such as food manufacturing equipment automation, hand detection for sanitation equipment, and touchless sensing for dental equipment depend on light convergent sensors for object detection.

 

Let's Recap: Light Convergent Reflective Sensor Technology

Light convergent sensors have several advantages over conventional reflective sensors for many applications, the primary one being increased sensitivity to a wider range of colors and textures. Light convergent sensors have a smaller detecting area, making them ideal for applications where the target object is at a predictable distance from the sensor. Like traditional diffuse reflective sensors, they are self-contained, making them convenient for applications with space constraints.

 

B5W-LB2101-1B5W-LB2122-1B5W-LB1122-1

B5W-LB2101-1

 

 

Light Sensor, Miniature

Buy NowBuy Now

B5W-LB2122-1

 

Light Sensor, Miniature

Buy NowBuy Now

Home> Sensors & Transducers> Sensors> Light Sensors> Optical / Slot Photoelectric Sensors  Spotted an Error?  Print Page B5W-LB1122-1

 

Light Sensor, Super Miniature

Buy NowBuy Now

  • ability to detect objects of specific shapes
  • cup detection in a coffee machine
  • object detection
  • texture
  • sensitivity
  • colors
  • touchless sensors on a vending machine
  • accuracy
  • reflectiveness
  • diffuse reflective sensors
  • transmitter
  • b5w-lb
  • phototransistor
  • stability
  • photoelectric
  • target
  • ability to detect shifting objects
  • light convergent reflective sensors
  • shapes
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • dougw
    dougw over 4 years ago

    Interesting - I had not seen this technology before.

    By a strange coincidence I am building a sensor that I think uses the same or similar principle, although it doesn't look anything like these sensors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago

    I'm not sure I'm getting the point.

    Article says a light source is directed toward direction, and the receiver is focused along the beam's pathway so wherever its focused gets the best detail ? seems kinda obvious. Anywhere the receiver is focused would be a sensor's sweet spot, no ?

    Is it like a Autostereogram, where you cross your eyes to see an image ?

     

    The mini is fairly inexpensive, maybe will have to play with it.