DC to Daylight
  • Challenges & Projects
  • element14 presents
  • DC to Daylight
  • More
  • Cancel
DC to Daylight
Documents Driving LEDs to Create a Flux Capacitor -- DC to Daylight 08
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DC to Daylight to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 10 Mar 2022 3:57 PM Date Created
  • Last Updated Last Updated: 16 Mar 2022 8:24 AM
  • Views 36664 views
  • Likes 6 likes
  • Comments 6 comments
Related
Recommended

Driving LEDs to Create a Flux Capacitor -- DC to Daylight 08

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In this episode we make a PWM LED driver using transistors and an Arduino Nano, which provide dimming and sequencing functionality for a Flux Capacitor. While not an exact replica, it does make a good demonstration of pulse width modulation and how to drive LEDs with a current sink/source

Supplemental Content:

  • Resources

element14 presents

element14 presents  | About Derek  |  DC to Daylight

  • LED driver
  • arduino nano
  • back to the future
  • derek
  • arduino pwm
  • current source
  • flux capacitor
  • pulse width modulation
  • pwm led
  • light emitting diode driver
  • current sink
  • arduino
  • bttf
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • beacon_dave
    beacon_dave over 4 years ago

    Ever get the feeling that you may be underdressed and that your wardrobe is somewhat lacking when watching these Element14 videos ?  Slight smile

    Good to see the theory from a previous episode being put into practice in a project.

    One minor addition may be to add an external PWM driver to increase the number of LED's from the existing 5 per row so as to be able to increase the control you have over the lighting effects. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps
    #define A_OFFSET 0
    #define B_OFFSET 85
    #define C_OFFSET 130
    #define MAX_OFFSET C_OFFSET

    // helper method

    void setLed(uint8_t pin, uint32_t value, uint8_t offset) {
    uint8_t intensity = 0;
    if (value > offset) {
    intensity = (value - offset) > 255 ? 255 : (value - offset);
    }
      analogWrite(pin, intensity);
    }

    // ...
    for (uint32_t counter = 0; counter <= 255 + MAX_OFFSET; counter++) {
    setLed(A, counter, A_OFFSET);
      setLed(B, counter, B_OFFSET);
      setLed(C, counter, C_OFFSET);
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to e14 Contributor

    If you stick all 5 brightness values into an array then you can loop through that array to drive the LEDs.

    You then do 'math' on the array to change the effect.

    e.g. for a comet tail type effect you might reduce all the current values of the array by 'x', then set the leading LED value to max.

    The values of the array then get written to the LED's at the next update.

    You again reduce all the current values of the array by 'x', then turn the next leading LED value on to full.

    By doing so you get a fade-out effect following the leading LED.

    You may also want to replace your 'blocking' delay() functions with non-blocking code.

    If you assign the value returned by millis() to a variable to store the current time (since boot), then later in the code check to see if the time now is greater that the stored time plus an offset value in milliseconds and only if so, then write the contents of the array to the LEDs. Finally update the stored value with the current time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    ... but that will make led 2 and 3 flip directly to their offset value, and that's not what you want he?

    Changing the helper function should fix that. Thinking ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to e14 Contributor

    One loop should do:

    Let's say as example that when LED A is 0, then B is 85, 3 = 130 (each 1/3 offset of each other).

    #define A_OFFSET 0
    #define B_OFFSET 85

    #define C_OFFSET 130

    uint8_t counter = 0;



    // helper method

    void setLed(uint8_t pin, uint8_t value, uint8_t offset {

      uint8_t intensity = ((uint32_t)(value + offset)) > 255 ? 255 : (value + offset);

      analogWrite(pin, intensity);

    }




    // where you want to make them glow:

    for (counter = 0; counter <= 255; counter++) {

      setLed(A, counter, A_OFFSET);

      setLed(B, counter, B_OFFSET);

      setLed(C, counter, C_OFFSET);

    }
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 4 years ago

    Hello all! If you have suggestions on how to improve this project, especially related to software let me know here. One of the things I'd like to do is to "power up" three LEDs at the same time so the pulsing looks more natural... meaning three of the LEDs are actively ramping through the PWM values out of phase. I think this would require three nested loops and maybe a state machine. Ideas?