DC to Daylight
  • Challenges & Projects
  • element14 presents
  • DC to Daylight
  • More
  • Cancel
DC to Daylight
Documents DC to Daylight 31: How a Wheatstone Bridge Works
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DC to Daylight to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 10 Oct 2023 3:01 PM Date Created
  • Last Updated Last Updated: 10 Oct 2023 3:15 PM
  • Views 1951 views
  • Likes 3 likes
  • Comments 2 comments
Related
Recommended

DC to Daylight 31: How a Wheatstone Bridge Works

In this episode of DC to Daylight, Derek gives us an overview of Wheatstone bridges and how they work. Wheatstone bridges are a clever configuration of resistors arranged in a diamond pattern, with voltage sources connected at one set of terminals and a galvanometer across the remaining two terminals. By adjusting the resistances in each arm of the bridge, we can control the voltage ratios across each resistor. When these ratios are balanced, no current flows through the meter, indicating an equilibrium. This balance allows us to accurately determine an unknown resistance when compared to known resistors. 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
 

Derek explains this concept of the Wheatstone bridge using an easy-to-grasp water analogy. When both arms of the bridge have equal flow rates and directions, there's no flow between them, representing the bridge in equilibrium. If there's an imbalance due to unequal resistances, current flows, providing a way to calculate the unknown resistance. 

image

Derek goes on to explore the practical implementation of Wheatstone bridges, explaining how they can be used to measure unknown resistors with great accuracy. He shows a mini-teardown of a Wheatstone bridge on his bench, demonstrating how it's set up and used to measure a 47-ohm resistor within a 5% tolerance, showcasing its practicality and precision. 

image 

The teardown also reveals the inner workings of the Wheatstone bridge, with precision wire-wound resistors and multiple layers of contacts to reduce contact resistance. It's evident that the device uses dielectric grease to prevent corrosion, ensuring its reliability over time. 

 image

In conclusion, Derek highlights the enduring relevance of Wheatstone bridges in applications such as load cells and sensors, even as digital multimeters become more common for these applications today.  

image

image

 

element14 presents

element14 presents  | About Derek  |  DC to Daylight

  • Wheatstone Bridge Teardown Breakdown
  • Electronics safety
  • Electronics Tutorial on Wheatstone Bridges
  • Wheatstone Bridge Operation
  • wheatstone circuit
  • Precision Resistance Measurement Guide
  • voltage divider
  • Exploring Electronics Insights
  • Advanced Resistance Measurement
  • In-depth Circuit Analysis
  • Understanding Precision Resistors
  • Electronic Enthusiast Resources
  • Electronic Component Explained
  • Opto-isolation
  • Inside a Wheatstone Bridge Device
  • Demystifying Wheatstone Bridges
  • Electrical Measurement Techniques
  • Electrical components
  • unknown resistance
  • Accuracy in Resistance Measurement
  • wheatstone bridge
  • Electronic Circuit Insights
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • beacon_dave
    beacon_dave over 3 years ago

    Another nice episode.

    I think I last played with a Wheatstone bridge circuit in Physics class at college. I recall it was more of a plugboard and box of resistors type setup though rather than an all in one instrument. I suspect I may use them daily though in the form of strain gauge circuits in bathroom weighing scales.

    It looks like your vintage Rubicon bridge is wired to use reverse polarity from that of your (and most other) schematic drawings ? 

    Do you know what resistances they have used in the multiplier ratio ladder ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 3 years ago

    Very good episode.

    We had a meter like that back in high school.

    Unfortunately, we never got to use it.

    When I got to tech school, they had already moved on to Simpson meters, but we did talk about them in class and ran some simple experiments in the lab.