1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog 1 Meter of Pi, blog #6
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
  • Author Author: hugohu
  • Date Created: 28 Dec 2020 2:38 AM Date Created
  • Views 456 views
  • Likes 2 likes
  • Comments 0 comments
Related
Recommended

1 Meter of Pi, blog #6

hugohu
hugohu
28 Dec 2020

Welllll

 

Relays are very interesting.

 

I'm setting up one right now, with an arduino uno.

 

I've set the setting for 1 second of high-stream water dispense, per every 6 hours.

 

Here's the code.

 

int RelayPin = 12;


void setup() {
  // Set RelayPin as an output pin
  pinMode(RelayPin, OUTPUT);
}


void loop() {
  // Let's turn on the relay...
  digitalWrite(RelayPin, LOW);
  delay(21600000);
  
  // Let's turn off the relay...
  digitalWrite(RelayPin, HIGH);
  delay(3000);
}
int RelayPin = 12;


void setup() {
  // Set RelayPin as an output pin
  p

 

I mean according to my mental math tis is 6 hours

 

I'll come and post more updates once I'm done.

 

BTW a bit more:

 

I'm using a 4 channel relay, only one is activated, powering with 12V DC, (Breadboard PSU because I don't have any of those connectors) and a standard 12V DC adapter. I've hooked it up to an UNO and a 12V water pump, with a straw(since I ran out of those TPU tubes) and a TPU tube.