1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog 1 METRE OF PI – SEVENTH POST – MAIN ELEMENTS – SPECIAL PUMP
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
  • Author Author: stevotech
  • Date Created: 9 Dec 2020 3:32 PM Date Created
  • Views 832 views
  • Likes 3 likes
  • Comments 1 comment
  • 1meterofpi
Related
Recommended

1 METRE OF PI – SEVENTH POST – MAIN ELEMENTS – SPECIAL PUMP

stevotech
stevotech
9 Dec 2020

Since my last blog on Construction, I have been focusing on Item 4 on the list of Main Elements. Bringing to the fore the need to maintain good growing conditions, I have spent a huge amount of time working on an automated system – eventually to be controlled by a Raspberry Pi 4 and PIM 487/486/300 assembly - to provide controlled levels of moisture/water, humidity, and adjustable temperatures - and I think I have an answer: ‘GIZZMOTO’ a no-moving parts pump with a telescopic outlet/extension and distribution head attachment.

 

A full-size pump body/base/stand assembly has been 3D printed.

See: MVF-GIZZMOTO.jpg

It works on fluid dynamics principles, using low pressure compressed air (*). A significant feature is that it propels water (or air) with a spinning action. It has been tested and works.

See: GIZZMOTO Spinning Action.mp4

The spinning action can be used in conjunction with the distribution head attachment.

 

I have designed and made a scale-model of the special pump with a telescopic outlet/extension and a distribution head attachment. For comparison, I have taken a photograph showing the comparison with the full-size GIZZMOTO (no outlet or head attachment) and the scale-model, complete with its base tank, telescopic extension, and head attachment.

See: MVF-GIZZMOTO SM & FULL A.jpg

The assembly can be extended in 4 stages.

See: MVF-GIZZMOTO STAGE 1.jpg, MVF-GIZZMOTO STAGE 2.jpg, MVF-GIZZMOTO STAGE 3.jpg, MVF-GIZZMOTO STAGE 4.jpg

 

The scale-model special pump has been physically located in the centre of the previously constructed scale-model multi-level vertical farm and each stage manually positioned at each of the four levels.

See: MVF-LEVEL 1.jpg, MVF-LEVEL 2.jpg, MVF-LEVEL 3.jpg, MVF-LEVEL 4.jpg

 

It should be evident that at each level the special pump’s distribution head attachment will be positioned to use the spinning action generated by the pump to spray out a water aerosol across the plants.

See: MVF-GIZZMOTO HEAD 1.jpg

The head attachment is shaped to accentuate the spinning action.

See: MVF-GIZZMOTO HEAD ATTACHMENT.jpg

 

*Extra Note: As well as using compressed air, the special pump could be powered by carbon dioxide or nitrogen, that might speed-up the growing process.

1meterofpi raspberry_pi, design challenge, raspberry pi 4 2gb, 1 meter of pi, 1_meter_of_pi, 1 meter of pi - design challenge

Attachments:
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
  • ajcc
    ajcc over 5 years ago +1
    You can add the pictures into the text either by dragging and dropping them into the online editor or by uploading them with the picture tool. Leave the cursor at the location in the text where you want…
  • ajcc
    ajcc over 5 years ago

    You can add the pictures into the text either by dragging and dropping them into the online editor or by uploading them with the picture tool. Leave the cursor at the location in the text where you want to add the image, then click the [Insert image] icon:

    image

    Then click [Browse...] and use the file manager to open your image.

    image

    Then write a description and [Insert image] to insert it into the text.

    image

    That's it! There's also an [Insert video] that works in a similar way. Hope that helps in creating a nicer blog!

    Sadly I can't find a way to add the images from the attachments so you will have to re-upload them again.