1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Mushrooms' Paradise #1. Initial Plan
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
  • Author Author: ilvyanyatka
  • Date Created: 1 Nov 2020 7:45 AM Date Created
  • Views 2238 views
  • Likes 10 likes
  • Comments 8 comments
  • 1meterofpi
  • raspi
  • 1 meter of pi
  • 1 meter of pi - design challenge
  • raspberry pi
  • mushrooms' paradise
  • growing mushrooms
Related
Recommended

Mushrooms' Paradise #1. Initial Plan

ilvyanyatka
ilvyanyatka
1 Nov 2020

The whole Mushrooms' Paradise blog

 

 

  • Abstract
  • Setup
    • Environment
    • Enclosure
    • Light
    • Irrigation
    • Power source
    • Air circulation
    • Camera

Abstract

 

My project will be to grow as many mushrooms as possible in a contained space. I also want to experiment and see if I can grow lettuce and radishes in the same environment.

 

 

 

 

Choice of crops

 

All the crops are chosen to maximize the amount of protein, fiber, vitamins and micro elements.

 

Mushrooms are selected because they are a superfood. They are full of vitamins, protein, fiber and antioxidants. Protein and vitamins make them a great choice for nutrition. They are also a good choice for health reasons. Antioxidants help to prevent cancer, beta glucan – soluble fiber  - helps to prevent diabetes by regulating blood sugar and lowering cholesterol. Mushrooms are packed with B vitamins that prevents heart diseases and depression. Copper is available for red blood cells, bones and nerves. Potassium is good for the heart, muscles and nerve functions.

Mushrooms are efficient to grow because of ratio of harvest per square foot. They also can grow on shelves stacked together, as they are not growing high.

 

Lettuce has good nutritional value, and is a source of fiber, vitamins and bioactive compounds. Lettuce has anti-inflammatory, cholesterol-lowering, and anti-diabetic properties.

Lettuce is very efficient to grow, you can harvest up to 5 times from one crown.

 

Radishes are highly effective crop, with a short time to harvest and both roots and leaves are edible.

They contain vitamin C, potassium, folate, riboflavin, niacin, vitamin B-6, vitamin K, calcium, magnesium, zinc, phosphorous, copper, manganese, and sodium.

They are a good source of protein and fiber, used as folk remedies to treat many conditions such as fever, sore throat, bile disorders, and inflammation. Fiber and antioxidants in radishes work to prevent cancer. Radishes juices work to prevent gastric ulcers and inflammation.

 

 

Setup

 

Environment

Enclosure will be indoors, with outside temperature 68-78F (20-26C), 1g gravity

 

Enclosure

1 m3 enclosure made inside of an up-cycled old fridge. As a back up plan (in case fridge enclosure will not work out) – separate plywood enclosure. Inside enclosure there will be the shelves with the containers for the crops. All the crops are low growing, so I can stack several shelves there.

 

Light

Mushrooms don’t need much light and dim light for 6 hours a day will be enough. Radishes and lettuce don’t need much light also, but still need more than mushrooms. Therefore I will put them on the shelves closest to the light source. The light will be turned on/off automatically by timer.

 

 

 

 

Medium

 

Mushrooms: For the medium I will use a mix of perlite and vermiculite. Initially I wanted to grow boletus mushrooms, but after some research I realized they need living tree roots to grow. So I decided to grow chicken of the woods and puffballs due to their nutritional value and shape that maximize volume. I will use liquid mycelium as well.

Lettuce and radishes: I will use the same medium but with liquid fertilizer provided. I will start growing these crops from seeds.

 

 

Irrigation

 

Irrigation will be done for top shelves only, for lettuce and radishes. Mushrooms don’t need irrigation as they take all necessary water from air. I will use soil humidity sensors to control water flow for irrigation.

 

 

 

 

Humidity

 

Humidity is critical for mushrooms. I will use humidity/temperature sensor to keep humidity around 80% all the time. There will be hot humidifier controlled by PI. Because enclosure from the fridge is sealed, temperature will be controlled by humidifier as well. As a back up plan, I can put a small heater into the enclosure, but I prefer to avoid it to save the space for the crops.

 

 

Power source

Outside 110V 1500W max power source. If outside source is not available – Jackery battery and a solar panel.

 

 

Air circulation

It will be done with an exhaust fan from an old computer and an intake with a filter.

 

 

Camera

To monitor crops growth and ideally make a time lapse.

 

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 6 years ago +4
    "...Mushrooms are packed with B vitamins..." I seem to recall that if you expose mushrooms to UV light you can get a source of vitamin D from them as well. A Review of Mushrooms as a Potential Source of…
  • DAB
    DAB over 6 years ago +3
    Good plan. Mushrooms are a nice space efficient source of food. You might want to add an air humidity sensor with them, they do not like to get too dry and the recycled air in space is usually very dry…
  • DAB
    DAB over 6 years ago in reply to feiticeir0 +3
    You left out dangerous. Not all mushrooms should be eaten, know what they are before you consume. DAB
  • feiticeir0
    feiticeir0 over 6 years ago in reply to DAB

    I know that there are some mushrooms you only eat once ! image But those I don't know (and I don't want to know) if they are delicious or not ! I just care about the ones one can eat without worrying if it's the last meal or not !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ilvyanyatka
    ilvyanyatka over 6 years ago in reply to beacon_dave

    Thank you, I will read it. Yes, vitamin D is a problem with my design as it is now. I was not planning on using UV lights, but now it sounds like a great solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago

    "...Mushrooms are packed with B vitamins..."

     

    I seem to recall that if you expose mushrooms to UV light you can get a source of vitamin D from them as well.

     

    A Review of Mushrooms as a Potential Source of Dietary Vitamin D

    https://www.ncbi.nlm.nih.gov/pmc/articles/PMC6213178/

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ilvyanyatka
    ilvyanyatka over 6 years ago in reply to feiticeir0

    Thank you. I am a big fan of (edible) mushrooms too. But never tried to grow them so far. I think it will be fun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago in reply to feiticeir0

    You left out dangerous.

    Not all mushrooms should be eaten, know what they are before you consume.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>