1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Forum Is Enviro HAT working for you reliably?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 6 answers
  • Subscribers 4 subscribers
  • Views 3153 views
  • Users 0 members are here
  • enviro hat
  • 1 meter of pi
  • 1 meter of pi - design challenge
Related

Is Enviro HAT working for you reliably?

ilvyanyatka
ilvyanyatka over 5 years ago

Hello,

I am having issues with Enviro HAT humidity and temperature sensors. I wonder if mine is defected or if I am missing something on how to use it. It is not snapped on Raspberry PI but connected by jumper wires.

1) The first humidity reading is often (not always) more than 90, the second and so on drops down to 30-40

2) In the same room 2 minutes apart humidity value can change up to 15 points. For example, first reading - 42, second - 27

3) Temperature value drops much below real value if humidity grows. For example, in the same room with 22C/40% humidity, if humidifier is running, next reading it 10 minutes will show 16C/55% humidity

 

Do you have any idea why?

TIA

  • Sign in to reply
  • Cancel

Top Replies

  • feiticeir0
    feiticeir0 over 5 years ago +2 suggested
    Hi Victoria. I'm going to guess that the problem may be the connections - maybe the jumper wires are not well connected to the PINs or some may be faulty ? I had problems before with loose jumper wires…
  • ilvyanyatka
    ilvyanyatka over 5 years ago in reply to feiticeir0 +2
    Thank you Bruno. When I initially tested it while it was snapped on the PI - the first issue definitely was happening. The one with 90% of humidity readings. It will be hard to snap it on now to test the…
  • skruglewicz
    skruglewicz over 5 years ago +2 suggested
    Hi ilvyanyatka I have the enviro hat connected with jumper wires and the sensor is behaving reasonable well in My blog# 10 at this location I describe my script to check the Humidity in the growing house…
Parents
  • feiticeir0
    0 feiticeir0 over 5 years ago

    Hi Victoria.

     

    I'm going to guess that the problem may be the connections - maybe the jumper wires are not well connected to the PINs or some may be faulty ? I had problems before with loose jumper wires.

     

    Can you test it by snap the two together ?

     

    Mine is working fine without those reading swings.

     

    Try and test both snapped to see.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • feiticeir0
    0 feiticeir0 over 5 years ago

    Hi Victoria.

     

    I'm going to guess that the problem may be the connections - maybe the jumper wires are not well connected to the PINs or some may be faulty ? I had problems before with loose jumper wires.

     

    Can you test it by snap the two together ?

     

    Mine is working fine without those reading swings.

     

    Try and test both snapped to see.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ilvyanyatka
    0 ilvyanyatka over 5 years ago in reply to feiticeir0

    Thank you Bruno.

     

    When I initially tested it while it was snapped on the PI - the first issue definitely was happening. The one with 90% of humidity readings.

    It will be hard to snap it on now to test the other 2 issues because I use a lot of other GPIO pins that Enviro HAT will cover if I snap it on the PI. I will really need to disassemble the whole setup.