At The Core Design Challenge
  • Challenges & Projects
  • Design Challenges
  • At The Core Design Challenge
  • More
  • Cancel
At The Core Design Challenge
Blog ATCDC: Digimorf, Day 20, The project SEGA SG-1000 Emulator, VGA on PSoC62S4 Pioneer kit - part 5
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join At The Core Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Digimorf
  • Date Created: 19 Mar 2023 7:10 PM Date Created
  • Views 1242 views
  • Likes 11 likes
  • Comments 8 comments
  • infineon
  • PSoCTm︎ 62 MCU
  • gpio
  • video
  • pwm
  • PSoC 62S4 pioneer kit
  • 320x240
  • vga
Related
Recommended

ATCDC: Digimorf, Day 20, The project SEGA SG-1000 Emulator, VGA on PSoC62S4 Pioneer kit - part 5

Digimorf
Digimorf
19 Mar 2023
ATCDC: Digimorf, Day 20, The project SEGA SG-1000 Emulator, VGA on PSoC62S4 Pioneer kit - part 5

I think that the first goal is reached. the Pioneer Kit is able to show a real 320x240 8bpp image!

image

image

Now it's time for making the VGA video driver more flexible so that I can change the horizontal and vertical resolution for my emulator. I need also to build a better 8-bit resistor DAC to improve the colors.

This driver makes use of one TCPWM that drives the HSync pulse with a PWM wave. An interrupt fired by this counter launches an ISR that handles the VSync, and the stream of pixels for every scanline of the vertical active area.

The clocking system uses the ECO clock, and the PLL to generate a 100MHz clock signal for the peripheral clock. I decided not to go at 150 MHz because the peripheral clock can only work at maximum 100MHz, and I should have divided the clock by 2, resulting in a peripheral clock of 75MHz, not enough fast for the DMA to transfer all the pixels of a scanline.

Thanks to misaz for helping with suggestions, especially for saving me a lot of soldering work for the 8-bit RGB port assigned to pins P2_0..7

What to say, I am very impressed by this MCU so far, and this successful step gives me a lot of enthusiasm and energy to move on in this project!

  • Sign in to reply

Top Comments

  • dougw
    dougw over 3 years ago in reply to Digimorf +1
    Great progress - impressive.
  • baldengineer
    baldengineer over 3 years ago in reply to Digimorf +1
    I prefer the former because it makes code more compact. But, it is more important to be consistent. I can adapt even when people use the wrong one.
  • dougw
    dougw over 3 years ago in reply to Digimorf

    Great progress - impressive.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago in reply to Digimorf

    I like the latter, but I am not a programmer......Relaxed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Digimorf
    Digimorf over 3 years ago

    Before moving on, I think it's better to beautify a bit the source code. Since I am still into this I will add comments so that this project at the end will be useful to users.

    1M$ question: What do you like most...

    if (something) {

    Or

    if (something)
    {

    Sweat smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<