At The Core Design Challenge
  • Challenges & Projects
  • Design Challenges
  • At The Core Design Challenge
  • More
  • Cancel
At The Core Design Challenge
Forum PSoC6S4 Vector table of the cm0+ in flash.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join At The Core Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 50 subscribers
  • Views 1462 views
  • Users 0 members are here
Related

PSoC6S4 Vector table of the cm0+ in flash.

Digimorf
Digimorf over 3 years ago

Has anyone tried to leave the vector table of the cm0+ in flash and configure an interrupt?

By default it is copied into SRAM. No doubt about it's faster to fetch the addresses of the IRQ handlers at runtime, but I need to check if the access to SRAM by both cores causes jitter in fetching the IRQ handlers. 

I tried to customize the startup file of the cm0+, but something must be inherited by the PDL such as the ram_table_address. 

Thanks 

  • Sign in to reply
  • Cancel

Top Replies

  • misaz
    misaz over 3 years ago +3
    Yes. SRAM access on different cores (or caused by DMA or otherm AHB masters) can influence interrupt latancy. I tested it on different PSoC for evaluating Profiler peripheral (which is unluckily not avalaible…
  • ljking
    ljking over 3 years ago +2
    There are actually several independent SRAM blocks and controllers inside the part (it is not just a single large SRAM). if you put the Video buffer in a different SRAM block from the vectors I suspect…
  • ljking
    ljking over 3 years ago in reply to Digimorf +1
    That was my thinking also, but I don't want to assume that is the correct answer. For an example, a single controller could control two 32k blocks. Until I get to see the answer formally documented, I…
Parents
  • Digimorf
    0 Digimorf over 3 years ago

    Thanks for the support. I think I will try first to leave vectors in the flash. I can't understand why this is not the standard configuration.

    Anyway the PDL documentation shows how to configure an interrupt to use the vector table in the flash, but that doesn't work for me. Probably I am missing something.

    https://infineon.github.io/mtb-pdl-cat1/pdl_api_reference_manual/html/group__group__sysint.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Digimorf
    0 Digimorf over 3 years ago

    Thanks for the support. I think I will try first to leave vectors in the flash. I can't understand why this is not the standard configuration.

    Anyway the PDL documentation shows how to configure an interrupt to use the vector table in the flash, but that doesn't work for me. Probably I am missing something.

    https://infineon.github.io/mtb-pdl-cat1/pdl_api_reference_manual/html/group__group__sysint.html