BeagleBone Black Radio Challenge
  • Challenges & Projects
  • Design Challenges
  • BeagleBone Black Radio Challenge
  • More
  • Cancel
BeagleBone Black Radio Challenge
Forum I2S input - Beaglebone Black
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 1 subscriber
  • Views 812 views
  • Users 0 members are here
Related

I2S input - Beaglebone Black

e14 Contributor
e14 Contributor over 10 years ago

Hello guys,

I am new with linux and the beaglebone. I have a project that will use the same processor of the beaglebone black, so I`ve decided to use this board to build a prototype. The kernel from my beaglebone black is 3.8.13-bone47 and I am using a BlueGiga board to send I2S (using 3 wires) audio to the beaglebone. My goal is to make the beaglebone receive I2S (maybe using arecord - alsa), compress the audio using opus enconder and send it to a web browser. At this moment, I am able to receive a audio from a web radio in wav format (I need to change that to audio receive from BlueGiga), encode the audio to opus format and send to a web browser (I create a server that runs inside the beaglebone). However, I am having a lot of difficulties to turn the beaglebone able to receive I2S. I am trying to use the device tree overlay but without success. I disable the HDMI in the Uenv.txt and I am able to achieve the new overlay (I check the slots and the pins modes). However, I can`t use arecord because alsa do not recognize the audio coming from the bluegiga using wires. My dts file is:

/dts-v1/;

/plugin/;

/ {

        compatible = "ti,beaglebone", "ti,beaglebone-black";

        part-number = "BBB-AUDIO-01";

        version = "00A0", "A0";

        exclusive-use =

                "P9.27",                /* mcasp0_fsr */

                "P9.30",                /* mcasp0_axr0 */

                "P8.35",                /* mcasp0_aclkr */

                "mcasp0";

        /* the offsets come from the bone.js file from adafruit */

        fragment@0 {

                target = <&am33xx_pinmux>;

                __overlay__ {

                        tdm_pins: tdm_pins {

                                pinctrl-single,pins = <

                                        0x1a4 0x20      /* P9.27 INPUT/MODE 0*/

                                        0x198 0x20      /* P9.30 */

                                        0x0d0 0x23      /* P8.35 */

                                >;

                        };

                };

        };

        fragment@1 {

                target = <&mcasp0>;

                __overlay__ {

                        compatible = "ti,omap2-mcasp-audio";

                        pinctrl-names = "default";

                        pinctrl-0 = <&tdm_pins>;

                        status = "okay";

                        op-mode = <0>;          /* MCASP_IIS_MODE */

                        tdm-slots = <2>;

                        num-serializer = <16>;

                        serial-dir = <          /* 0: inactive, 1:TX, 2:RX */

                         2 0 0 0

                         0 0 0 0

                         0 0 0 0

                         0 0 0 0

                        >;

                        tx-num-evt = <1>;

                        rv-num-evt = <1>;

                };

        };

fragment@2 {

        target = <&ocp>;

        __overlay__ {

            sound {

                compatible = "ti,da830-evm-audio";

                ti,model = "DA830 EVM";

                ti,audio-codec = <&tlv320aic3x>;

                ti,mcasp-controller = <&mcasp0>;

                ti,codec-clock-rate = <12000000>;

                ti,audio-routing =

                    "LINE1L", "Line In",

                    "LINE1R", "Line In";

            };

        };

    };

};

 

Thank guys for the help.

 

ps: I can see the I2S with a scope after the BLUEGIGA.