Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog Bluetooth Unleashed : AAPSAD #4 : The Rise of the Fallen!
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
  • Author Author: sakthi.1260
  • Date Created: 26 May 2018 6:02 PM Date Created
  • Views 536 views
  • Likes 6 likes
  • Comments 2 comments
Related
Recommended

Bluetooth Unleashed : AAPSAD #4 : The Rise of the Fallen!

sakthi.1260
sakthi.1260
26 May 2018

Hello guys,

Before I start I need to thank our community members.

image

That was a lot of thoughts and tips tried a few and realized the issue was the model itself, that was a huge data set to be processed and matched so we decided to do something else.

So before starting with the that, there was sweet suprise, thanks todanzima.

The kits have arrived....

imageimage

It was the Rpi 7" Display, Camera Module and Arduino.

Although I'm having some issues with Camera Module v2.1, working on it, for now we are using Haar Cascade to detect smile anything other than a smile will be sending data over Bluetooth, we are now using a very small model and Rpi runs smooth without no lag. A code snippet of the while block here.

    gray = cv2.cvtColor(frame, cv2.COLOR_BGR2GRAY)

    faces = faceCascade.detectMultiScale(
        gray,
        scaleFactor= sF,
        minNeighbors=8,
        minSize=(55, 55),
        flags=cv2.CASCADE_SCALE_IMAGE
    )
   
    for (x, y, w, h) in faces:
        roi_gray = gray[y:y+h, x:x+w]
        roi_color = frame[y:y+h, x:x+w]
        smile = smileCascade.detectMultiScale(
         roi_gray,
         scaleFactor= 1.7,
         minNeighbors=22,
         minSize=(25, 25),
         flags=cv2.CASCADE_SCALE_IMAGE
        )
        
        
        if len(smile):
            print("All Good")
        else:
            print("Send data over BT")
        
 

I've removed the feed window. and the output was satisfactory.

imageimage

I'm trying to bring much more detailing on the mood identification part. Code will be available in our github

Whats next? Its time to unleash the power of Bluetooth and complete the secondary unit.

 

Cheers and Thanks to everyone! image

  • Sign in to reply

Top Comments

  • aspork42
    aspork42 over 8 years ago +1
    Ahhh! So cool! I love it! Was just readin about Haar Cascades the other day for a project at work with OpenCV.
Parents
  • aspork42
    aspork42 over 8 years ago

    Ahhh! So cool! I love it! Was just readin about Haar Cascades the other day for a project at work with OpenCV.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 8 years ago

    Ahhh! So cool! I love it! Was just readin about Haar Cascades the other day for a project at work with OpenCV.