Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog Bluetooth Unleashed : AAPSAD #7 : Moisture Matters
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
  • Author Author: sakthi.1260
  • Date Created: 16 Jun 2018 3:56 PM Date Created
  • Views 1008 views
  • Likes 6 likes
  • Comments 4 comments
  • arduio
Related
Recommended

Bluetooth Unleashed : AAPSAD #7 : Moisture Matters

sakthi.1260
sakthi.1260
16 Jun 2018

Hello guys,

 

Most of the work with Rpi is over, the next part is to prepare the control unit.

This week we gonna break open a USB humidifier and try to control it using the arduino.

Does humidity affects emotions?

Even I had the question till this was started, and after little search found a lot of interesting facts over this, so the conclusion they do play a vital role over the mood, higher humidity makes you lazy, that's something you might want when you are angry.

imageimage

 

I opened it, there is small control board and a pair of wire connected to the piezo. I removed the board to inspect and found the IC marking to be erased.

image

Since its was ON OFF controller decided to do it in another way, permanently shorted the humidifier switch to ground and attached a NPN to the power supply

image

 

and as final touch sprayed a layer of conformal coating ()

image

 

The Bluetooth is yet to be unleashes so I'm gonna send data over the arduino serial monitor

Its already humid weather here, so the only test case possible was 'anger' (did a mistake over the case in the snippet), but still it works. I don't want the humidifier to be turned ON based on the Relative humidity so hooked up a DHT11 to the arduino.

 

The code

#include <TroykaDHT.h>
DHT dht(10, DHT11);
void setup()
{
  pinMode(9, OUTPUT);
  Serial.begin(9600);
  dht.begin();
}

void loop()
{ digitalWrite(9,LOW);
  dht.read();
  delay(1000);
  int hum = dht.getHumidity();
  char c = Serial.read();
  switch(c)
  {
  case 'a': //anger
  if (hum<80)
  Serial.println(hum);
  digitalWrite(9,HIGH);
  delay(10000);
  break;
  case 's': //sad
  if (hum<60)
  Serial.println(hum);
  digitalWrite(9,HIGH); 
  delay(10000);
  break;
}
}

imageimage

 

I started to visualize the final outcome, hoping for a great end.

Cheers,

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +3
    Nice update. I have found that humidity changes can affect my migraine headaches. It is amazing how little things can affect the human body. DAB
  • genebren
    genebren over 8 years ago +2
    Nice update on your design challenge project. It was not too clear to me the relationship between humidity and mood, does an increase in humidity improve your mood? I am only wondering as here in Texas…
  • sakthi.1260
    sakthi.1260 over 8 years ago in reply to genebren +2
    Hi Gene, Thanks. The humidity indirectly affects psychology, a higher humidity means a less perspiration which in turns give a lethargic feel if you are angry a humidity raise should somewhat bring your…
Parents
  • aspork42
    aspork42 over 8 years ago

    Cool update!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 8 years ago

    Cool update!