Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog [Bluetooth Unleashed] Felo'melorn #2: Redbear Blend
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
  • Author Author: fvan
  • Date Created: 12 May 2018 12:26 PM Date Created
  • Views 1104 views
  • Likes 13 likes
  • Comments 8 comments
  • felomelorn
  • fvan
  • arduino_projects
  • ardexpert
  • bluetooth unleashed
  • world of warcraft
  • redbear
Related
Recommended

[Bluetooth Unleashed] Felo'melorn #2: Redbear Blend

fvan
fvan
12 May 2018

My hero board has arrived!

image

 

  • Redbear Blend v1
  • Redbear Blend v2
  • Redbear Blend ... Retired
  • Alternatives
  • Felo'fact

 

Redbear Blend v1

 

The Redbear Blend is an Arduino compatible board "blending" it with BLE 4.0 functionality, hence the name "Blend". It is basically an Arduino Leonardo powered by an Atmel ATmega32U4, combined with a Nordic nRF8001 BLE chip.

image

Source: redbear

 

It has the classic Arduino header layout and reset button, but also has a switch to toggle between 5V and 3.3V I/O and a whole bunch of jumpers. I haven't been able to find what these jumpers are for, except switch certain I/O from REQN to RDYN, making a connection to the BLE chip. Probably wisest to no touch and leave as is, for the moment.

 

There is also a micro version of the board, for more compact applications, where size is relevant.

 

This is the version of the board I received for this challenge, but there is a successor ...

 

Redbear Blend v2

 

The Blend v2 has an upgraded MCU and BLE chip. It is powered by a Cortex-M3 MCU and the newer nRF52832 BLE 5.0 chip.

image

Source: seeedstudio

 

It adds two Grove connectors to the board, but no longer has the configurable 5V/3.3V operation switch (now 3.3V only). Everything still packaged in the classic Arduino form factor.

 

But ...

 

Redbear Blend ... Retired

 

And this is where the importance of research comes in. I applied quite late to the challenge, and intuitively went for something that wasn't completely new to me. Not being too familiar with bluetooth, I opted for familiar hardware and coding technique.

 

I saw two options: pick the Raspberry Pi or go with Arduino.

 

Because of the nature of the project, Arduino seemed like the way to go: low power, small form factor, easier hardware control. So, at the time, I picked the Redbear Blend.

 

It was only later, when I was looking at potentially purchasing more, or even smaller variants like the Redbear Blend Micro, that I discovered that range of boards had been retired. This means that I'm now building a project with obsolete hardware, which is not ideal for anyone trying to reproduce this projects or some elements from it.

 

From what I understood, Redbear has recently been acquired by Particle, which you may know from their original Spark Core or more recent Particle Photon and Electron, meaning the company's focus is shifting and there is no longer room many dev boards.

 

Redbear has published an announcement on their website: https://redbear.cc/particle

 

image

 

In case of the Blend, the most relevant line, is the following:

All other products will be discontinued once the existing stocks are cleared and supported till end of September 2018

 

Ouch ... image

 

Alternatives

 

Though it's not the best feeling to know I'll be working with obsolete hardware from the start, it's comforting to know there are alternatives out there, like Adafruit's nRF8001 breakout board for example.

 

The fact that this device is Arduino compatible, also makes the code easily portable to another type of Arduino, apart from the Bluetooth part, depending on the module used.

 

Could perhaps be an interesting thing to test near the end of the project: port the code to a non-obsolete hardware combination and see if everything still works.

 

Felo'fact

 

Let's finish this post with another fact about Felo'melorn:

Elven blades grow stronger with each reforging, but only in the hands of the finest craftsmen.

 

 

See you soon, as I get started with the Redbear and blink an LED!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +4
    fvan That is a shame, and makes little sense if the hardware is already developed. I tried to get one of these boards when the challenge first appeared, but for some reason they are a restricted item and…
  • fvan
    fvan over 8 years ago in reply to mcb1 +4
    I'm wondering if there is any coincidence in these Challenges and products being discontinued ... reminds me of the Intel Edison It indeed looks like a way to get rid of leftover stock. Don't get me wrong…
  • e14phil
    e14phil over 8 years ago in reply to fvan +4
    Hey Guys, that's a shame! To clarify, this design challenge is not a way of clearing stock and is a coincidence, for example, if we wanted to clear stock, we would have to ship out way more than 2 boards…
Parents
  • mcb1
    mcb1 over 8 years ago

    fvan

    That is a shame, and makes little sense if the hardware is already developed.

     

    I tried to get one of these boards when the challenge first appeared, but for some reason they are a restricted item and needed a whole load of paperwork, hence we canceled the order.

    Seems it was the right choice, so I'm glad you've brought this to our attention.

     

    I'm wondering if there is any coincidence in these Challenges and products being discontinued ... reminds me of the Intel Edison image

     

    Perhaps you can still do the development to meet the T&C's, and then consider it dead.

     

     

    Cheers

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 8 years ago in reply to mcb1

     

    I'm wondering if there is any coincidence in these Challenges and products being discontinued ... reminds me of the Intel Edison

    It indeed looks like a way to get rid of leftover stock. Don't get me wrong, nothing wrong with that, but a disclaimer/warning would be useful if it is indeed the case.

     

    Perhaps e14phil could clarify?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 8 years ago in reply to fvan

    Hey Guys, that's a shame!

     

    To clarify, this design challenge is not a way of clearing stock and is a coincidence, for example, if we wanted to clear stock, we would have to ship out way more than 2 boards and from warehouses all over the world. The Redbear and the Pycom where my choices as I thought they were really cool bluetooth concept boards. The other heros on the list made sense and these were my curveballs!

     

    But interestingly related, the element14 community team also has a stock cupboard with lots of older board samples that we are currently cataloging to give away for free in the near future.

     

    Edit:

    Addendum - The edison line being discontinued was a real shock to us because Intel were really promoting it until they decided I was not working for them. It was a real shame as they were very powerful boards!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 8 years ago in reply to e14phil

    Just bad luck then image

    But as I stated, there are alternatives, and since it is Arduino compatible, there shouldn't be much impact when swapping out the hardware.
    I just hope things like the Bluetooth app they have for iOS for example remains supported ...

     

    Thanks for the clarification, Phil!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to e14phil

    I have to agree with your thoughts on Intel Edison.

     

     

    IMO It did have some issues ...

    A very small powerful board, but sadly required another board even to power it.

    The 1.8v I/O also wasn't the most favourable in a maker world, but the processor and interface was worthwhile.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to e14phil

    Hi Phil!

    At the time, I got the feeling maybe it was a surprise even within some departments in Intel, it was so very quick to occur. I'd spent some time designing an Edison board - nothing to do with Holland & Barrett, that's just there for size comparison image

     

    It was awesome how tiny that Edison module really was..

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago in reply to e14phil

    Hi Phil!

    At the time, I got the feeling maybe it was a surprise even within some departments in Intel, it was so very quick to occur. I'd spent some time designing an Edison board - nothing to do with Holland & Barrett, that's just there for size comparison image

     

    It was awesome how tiny that Edison module really was..

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14phil
    e14phil over 8 years ago in reply to shabaz

    Thats pretty cool!

    • Cancel
    • Vote Up +3 Vote Down