Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog [Bluetooth Unleashed] Felo'melorn #5: Mod
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
  • Author Author: fvan
  • Date Created: 7 Jul 2018 6:53 PM Date Created
  • Views 1244 views
  • Likes 9 likes
  • Comments 5 comments
  • felomelorn
  • fvan
  • bluetooth unleashed
  • world of warcraft
  • redbear
Related
Recommended

[Bluetooth Unleashed] Felo'melorn #5: Mod

fvan
fvan
7 Jul 2018

In order to enhance the fire element of Felo'melorn, I wanted to add smoke in addition to the lights. Searching the vast world wide web, I came across a mod(ification) for electronic cigarettes for cosplay purposes. Just what I needed for this project ...

 

  • Parts
  • Assembly
  • Felo'fact
  • Sources

 

Parts

 

Being totally unfamiliar with e-cigarettes, I had to do some research on which parts to buy. I've linked the sources for this mod at the end of this post.

 

The core component is obviously the e-cigarette. I found a cheap one at about 5EUR on eBay, a "Kangertech T3S Clearomizer".

image

 

The next part is very specific and only compatible with specific e-cig models, which narrowed down the options when selecting the e-cig, an "eGo Unsealed Battery Mod Connector".

This part will allow me to use my own power supply for the e-cig or even replace the e-cig without hassle.

image

 

Because the e-cig will be embedded in the prop, there needs to be a mechanism to have the smoke come out of the e-cig, which achieved by using a small air pump.

image

 

Normally, someone would suck air through it, releasing the smoke. In this mod, a small air pump is used to blow the smoke out of the device. Using some flexible tubing, the air pump can be connected to the e-cig, forcing the air though it.

image

 

That's the theory at least. Next step is to get all of this assembled.

 

Assembly

 

The trickiest part of this build was to solder the wires inside the connector. The center ring is isolated from the rest of the connector via a rubber seal. Soldering the red wire, without blocking the ventilation hole with solder, was a real pain ...

After various attempts and the assistance of my desoldering pump, I finally managed to get the red wire in place without blocking the ventilation hole. Using my multimeter, I confirmed there was no short between the red and black wires.

image

 

Once the wires were soldered on, the flexible tube was put over the ventilation hole. That meant that a part of the red wire had to be inside the tube. The red wire exits the tube about halfway, trough a little hole I made.

To avoid putting too much strain on the wires and the tube, I filled the connector with hot glue.

image

 

Finally, the e-cig was screwed on the connector, and the airpump hooked up to the flexible tube.

image

 

That's the smoke machine done. Next, I'll have to create a circuit to control the pump via a PWM signal to control intensity, and find the best way to power the e-cig.

 

Felo'fact

 

Felo'melorn is rumored to be located in Icecrown Citadel, the Lich King's fortress.

image

Source: https://wow.gamepedia.com/Icecrown_Citadel

 

Sources

 

Sources I used to find information on type of e-cig, modifications to make, etc ...:

  • How to make a compact smoke machine for cosplay (for under $30!) – Cosplay by Henchwench
  • DIY Smoke Machine From Ecig Clearomiser
  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 8 years ago +3
    I'm looking forward to seeing this in action. Had a chat with my wife who's been vaping for a few years now. You might find a fruit rather than tobacco juice is less likely to gum up the pipes. Also look…
  • mcb1
    mcb1 over 8 years ago +2
    Nice trick. I've played with smoke machines in the past which pump a fluid through a large heated block. The biggest issue was blocking up, as everyone had cheaper fluid, but it usually came at a cost…
  • fvan
    fvan over 8 years ago in reply to genebren +1
    Thanks Gene! This is my first time using something like this. Though I assume it's probably quite safe, I'll still be careful and keep an eye on it. Perhaps I should strap a temperature sensor to it and…
Parents
  • genebren
    genebren over 8 years ago

    Nice update on your design challenge product.  Normally I would have nothing to do with e-cigs, but this is a creative approach.  I remember the good old days when out old electric train would puff around the Christmas tree, with smoke and lights.  If I remember correctly it was smoldering oil with a hot wire.  I wonder how many fires that caused?

     

    Good luck on bringing all the pieces together.

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Nice update on your design challenge product.  Normally I would have nothing to do with e-cigs, but this is a creative approach.  I remember the good old days when out old electric train would puff around the Christmas tree, with smoke and lights.  If I remember correctly it was smoldering oil with a hot wire.  I wonder how many fires that caused?

     

    Good luck on bringing all the pieces together.

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fvan
    fvan over 8 years ago in reply to genebren

    Thanks Gene!

    This is my first time using something like this. Though I assume it's probably quite safe, I'll still be careful and keep an eye on it. Perhaps I should strap a temperature sensor to it and cut the power when beyond a certain threshold ...