Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog BTU - Project LOKI.10 - Success!
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
  • Author Author: jkutzsch
  • Date Created: 18 Jul 2018 4:52 AM Date Created
  • Views 1160 views
  • Likes 4 likes
  • Comments 1 comment
  • raspberry pi 3 b+
  • kali
  • bluetooth unleashed design challenge
Related
Recommended

BTU - Project LOKI.10 - Success!

jkutzsch
jkutzsch
18 Jul 2018

Welcome back to my 10th blog on Project Loki!

 

I do have a request for you the reader.  If you happen to know of a Linux bluetooth tool that is not in the list I have came across and believe it would be an interesting one to test on the Raspberry Pi Kali setup.  Please let me know.  It seems the core tools are over 10 years old and I would think something new must be out there in the Linux world!

 

Now back to Loki:

 

image

So I am still using the StickyPi menu system even though I have not added any tools specifically into the menu system.  I do want to pursue the potential but I wanted to be sure Project Loki worked as a Bluetooth Scanner prior to getting stuck on a menu.  :-)

 

So at this point I just touch the Terminal option.

 

image

 

I apologize about the quality of pictures.  The Touchscreen is being very glaring tonight and as such the camera is having serious issues getting it focused.

 

image

 

First off let's use the hciconfig command to verify I have bluetooth recognized and running.

 

image

 

As you can see it recognizes my internal bluetooth and it is showing as UP RUNNING. 

Good to Go!

 

image

 

Lets use the command hcitool scan to see what can be discovered before going over to our new tools.

 

image

 

Here we can see it discovers 2 devices.  One is a tablet and one is a phone.  Showing the Mac addresses and names for each.

 

image

 

Now let's see what our new tools can do!  sudo btscanner

 

Just as a reminder, last blog we went over Btscanner:  btscanner- "btscanner is a tool designed specifically to extract as much information as possible from a Bluetooth device without the requirement to pair. A detailed information screen extracts HCI and SDP information, and maintains an open connection to monitor the RSSI and link quality. btscanner is based on the BlueZ Bluetooth stack, which is included with recent Linux kernels, and the BlueZ toolset. btscanner also contains a complete listing of the IEEE OUI numbers and class lookup tables. Using the information gathered from these sources it is possible to make educated guesses as to the host device type.btscanner is a tool designed specifically to extract as much information as possible from a Bluetooth device without the requirement to pair. A detailed information screen extracts HCI and SDP information, and maintains an open connection to monitor the RSSI and link quality. btscanner is based on the BlueZ Bluetooth stack, which is included with recent Linux kernels, and the BlueZ toolset. btscanner also contains a complete listing of the IEEE OUI numbers and class lookup tables. Using the information gathered from these sources it is possible to make educated guesses as to the host device type."

 

image

 

enter password...

 

image

 

Here we have the btscanner "gui".  :-)

 

image

 

A better view of the options.

h=help

i=inquiry scan

b=brute force scan

a=abort scan

s=save summary

o=select sort

enter=select

q=quit

 

image

 

So let's hit i for inquiry scan.

 

image

 

Here at the bottom it shows you it has found 2 devices.  Or at least the mac addresses seen.

 

image

 

Another full screen view showing bottom and information displayed at top for the 2 devices found.

 

image

 

Here is a zoomed look at the top.  You can see a little more information up here including date/time.

 

image

 

By using the arrow key you can toggle between the two.

 

image

 

Before we get into why we want to toggle between the devices, lets type A to abort scan.

 

image

 

Now let's arrow back down to the NS-15T8LTE and hit enter to select.

 

image

 

Here you are provided with a variety of more detailed information including that it is a Computer/Handheld PC-PDA and that it has Networking, Capturing, and Object Transfer as services.

 

Plenty of more details here so if you were to see an interesting item you had scanned this allows you to look deeper.

 

image

 

Okay, let's take a look at a couple of more tools we downloaded.  Starting with bluelog.

 

From our last blog:

bluelog- "Bluelog is a Linux Bluetooth scanner with optional daemon mode and web front-end, designed for site surveys and traffic monitoring. It’s intended to be run for long periods of time in a static location to determine how many discoverable Bluetooth devices there are in the area."

 

We are just using it as a long term scanner with logging option right now.

 

image

 

As you can see it is scanning.  We can leave this for a length of time unattended and come back later to see what it has found.

 

image

 

Okay, Ctrl-C, our time is done.  Since I know I won't find anything more then what it has seen.  :-)

 

image

 

A quick ls to display the directory.  Here we see the log file for today.

 

image

 

Using handy dandy nano, we nano bluelog-2018-07-18*

 

image

 

There we go, it has found the two mac addresses.  No names, just the addresses.  But it is logged.

 

image

 

After exiting from nano I wanted to check on Red Fang.  The bruteforce scanner.

So type in sudo fang

 

image

 

enter ye olde password

 

image

 

And you can see it start the slow and steady scan of incrementing addresses.  This is Sssssllllloooowwww.

 

But I can see where it would be interesting if left in an area for a long time.

 

So some useful tools to monitor the bluetooth networks and to even leave in place and brute force devices that are "hidden".

 

I will continue to look into getting the menu system working but I feel good that this is a working bluetooth security platform and expect to be able to finetune and enjoy it more.

 

As I mentioned before, if you know of other useful bluetooth linux tools please share over to me and I will see how the work with Project Loki.

 

Thank you!

 

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +1
    Nice update to your design challenge project. It is good to see that you were able to get your tools up and running and doing something useful. Good job, keep up the good work! Gene
Parents
  • genebren
    genebren over 8 years ago

    Nice update to your design challenge project.  It is good to see that you were able to get your tools up and running and doing something useful.

    Good job, keep up the good work!

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Nice update to your design challenge project.  It is good to see that you were able to get your tools up and running and doing something useful.

    Good job, keep up the good work!

    Gene