Connected Cloud Challenge
  • Challenges & Projects
  • Design Challenges
  • Connected Cloud Challenge
  • More
  • Cancel
Connected Cloud Challenge
Blog #5 GPIO read and write
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
  • Author Author: wanfp97
  • Date Created: 7 May 2020 8:37 AM Date Created
  • Views 2014 views
  • Likes 2 likes
  • Comments 0 comments
  • psoc6
Related
Recommended

#5 GPIO read and write

wanfp97
wanfp97
7 May 2020

The next thing I would like to do is to get familiarize with the GPIO as it is one of the easiest way to read and write a single bit of data.

 

BOM: PSoC6 WiFi-BT Pioneer Kit, a servo motor, a green LED, a red LED, 2 potentiometer with resistance adjusted to around 300 ohm, a push button, and some jumper wires.

 

image

I start by using the application I have create during the last blog post. I leave the tcpwm1 and the clock divider untouched.

 

image

Enable a pin and named it button. Set its Drive Mode to Resistive Pull-Down. input buffer on. Resistive Pull-Down means that the pin will discharge to logic low when the pin is not connected to a logic high source. This can eliminate the undefined state when the pin is not connected. Meanwhile, input buffer on allow the pin to work as an input pin.

 

image

I have also enabled another 2 pins and named them green and red, which they will be connected to a green and a red LED later on. I chose Strong Drive. input buffer off which will let the pin transition faster and act as an output pin.

 

I then tried the following code on the PSoC6:

#include "cy_pdl.h"
#include "cycfg.h"

int main(void)
{
    /* Initialize the device and board peripherals */
    __enable_irq();
    init_cycfg_all();
 Cy_TCPWM_PWM_Init(tcpwm1_HW, tcpwm1_NUM, &tcpwm1_config); // initialize tcpwm
    Cy_TCPWM_PWM_Enable(tcpwm1_HW, tcpwm1_NUM); // enable tcpwm1
    Cy_TCPWM_TriggerStart(tcpwm1_HW, tcpwm1_MASK); //Start the tcpwm1 (initially 0.5ms high per cycle) (servo positioned at right)
    for (;;)
    {
     if(1UL == Cy_GPIO_Read(button_PORT, button_NUM))
     {
      Cy_GPIO_Write(green_PORT, green_NUM, 1UL); // green LED on
      Cy_GPIO_Write(red_PORT, red_NUM, 0UL); // red LED off
      Cy_TCPWM_TriggerCaptureOrSwap(tcpwm1_HW, 1UL); // tcpwm1 swap to 2.5ms(left) high per cycle
     }
     else
     {
      Cy_GPIO_Write(green_PORT, green_NUM, 0UL); // green LED off
      Cy_GPIO_Write(red_PORT, red_NUM, 1UL); // red LED on
      Cy_TCPWM_TriggerCaptureOrSwap(tcpwm1_HW, 1UL); // tcpwm1 swap to 0.5ms(right) high per cycle
     }
    }
}

Notice that the Cy_GPIO_Read and Cy_GPIO_Write function can be found on PSoC6 PDL API Reference page that I have mentioned on previous blog.

 

Initially, I have meant to program the code to have the following function:

image

Block diagram of servo and LED controller.

 

The LEDs work find just like I want them to, however, the servo is behaving weird.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I will try to troubleshoot it and update its' solution on my future blog post.