Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Final Week...
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
  • Author Author: roborob1266
  • Date Created: 27 Aug 2018 3:25 AM Date Created
  • Views 2544 views
  • Likes 3 likes
  • Comments 4 comments
  • adxl335eb
  • adafruit vs1053 mp3 player
  • 5" touch screen
  • design for a cause - design challenge
  • uno
  • mkr1000
  • adafruit ra8875
  • ultrasonic proximity sensor
Related
Recommended

Final Week...

roborob1266
roborob1266
27 Aug 2018

Hello all

I was able to get the RA8875 and the VS1053 to work with the Arduino UNO.

I also connected the HC-SR04 Ultrasonic Sensor and the ADXL335EB board to the MKR1000 to account for movement as well as distance from the MKR1000 itself.

I will be connecting both of these devices via the SDA/SCL connections for communications.

 

I took a photo just now of what is going on so far!

As you can see there are the touch screen buttons and I am scratching my head on how to get the image file off the SD card from the VS1053 to the TFT touch screen via the RA8875.

I have looked at code to do this but it doesn't work with my RA8875.

Also I need to just have the background be only one image file (a BMP file I already have) on the SD card ready to go.

Then when the "button" is pressed, it will play the audio file associated to that button. I tested the audio and it works and the blue buttons register X/Y touch coordinates.

 

I then need to get code to have the touch area to be over each part of the image that shows below on the display (it will replace the blue buttons at this time).

The border will be around each image (5 of them) that is on the BMP file similar to the buttons below.

Any assistance is appreciated.

image

  • Sign in to reply

Top Comments

  • aspork42
    aspork42 over 8 years ago +3
    Glad you were able to get them all going off the Uno. I've never used either of the other two modules, so not really sure where to start. Perhaps you could start by just using text instead of trying to…
  • roborob1266
    roborob1266 over 8 years ago in reply to shabaz +2
    Hello Shabaz I just need one image to go to the display, that's all. The rest of it is having a place holder over each of the images on the display so when someone touches in that area, it will trigger…
  • shabaz
    shabaz over 8 years ago +1
    Hi Rob, Unless there's an API that will accept the BMP file format (i.e. check the Adafruit library for the RA8875 board - but I'm fairly sure there isn't, I briefly checked the API but I may have missed…
Parents
  • aspork42
    aspork42 over 8 years ago

    Glad you were able to get them all going off the Uno. I've never used either of the other two modules, so not really sure where to start. Perhaps you could start by just using text instead of trying to get bitmaps to load. Try to get the most basic functionality working first before making it pretty image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 8 years ago

    Glad you were able to get them all going off the Uno. I've never used either of the other two modules, so not really sure where to start. Perhaps you could start by just using text instead of trying to get bitmaps to load. Try to get the most basic functionality working first before making it pretty image

    • Cancel
    • Vote Up +3 Vote Down