Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Week 5 - Getting Down To Business
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
  • Author Author: kyle90
  • Date Created: 15 Aug 2018 3:34 PM Date Created
  • Views 1100 views
  • Likes 5 likes
  • Comments 3 comments
Related
Recommended

Week 5 - Getting Down To Business

kyle90
kyle90
15 Aug 2018

With Dan returned from his vacation, we had a meeting to integrate all the code we had written so far, work on the circuitry, and begin the design for the case that will house the device when it is done. The code went together easily enough, though there were some bugs we had to work out. The first was that the Arduino audio library seems to interfere with the tone() function which will send a simple square wave to a piezo buzzer. We decided that if we were going to have full audio output anyway, we could simply record an alert tone and play it back through a speaker, rather than using a buzzer. This means we will need to include a small audio amplifier, which is easy to accomplish with an op-amp like the LM386. For now we tested it using speakers which have their own internal amplifiers, and the audio output works as expected.

image

 

We also hooked up the accelerometer and started getting some testing data from it. Once we have the case built we will able to record what it actually looks like when someone falls, and this will give us a better idea of what we need to be looking for in the data. For now it assumes the acceleration is only along one axis (so the three axes are combined into one), but of course if it is moving laterally while falling, which will likely be the case, this won't be true. Anyway, we were pleased at its sensitivity and that the calculations done on the data would indeed sort of give a position and velocity measurement.

image

 

We will be meeting again on Monday, but in the meantime our next steps are:

 

Dan: measure all components, design a housing that they will fit inside, 3D print the housing

Kyle: refine the accelerometer calculations, build the audio amplifier

 

We're making progress!

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago +2
    A very interesting project and a good start. It is always more fun to build something if you have someone to collaborate with. John
  • genebren
    genebren over 8 years ago +1
    Nice update on your design challenge project. Interesting chart of a fall. Are the oscillations due to a bounce at the end of a fall? Good luck on your next steps. Gene
  • kyle90
    kyle90 over 8 years ago in reply to genebren +1
    Thanks, the oscillations are because the accelerometer was just hanging from wires at this point rather than attached to anything solid.
Parents
  • genebren
    genebren over 8 years ago

    Nice update on your design challenge project. Interesting chart of a fall.  Are the oscillations due to a bounce at the end of a fall?

    Good luck on your next steps.

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kyle90
    kyle90 over 8 years ago in reply to genebren

    Thanks, the oscillations are because the accelerometer was just hanging from wires at this point rather than attached to anything solid.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kyle90
    kyle90 over 8 years ago in reply to genebren

    Thanks, the oscillations are because the accelerometer was just hanging from wires at this point rather than attached to anything solid.