Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Forum Enocean Press Switch Circuit
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 3 subscribers
  • Views 1831 views
  • Users 0 members are here
  • push-to-select
  • push button switches
Related

Enocean Press Switch Circuit

deepak.domingo@ucdconnect.ie
deepak.domingo@ucdconnect.ie over 8 years ago

Hi,

 

I want to build a simple sensing circuit, where the transmitter sends a signal to a reciever on the press of a piezo-electric switch and the reciever threin drives a 5VDC LED circuit.

 

Could anyone suggest the optimal part numbers for the enocean sensors?

 

Many Thanks,

 

Deepak

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +2
    Greetings, The heart of the Enocean switch is http://www.newark.com/enocean/ptm215ze/push-button-transmitter-mod-2/dp/18AC0118 this will transmit the switch activations. And the transceiver module that…
  • deepak.domingo@ucdconnect.ie
    deepak.domingo@ucdconnect.ie over 8 years ago in reply to genebren +1
    Hi, My requirement is to just power two 5V DC LED circuits. Range is not a problem as a radius of 2 meters is sufficient. The design I am looking at is enocean sensor (piezoelectric) push button to reciever…
  • genebren
    genebren over 8 years ago in reply to deepak.domingo@ucdconnect.ie +1
    Deepak, The parts above could be used to do what you are referring to. You need the piezoelectric switch (with transmitter), a receiver and then your arduino to light your LEDs. This is not really a low…
Parents
  • genebren
    genebren over 8 years ago

    Greetings,

     

    The heart of the Enocean switch is http://www.newark.com/enocean/ptm215ze/push-button-transmitter-mod-2/dp/18AC0118  this will transmit the switch activations.

    And the transceiver module that can receive this signal is http://www.newark.com/enocean/tcm515z/wireless-transceiver-mod-2-4ghz/dp/18AC0622

     

    There is a pretty cool development kit http://www.newark.com/enocean/edk-350/energy-harvest-868mhz-developer/dp/98W2496

     

    This stuff is pretty cool.  I have used a lot of enocean modules and developed a enocean to Zigbee bridge to use enocean switches in commercial lighting systems.  These parts are not really cheap, but what things are?

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • deepak.domingo@ucdconnect.ie
    deepak.domingo@ucdconnect.ie over 8 years ago in reply to genebren

    Hi,

     

    My requirement is to just power two 5V DC LED circuits.

     

    Range is not a problem as a radius of 2 meters is sufficient.

     

    The design I am looking at is enocean sensor (piezoelectric) push button to reciever connected to arduino powering 2 output 5VDC LED circuits.

     

    Would you reccommend Enocean as a low cost solution?

     

    Thanks & Regards,

     

    Deepak

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • deepak.domingo@ucdconnect.ie
    deepak.domingo@ucdconnect.ie over 8 years ago in reply to genebren

    Hi,

     

    My requirement is to just power two 5V DC LED circuits.

     

    Range is not a problem as a radius of 2 meters is sufficient.

     

    The design I am looking at is enocean sensor (piezoelectric) push button to reciever connected to arduino powering 2 output 5VDC LED circuits.

     

    Would you reccommend Enocean as a low cost solution?

     

    Thanks & Regards,

     

    Deepak

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to deepak.domingo@ucdconnect.ie

    Deepak,

     

    The parts above could be used to do what you are referring to.  You need the piezoelectric switch (with transmitter), a receiver and then your arduino to light your LEDs.  This is not really a low cost solution, but if you can not tolerate a battery in your switch, this is about the only solution that you have.  The switch is ~$33.00, and the receiver is ~$16.00.  If you could tolerate the battery, or used a small solar cell to harvest energy to charge a supercap/battery, then you could use some of the very low cost ESP-01 like modules to broadcast your switch signal over WiFi  (there are a lot of examples using these parts here on element14 blogs/projects).

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • deepak.domingo@ucdconnect.ie
    deepak.domingo@ucdconnect.ie over 8 years ago in reply to genebren

    Thanks for the advise Gene.

     

    Taking the cost into account, would you advise that Zigbee GreenPro or Z wave would be priced lower?

     

    I am looking at 2 sensors and 2 recievers with a simple MCU to drive the LEDs to be under $50 for a college project.

     

    Your suggestions would be helpful.

     

    Thanks & Regards,

     

    Deepak

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to deepak.domingo@ucdconnect.ie

    Deepak,

     

    There are so many ways to go.  What you are proposing it a very simple communication, so unless you need to, don't complicate it.  Zigbee is a very powerful mesh device with a high level of complexity and relatively high cost.  I would consider looking at something mush simpler.  There are some sub GHz band transceivers that are available for ~$1.00.  One of these paired with a small microprocessor (also ~$1.00) would make a simple solution to the design that you mention.  If you want to move to a slightly higher technology solution there are some Bluetooth transceivers available at ~$5.00.  These two could be paired with a small microprocessor to build either sensor or receiver.

     

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • deepak.domingo@ucdconnect.ie
    deepak.domingo@ucdconnect.ie over 8 years ago in reply to genebren

    Thanks for the advice Gene. Much appreciated.

     

    Best Regards,

     

    Deepak