Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog A Human-Centred Internet of Things
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
  • Author Author: e14 Contributor
  • Date Created: 13 Apr 2015 5:19 PM Date Created
  • Views 769 views
  • Likes 2 likes
  • Comments 3 comments
  • internet_of_things
  • iot
Related
Recommended

A Human-Centred Internet of Things

e14 Contributor
e14 Contributor
13 Apr 2015

The Internet of Things will be built on a base-layer of Internet-connected “Smart Objects”. However, there is a growing discomfort among individual users about being surrounded by Objects that collect information and then send it to who knows where to be shared with who knows who to be used for who knows what. There is growing alarm about Objects being used to spy on people, about smart home and smart car technology being hacked for break-ins and hijackings. Could somebody hack my smart thermostat data to identify when my house is unoccupied? Could somebody remotely lock me into my driverless car and kidnap me? With lots of Internet scare stories about strangers shouting out of web-connected baby-monitors and implanted medical devices being taken over remotely, such discomfort and alarm are very understandable.

 

As technologists, we perhaps tend to think that technology is a sufficient end in itself – that using technology to do something interesting or make something new is enough. However, for the Internet of Things to work, we need to go a few steps further: we need to ask ourselves questions such as “How can I reassure the user that this Object is safe and secure to use?”, “How can I make my Object so Enchanting that the user is happy to accept the added risk of having an Internet-connected Object in their lives”? People are happy to accept that their computers and phones are connected to the Internet but anti-virus and firewall software acts as a “comfort blanket” . Such a comfort blanket is not, however, available with many Objects.

 

How do we overcome these concerns? The first step is to ensure that the Object adds real value to the user’s life – this could be in terms of its practical functionality, its ease of use, its personal benefit or its aesthetics but, ideally, all four. All Objects will have functionality but we technologists again need to look beyond this. The withdrawn Google Glass could be viewed as having good functionality and relatively good ease-of-use but poor aesthetics and, as all too readily-identifiable Glass public users faced growing hostility, the opposite of personal benefit[1]. If an Object can hit all four areas of value, the user is more likely to be interested in being convinced how we technologists have made the Object private, safe and secure to use. With HealthKit, as with many of their products, Apple hit functionality, personal benefit, ease of use and aesthetics but users still had many concerns about data privacy and security[2] and Apple have been taking urgent action to reassure users.

 

It’s a very big challenge for Object designers: functionality, ease of use, personal benefit and aesthetics PLUS privacy, security and safety – and all of these across the many different application domains for the IoT. This is why phrases like “User Experience (UX)” and “Human Centred Design” are increasingly being heard in IoT discussions. In the Nimbus Centre where I work, our Smart Object development teams always include different varieties of technologist but may also include application domain experts, users, creative designers, UX designers, psychologists and sociologists. As technology specialists, we can’t hope to be expert in all of these topics but we do need to at least understand the importance of taking their influence into account in the Object design process and reach out for expert help as needed.

 

 


[1] http://www.forbes.com/sites/andrewcave/2015/01/20/a-failure-of-leadership-or-design-why-google-glass-flopped/

[2] (http://www.forbes.com/sites/dandiamond/2014/09/08/can-apples-healthkit-protect-your-data/)

  • Sign in to reply
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    One thing you've not mentioned is transparency. Perhaps people would not object to objects so much if the providers were more honest and open about what they were doing. It might also be good to give a user a choice to provide less information or deny requests, an information firewall for example.

     

    For example, "Upon first initialisation the Enchanted Cottage will request your location information which will be shared with the Yahoo weather forecast service in order to attain weather information, if you choose to general area or country rather than your exact position the Enchanted Cottage may provide a less accurate forecast."

     

    One thing that always annoys me is "Date of Birth" requests, yes a system wants to ensure I am older than a particular age but does it need my date of birth to do that?

    My other gripe is data collection by stealth in the guise of security such as asking for a mobile phone number so that I can do "two factor authentication".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago

    One thing you've not mentioned is transparency. Perhaps people would not object to objects so much if the providers were more honest and open about what they were doing. It might also be good to give a user a choice to provide less information or deny requests, an information firewall for example.

     

    For example, "Upon first initialisation the Enchanted Cottage will request your location information which will be shared with the Yahoo weather forecast service in order to attain weather information, if you choose to general area or country rather than your exact position the Enchanted Cottage may provide a less accurate forecast."

     

    One thing that always annoys me is "Date of Birth" requests, yes a system wants to ensure I am older than a particular age but does it need my date of birth to do that?

    My other gripe is data collection by stealth in the guise of security such as asking for a mobile phone number so that I can do "two factor authentication".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Workshopshed

    Good point. I have seen that even if providers are open and transparent, it does not necessarily establish trust - there have been so many large scale data breaches and scare stories about government data gathering in recent years that trust is badly broken and will need to be restored if the IoT is to work as best it can. The general feeling is that data is like a bad smell - once it's out there, there's no telling where it's going to end up. Complete privacy may become the regulatory default for the IoT with explicit opt-in required for handing over any data to any Object.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to e14 Contributor

    Actually that raises another good technical point. Often data is sent from the object to the cloud when it does not need to be. A tiny web server could run on for example a central heating controller and I could connect directly to that rather than needing to connect to a web service at all.