Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Automatic Updates?
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
  • Author Author: Workshopshed
  • Date Created: 26 Jun 2015 12:02 PM Date Created
  • Views 843 views
  • Likes 3 likes
  • Comments 0 comments
  • enchanted_cottage
  • enchanted_objects
Related
Recommended

Automatic Updates?

Workshopshed
Workshopshed
26 Jun 2015

In the below presentation on security Rohini Pandhi mentions the problem of keeping your device updated.

 

Unconnected consumer items used to be simply build, distributed and sold with no process for doing any updates. Embedded systems did have options for updating but often this needed to be done by a trained field service engineer or by returning the item to the factory. Small issues spotted post production were fixed in new versions but often not patched in older versions. If there was a significant fault with a system then they would need to be an expensive product recall.

 

With connected devices there is the added issue of security. When there is a security issue these often need to be patched faster or there might be problems for the end users.

The fact that the device is connected means that patches can be downloaded and applied more easily as is done with mobile phones and PC.

 

For embedded products there are additional challenges

  • Lack of user interface
  • Always on
  • Power requirements (flashing a ROM could use a lot of power)
  • Handling failures
  • Automating the installation process

 

I've not really looked into these issues for my project so would be interested to know what other peoples thoughts are?

References

The 10 challenges of securing IoT communications | Atmel | Bits & Pieces

Efficient over-the-air software and firmware updates for the Internet of Things - Embedded Computing Design

Meraki firmware updates while you sleep

Open source solutions ease process of updating leg - AMD – Aerospace Manufacturing and Design

A router firmware update goes bad | Computerworld