Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects - Enchanted Clock (#6) "Its got a name!!"
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
  • Author Author: dwinhold
  • Date Created: 11 May 2015 4:09 AM Date Created
  • Views 654 views
  • Likes 2 likes
  • Comments 2 comments
  • enchanted_clock
  • enchanted-objects-design-challenge
  • enchanted-objects
Related
Recommended

Enchanted Objects - Enchanted Clock (#6) "Its got a name!!"

dwinhold
dwinhold
11 May 2015

This update brings you how the clock will personally greet you when you stand in front of (it?, "It" seems so impersonal. My daughter Chrystal has named it "Tic", she says since we are going to make it talk. "Tic - T(alk)". Close enough explanation I guess. I use it as an acronym ("T"alking - "I"nteractive - "C"lock ). Here is the missing bracket).

 

So we programmed the Arduino to use the 2x16 LCD screen and Ultrasonic sensor to accomplish this. Below are pictures with the readout on the screen:

image

 

 

Please excuse the crudity of my drawing, Chrystal is still laughing about it.....

image

So right now we have got the family member recognition up and running. The binary clock attachment is working. We have the thermostat controller running but we have to get the voice control connected and working. The light control hasn't been set up yet, but the programming is complete. It works similar to the height recognition system except it looks for movement and non-movement. Still working on the clock itself, once it is built the time keeping program will be the final step.

 

More explanation of the light control:

 

So the ultrasonic sensor has set distances programmed into the Arduino, like from the clock to the couch unoccupied.

image

When someone is sitting on the couch the sensor reads a different distance which makes it aware that someone is there.

image

Now I have set the parameters to have a "<" and ">" value, if this value stays "=" for more then the set amount or reads the default of the couch being unoccupied the lights will dim for 2 minutes then shut off. If the couch is occupied and the occupant hasn't moved (value stays consistent for set time) it is considered they have fallen asleep. If someone walks in the room, the lights will only turn on to dim as to not wake the sleeping family member unless the couch is empty.

I will set the lights to turn on dim if it past a certain time of night unless you ask "Tic" to turn the lights on full.

 

Thank you for reading,

 

Dale and Chrystal Winhold

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago +1
    Nice idea. This is far more interactive than simple movement detectors ... I like your drawings ...tell your daughter to stop sniggering.. Mark
  • Workshopshed
    Workshopshed over 11 years ago +1
    Good work Dale and Chrystal, a great clock name. My daughter is growing so quickly at the moment we'd need to have some kind of dynamic calibration in our house. The pictures are clear so I'd not worry…
  • Workshopshed
    Workshopshed over 11 years ago

    Good work Dale and Chrystal, a great clock name. My daughter is growing so quickly at the moment we'd need to have some kind of dynamic calibration in our house.

    The pictures are clear so I'd not worry too much, I use clip art from PowerPoint and LibreOffice and as you might have spotted some friends have provided photos.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    Nice idea.

    This is far more interactive than simple movement detectors ...

     

    I like your drawings ...tell your daughter to stop sniggering..

     

    Mark