Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects Design Challenge - How much!?
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
  • Author Author: Workshopshed
  • Date Created: 23 Jun 2015 8:32 AM Date Created
  • Views 3544 views
  • Likes 6 likes
  • Comments 14 comments
  • enchanted_cottage
  • enchanted_objects
  • costs
Related
Recommended

Enchanted Objects Design Challenge - How much!?

Workshopshed
Workshopshed
23 Jun 2015

Cost Analysis

As well as the components kindly provided by Element14, Atmel and Infineon there were several additional components purchased for this project. These were bought as the project progressed or were already in the spares drawer. Where the original supplier was not known the costs were estimated based on current prices. Where more components were purchased than needed the costs were pro-rated. I've tried to include absolutely everything but it is possible that something was missed.

 

Parts provided

An attempt was made to use as many of the provided parts as possible. Although these parts did not cost me, they are incorporated into the cost estimates to give a more realistic reflection of the cost of the project. Rather than incorporating the entire cost for the workshop kit the individual parts used were estimated from the Farnell site. The exact switches could not be found so an equivalent was used.

PartSupplierCost
Ardino YunElement14£49.03
Infineon RGB boardElement14£21.04
Arduino ProtoshieldElement14£3.55
IRF520 Power MosFetElement14£0.61
220R resistorElement14£0.01
2* 330K resistorElement14£0.01
2 * 10k resistorElement14£0.01
1n4007 diodeElement14£0.03
2 * Tactile SwitchElement14£0.18

 

Parts purchased

These were specifically purchased for the project, postage is included in the cost and where multiple items were purchased the cost was pro-rated between the items. For the 3D printed parts the cost was estimated by uploading the items to Shapeways and using their material value to provide an estimate.

PartSupplierCost
Houseuksalesmaster on Ebay£17.38
SD CardWHSmiths£7.00
Mini Servobgood2010 on Ebay£2.19
RGB LEDOomlout£1.50
LM393 ComparatorD&M Components on Ebay£0.50
1M resistorD&M Components on Ebay£0.10
2x 5.1v ZennerD&M Components on Ebay£0.20
Piezo sensorElectronic Bits and Bobs on Ebay£0.40
WoodHobbyCraft£1.93
Stacking headersAdaFruit via CPC£1.59
SignSign-O-Matic£6.70
PaintB&Q tester pot£0.25
Lithium Polymer Battery - 2000mAhCool Components£13.69
Adafruit PowerBoost 500AdaFruit via Cool Components£13.00
Nuts and Threaded RodModel Fixing£4.28
Fibre OpticsFibreopticlightingsolutions on Ebay£0.99
Mechanical componentsWorkshopshed£1.96

 

Parts that were already available

These were found around in the workshop, either from abandoned projects, multipack purchases or salvaged. The solder was estimated using the method found on http://electronics.stackexchange.com/questions/30671/estimating-assembly-cost

PartSupplierCost
DHT22PENGHUIMEI on Ebay£3.74 (2013 cost)
Stripboard / Tri-pad boardRadioShack£0.50
MagnetsFirst4Magnets£3.74
Stainless steel wireHalfords£0.06
Self-tapping ScrewsUnknown£0.70
Sugru x 2Sugru£2.00
Bondloc Structural AdhesiveMaplin£0.50
Heat Shrink TubingProto-Pic£0.04
Connector housingsProto-Pic£0.32
Connector pinsProto-Pic£1.58
SolderUnknown£0.48

 

Totals

Provided parts: £74.66

Additional Components: £73.65

Things I had: £13.65

Grand total: £161.96

 

Reducing costs

The Enchanted Cottage is effectively a prototype so there's plenty of decision that were made along the way. This has resulted in additional materials use and less than optimal design. This means that there is plenty of scope for cost savings.

 

The key tasks to reduce cost are:

 

  • Reduce component count
  • Replace/Remove expensive components
  • Simplify design

 

Also many of the components were bought in small batches so buying components in larger batches the costs would be reduced and multiple different postage costs could be eliminated.

 

Reduce Component Count

 

The Arduino Yún is a good board but its focus is to be a generic prototyping board rather than an embedded solution. Key examples of this are that the ATMega32U4 microcontroller is capable of running at 3.3v same as the Wifi module but the Arduino team chose to run it at 5v to give it maximum compatibility. This means that the board contains lots of level shifters on the board to interface between the two sides. If a custom board was made then this could run at 3.3v and eliminate these level shifters.

 

Also having the 3 boards stacked together with separate power board means that headers, connectors, spacers, struts are used for the board. So again merging all of these onto a single board would bring the costs down as many of these could be eliminated.

 

Expensive Components

 

The Arduino Yún has already been mentioned, that is one of the highest cost items. A "Dragino HE" WiFi module is approx £15 and the ATMega32U4ATMega32U4 is £2.34 when bought in quantities of 10 or above, a few basic components such as capacitors and a crystal are needed.

 

The Infineon RGB LED driver board is again and expensive component, it was used for the project as it provided a quick an easy approach to providing the output. However it is really over specified for the job and is being run right on the lowest level of it's capability. The approach here would be to take swap this out with a driver using discrete MOSFets to power each of the channels for the LED such as the INFINEON  BSS131INFINEON  BSS131 as that's quite capable of being driven by the lower 3.3 supply. To standardise the bill of materials these could also be used to control the power to the servo and temperature sensor. Again the same MOSFet could be used to turn on and off the power to the WiFi module

 

The sign for the back of the cottage was made of plastic and most of it's cost was delivery charges rather than manufacturing costs. If the house was being produced in bulk then this could be swapped out with a sticker rather than a sign which is substantially cheaper.

 

The house itself is quite a large expense so this could be replaced with a hand made version, the wood could also be bought in larger sheets for greater savings.

 

The current power design incorporates a boost regulator to generate 5v from the 3.7v battery. This is then reduced back to 3.3v by two different regulators, one on the Infineon board and one on the Yún. By swapping to a 3.3v design this could be simplified to be a single regulator that would provide 3.3v. Assuming further savings in power can be achieved then the battery capacity could be reduced.

 

The magnets were surplus from a previous project so these could be swapped with cheaper ones for the same results.

 

In general SMD components are cheaper than through hole components and take up less space on the PCB, so this is an area where plenty of savings could be made.

 

Simplify design

 

One of the key improvements of swapping to a single PCB solution would be to remove the need for many connectors and small boards. For example by mounting the LED directly on the board the need for a daughter board, connectors and wires could be eliminated. Similarly by incorporating the power supply parts onto the main PCB further connectors and headers would be removed. The stacking headers needed for the Arduino shield approach would also be eliminated.

As mentioned above one method to reduce costs would be to scratch built the weather house, this would also allow the design to be simplified reducing the wood used and number of components. Rather than having a separate front and back these could be integrated together simplifying the design. Rather than hand cutting the parts these could be laser cut so that there was a single sheet with each of the parts that could be popped out. This would reduce assembly costs. Equally these could be pre-printed as per the original house saving on painting cost and

The 3D printer parts are currently screwed together, if the technique using clips could be made to work, or if these screws were swapped with plastic rivets then the assembly would be simpler and the time taken the make the parts could be easier.

The design incorporates an SDCard to hold some of the code, if the Linino side of the design was optimised then this card could be eliminated and hence component parts and set-up steps for that module would be reduced.

The Knock Knock sensor incorporates a variable resistor to "trim" the level detection. If a series of detectors was checked it might be possible to replace this with a simpler resistor network with a fixed level.

 

Estimated cost savings

 

Based on rough estimates and the changes above to the project components it should be possible to bring the cost down to approx £60, a saving of over £100 on the original bill of materials. No attempt has been made to calculate manufacturing costs but the above suggestions should bring those costs down too.

 

Next: Enchanted Objects Design Challenge - Painting, top panel and new magnet carriers

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1 +3
    I was trying to estimate the time spent on the project but I did not keep track of that. I'm guessing something in the order of 200 hours.... If someone manages to create a spin off product from my work…
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed +2
    Workshopshed , when really drilling down on the costs, I believe that there are significant savings that can be made in all the designs in this contest. The fact that we use development boards and shields…
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed +2
    Most of us are not using that RGB solution from Infineon for what it is intended. I'm rather impressed by what that controller with LED control peripheral can do. It can handle significant power with great…
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    This would make a nice low power alternative to the shield + RGB LED solution,

    https://www.adafruit.com/product/1612

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    Most of us are not using that RGB solution from Infineon for what it is intended.

    I'm rather impressed by what that controller with LED control peripheral can do. It can handle significant power with great finesse.

    I may purchase some raw power LEDs later to really put the Infineon solution to the test.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps

    I had to crank the settings right down to avoid over powering my little LED. I'd have liked to have played with programming that shield, it could potentially be used stand alone. I'll have to catch up with the Roadtests on the boards once the challenge is over.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps

    I had to crank the settings right down to avoid over powering my little LED. I'd have liked to have played with programming that shield, it could potentially be used stand alone. I'll have to catch up with the Roadtests on the boards once the challenge is over.