Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects Design Challenge - Painting, top panel and new magnet carriers
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
  • Author Author: Workshopshed
  • Date Created: 23 Jun 2015 1:35 PM Date Created
  • Views 2049 views
  • Likes 6 likes
  • Comments 7 comments
  • enchanted_cottage
  • enchanted_objects
Related
Recommended

Enchanted Objects Design Challenge - Painting, top panel and new magnet carriers

Workshopshed
Workshopshed
23 Jun 2015

The cottage was disassembled so that the base could be painted matt black. This is an old magician's trick to draw the eye away from the base and hidden mechanism underneath.

image

The top panel electronics were also put together with another bit of stripboard, a couple of buttons and a 3 way connector.

image

This was then glued to the top panel using some blobs of Sugru, of course it's best if you can avoid gluing your electronics into the product as it makes the whole thing harder to service. Given that it's the final week of the project, it's not appropriate to redo the whole of the top panel. Retrospectively it would be better to design some supports and slots into the top panel so that the board could simply be pushed into place.

image

As with pretty much all of the connectors, this one had to be bent at right angles so that there was space for the connector to be fitted. For future projects perhaps some preformed right angle connectors would be a good idea.

 

The top panel was added to the cottage and the buttons were tested.

image

The newly printed magnet carriers were fitted, and the magnet holders glued on top ensuring the correct orientation.

imageimage

Next: Enchanted Objects Design Challenge - System Overview

  • Sign in to reply

Top Comments

  • fvan
    fvan over 11 years ago +2
    It's all coming together nicely!
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1 +2
    Oh yes, will be ecstatic when I have a demo of it working. Hopefully one last push this evening.... There are plenty of other projects and DIY tasks that can leap up and fill the void but I think I'll…
  • gadget.iom
    gadget.iom over 11 years ago +1
    Looking good! I really need to get a 3D Printer.
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1

    Oh yes, will be ecstatic when I have a demo of it working. Hopefully one last push this evening....

    There are plenty of other projects and DIY tasks that can leap up and fill the void but I think I'll be taking a well deserved break and catching up on my reading and Ben Heck videos.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    Nice work.

     

    I'll bet you'll be glad when this challenge is over, along with a touch of sadness.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to DAB

    In my opinion, as the cottage is full of colours (roof, grass, the two characters etc.) it is not a bad idea to create a scenery out of the contour context. Don't you think ?

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Good progress, but I would have gone for a brighter color for the base just to draw attention to the cottage.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago

    All is coming with a flavour of complete and defined. Pro version! Good image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>