Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects Design Challenge - Windows 10
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
  • Author Author: Workshopshed
  • Date Created: 12 Jun 2015 8:08 AM Date Created
  • Views 2315 views
  • Likes 2 likes
  • Comments 9 comments
  • enchanted_cottage
  • enchanted_objects
  • 3dprinting
Related
Recommended

Enchanted Objects Design Challenge - Windows 10

Workshopshed
Workshopshed
12 Jun 2015

Matilda does not see the light

When Matilda tested the temperature status LED it was clear that it was not going to be visible from outside the cottage. The dark cottage interior sapped away the struggling coloured lumens. However, Matilda spotted that the LED was positioned right opposite the fake painted window on the front of the cottage.

image

If that could be replaced with a real window then the LED would be clearly visible. Now some people when thinking about new windows would be looking at curtain material and lace edging. Matilda was not that sort of a person, she was thinking about how best to smash a hole the front wall.  Matilda donned her safety glasses and removed the flower box to provide access. She drilled a hole in each corner and then used a cutting disk to join up the sides. Finally the edges were trimmed up to give a clean hole. Matilda was happy with the job.

image

New Windows

Matilda designed some new frames using OpenSCAD and these went through many iterations. The early versions barely looked like Windows at all and an alternative design for Windows 8 was terrible so she returned to a conventional design and Windows 10 turned out ok. She sent the designs off to the blacksmith to be assembled.

 

Frame source: https://github.com/Workshopshed/EnchantedObjects/blob/master/Mechanics/WindowFrame.scad

Frame model: https://github.com/Workshopshed/EnchantedObjects/blob/master/Mechanics/WindowFrame.stl

 

Printing

Remarkably the windows printed correctly first time and the best of the two examples was installed using contact adhesive.

image

image

Next: Enchanted Objects Design Challenge - The Lode Stone

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 11 years ago in reply to iayanpahwa +2
    I was lucky enough to get one in a RoadTest http://www.element14.com/community/roadTestReviews/1965
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1 +1
    Milling milling milling ... Seriously, Mark, when you have spent the needed time to setup a decent platform (including software I mean) you happily discover that in very ew time you setup what you need…
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1 +1
    Yes, I could have easily made these out of match sticks in less time than it took me to design and print them. However I am getting better at the OpenSCAD and can put some quite sophisticated shapes together…
Parents
  • mcb1
    mcb1 over 11 years ago

    A handy reason to buy a 3D printer ...

     

    I'm still resisting because I just know that the time spent in the design, etc will eclipse the savings made in construction.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago

    A handy reason to buy a 3D printer ...

     

    I'm still resisting because I just know that the time spent in the design, etc will eclipse the savings made in construction.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    Milling milling milling ...

     

    Seriously, Mark, when you have spent the needed time to setup a decent platform (including software I mean) you happily discover that in very ew time you setup what you need, start making and after few months you discover how much time you spent bit incomparable results of handy tools. And also including the fact that some materials are not so simple to manage by hand.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1

    Yes, I could have easily made these out of match sticks in less time than it took me to design and print them. However I am getting better at the OpenSCAD and can put some quite sophisticated shapes together quite quickly. I think the key advantages of the printer are when you have to make a lot of something or when you've got a complex shape such as the fibre housing, that would have been tricky with conventional methods because of the little holes and need to avoid the debugging socket.

     

    I was very happy to get an email the other day telling me that one of my other models had been adapted by someone. http://www.thingiverse.com/thing:728871/#remixes

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to balearicdynamics

    I do quite fancy a milling machine but I'm a bit short on space in the workshop, particularly if I went down the CNC route as I'd then need space for a PC too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed

    I could have easily made these out of match sticks in less time than it took me to design and print them

    See I was correct.

     

    I think the key advantages of the printer are when you have to make a lot of something or when you've got a complex shape

    Can't argue with that one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed

    I do quite fancy a milling machine

    I can see the beneft in a milling machine.

     

    I did have someone sorting out a 600 x 600mm one which suits the larger stuff I tend to be involved with.

    He argued that with an additional axis you could have a 3D printer as well ...

     

    Now if someone had  a laser cutter or waterjet ...

    Mark