Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Windows
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
  • Author Author: coolbox
  • Date Created: 24 Jun 2015 6:21 PM Date Created
  • Views 1090 views
  • Likes 2 likes
  • Comments 2 comments
  • enchanted_objects
  • enchanted_windows
  • arduino_yun
  • arduino
Related
Recommended

Enchanted Windows

coolbox
coolbox
24 Jun 2015

Hi,

Here,I want to post some update about may Enchanted windows project. I was able to control window using arduino yun’s wi-fi.I was not sure about a actual window so I have tried with thermo Cole model.

 

Here I have used 150 RPM DC geared motor with Infineon DC motor control shield.pic connections are:

Digital 2 in yun -> IN1 in motor shield

Digital 3 in yun -> IN2 in motor shield

INH1 and INH2 were connected to 5V in yun. Also I have shorted GND of Infineon shield and yun as power for both board are different. Yun was powered by 5V supply and motor shield was powered by 12V supply same as motor supply.

 

Yun Software:

I have modified Bridge example as per my requirement. Using REST APIs I was able to control motor. Code is as below:

 

 


 

#include <Bridge.h>

#include <YunServer.h>

#include <YunClient.h>

 

// Listen to the default port 5555, the Yún webserver

// will forward there all the HTTP requests you send

 

YunServer server;

boolean JustTwoSeconds;

 

void setup()

{

  // Bridge startup

  pinMode(13, OUTPUT);

  digitalWrite(13, LOW);

  Bridge.begin();

  digitalWrite(13, HIGH);

 

  // Listen for incoming connection only from localhost

  // (no one from the external network could connect)

  server.listenOnLocalhost();

  server.begin();

 

  // For Driving Motor We need this two pins.

  pinMode( 2, OUTPUT ); //IN_1

  pinMode( 3, OUTPUT ); //IN_2

 

 

}

 

void loop()

{

  // Get clients coming from server

  YunClient client = server.accept();

 

  // There is a new client?

  if (client)

  {

    // Process request

    process(client);

 

    // Close connection and free resources.

    client.stop();

  }

 

  delay(50); // Poll every 50ms

 

  if( JustTwoSeconds )

  {

    JustTwoSeconds = 0;

    delay(4900); // 1.5 sec

    digitalWrite( 2, LOW ); //IN_1

    digitalWrite( 3, LOW ); //IN_2   

  }

}

 

 

 

void process(YunClient client) {

  // read the command

  String command = client.readStringUntil('/');

 

  // is "digital" command?

  if (command == "digital") {

    digitalCommand(client);

  }

 

  // is "analog" command?

  if (command == "analog") {

    analogCommand(client);

  }

 

  // is "mode" command?

  if (command == "mode") {

    modeCommand(client);

  }

}

 

 

 

 

void digitalCommand(YunClient client)

{

  int pin, value;

 

     // Read pin number

     pin = client.parseInt();

 

    

   if( pin == 1 )

   {

         digitalWrite( 2, HIGH ); //IN_1

         digitalWrite( 3, LOW ); //IN_2

        

         JustTwoSeconds = 1;

   }

   else if( pin == 2 )

   {

         digitalWrite( 2, LOW ); //IN_1

         digitalWrite( 3, HIGH ); //IN_2

        

         JustTwoSeconds = 1;

   }

   else if( pin == 3 )

   {

         digitalWrite( 2, LOW ); //IN_1

         digitalWrite( 3, LOW ); //IN_2

   }

   else

   {

       ;

   }

}

 

 

 

 

 

 

 

HTML File:

For EASY interface I have created simple HTML file which you can open in any device. Code is as follow:

 

<body bgcolor = "yellow">

 

<a href = "http://192.168.240.1/arduino/digital/1 ">

<h3><center> OPEN WINDOW </center></h3>

</a>

 

</br>

</br>

 

<a href = "http://192.168.240.1/arduino/digital/2 ">

<h3><center> CLOSE WINDOW </center></h3>

</a>

 

</br>

</br>

 

<a href = "http://192.168.240.1/arduino/digital/3 ">

<h3><center> STOP </center></h3>

</a>

 

</body>

 

I will publish a video soon.

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 11 years ago +1
    Good to see the shield and motors working, the model window turned out nicely too.
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    Good to see the shield and motors working, the model window turned out nicely too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago

    Good to see the shield and motors working, the model window turned out nicely too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • coolbox
    coolbox over 11 years ago in reply to Workshopshed

    Thanks Andy