Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Generating a Mysterious Signal
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
  • Author Author: crjeder
  • Date Created: 7 Jun 2015 10:23 PM Date Created
  • Views 4852 views
  • Likes 4 likes
  • Comments 46 comments
  • smart_key_hooks
  • enchanted_objects
  • bit_banging
Related
Recommended

Generating a Mysterious Signal

crjeder
crjeder
7 Jun 2015

Let us assume that I want to create a signal like this:

 

image

Where:

 

Signal

Name

Duration in

μs ± 150 ns

T0H0.4
T1H0.8
T0L0.85
T1L0.45
Treset> 50

 

The usual way to generate arbitrary signals is called "Bit banging". It requires software to set the output in the "HIGH" and "LOW" state in the exact timing given by the protocol. The timing requirements for this signal look pretty strict that I do not believe that this would be possible or at least not very reliable. So I am looking for some hardware support.

After a lot of head ache and reading datasheets the idea of using the PWM came into my mind.

Bit Banging with PWM

 

Let's look at the signal again:

  • it starts always with "HIGH" and ends with "LOW" (except for reset which is always "LOW")
  • length of signal is 1.25 μs (reset again an exception)
  • 0.05 μs resolution (0.05 is the greatest common divisor of 1.25, 0.4, 0.85 and 0.45)

 

Exact Solution

The signal can be generated with PWM of 1/0.05 μs = 20 MHz frequency. Therefore the "alphabet" above translates to:

 

SymbolDuty %
"0"32
"1"64

 

The PWM frequency of 20 MHz is quite high, can the signal be done approximated with lower frequency?

 

Reasonable Approximation

The odd thing about the spec for this signal is that it is not symmetric, i. E. the high time for "0" is not equal to the low time for "1" as I had expected. Since the rising edge of the signal is every 1.25 μs this allows the receiver to synchronize. The sampling presumably takes place at exactly the half of the time which explains the asymmetry: It gives a safety margin for the timing or rather does not require steep edges.

The tolerance for the falling edge is quite high. I did not recognize it at first sight, but when I converted the whole timing into nano seconds (ns) It's pretty clear:

 

Signal Name

Time of Falling Edge

Nominal [ns]

Time of Falling Edge

Minimal [ns]

Time of Falling Edge

Maximal [ns]

T0H400350550
T1H800650950

 

This allows a much more reasonable approach:

Divide the 125 ns in three sections ad vary the duty cycle between 1/3 and 2/3 or in decimal:

 

SymbolDuty %
"0"33
"1"66

 

The frequency in this case is only 2.4 MHz. That's much better!

 

Reset

 

The reset symbol is an exception - it does not fit in the above timing. It can be generated by 40 periods with a duty cycle of 0%.

Since we are able to generate the signal there is only one question left: What is this for?

 

Usage of the Signal

 

Did you recognize / guess the signal? What do you think it is for? image

 

(solution in the next blog post)

  • Sign in to reply

Top Comments

  • crjeder
    crjeder over 11 years ago in reply to balearicdynamics +3
    Yes, the quiz with you guys balearicdynamics , mcb1 , clem57 and Workshopshed was a lot of fun! Thank you for participating!
  • Workshopshed
    Workshopshed over 11 years ago +2
    Will there be a small flower dancing along to the music?
  • mcb1
    mcb1 over 11 years ago in reply to crjeder +2
    It's been a very interesting trip back down memory lane... Looking at this sheet for WS2812B it says single NRZ protocol http://www.seeedstudio.com/document/pdf/WS2812B%20Datasheet.pdf There is some interesting…
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    Will there be a small flower dancing along to the music?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago in reply to Workshopshed

    He he! No!

    Much smaller image!

    12:00 hours left..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to crjeder

    But it IS Manchester protocol ???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago in reply to balearicdynamics

    No, I don't thik so. Frankly I had to look up manchester code in Wikipedia:

    771px-Manchester_encoding_both_conventions.svg.png

    Manchester encodes the symbols "0" and "1" by a falling or rising edge at the middle of the period respectively. The mysterious signal does never change in the middle of the period. This is what I meant by the signal beeing a bit "odd". The change takes place at roughly 1/3 or 2/3 of the period length to encode "0" or "1".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to crjeder

    So, maybe a motor controlled without a traditional encoder (no need of clock signal) or a lighting system

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to crjeder

    So, maybe a motor controlled without a traditional encoder (no need of clock signal) or a lighting system