Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Generating a Mysterious Signal
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
  • Author Author: crjeder
  • Date Created: 7 Jun 2015 10:23 PM Date Created
  • Views 4834 views
  • Likes 4 likes
  • Comments 46 comments
  • smart_key_hooks
  • enchanted_objects
  • bit_banging
Related
Recommended

Generating a Mysterious Signal

crjeder
crjeder
7 Jun 2015

Let us assume that I want to create a signal like this:

 

image

Where:

 

Signal

Name

Duration in

μs ± 150 ns

T0H0.4
T1H0.8
T0L0.85
T1L0.45
Treset> 50

 

The usual way to generate arbitrary signals is called "Bit banging". It requires software to set the output in the "HIGH" and "LOW" state in the exact timing given by the protocol. The timing requirements for this signal look pretty strict that I do not believe that this would be possible or at least not very reliable. So I am looking for some hardware support.

After a lot of head ache and reading datasheets the idea of using the PWM came into my mind.

Bit Banging with PWM

 

Let's look at the signal again:

  • it starts always with "HIGH" and ends with "LOW" (except for reset which is always "LOW")
  • length of signal is 1.25 μs (reset again an exception)
  • 0.05 μs resolution (0.05 is the greatest common divisor of 1.25, 0.4, 0.85 and 0.45)

 

Exact Solution

The signal can be generated with PWM of 1/0.05 μs = 20 MHz frequency. Therefore the "alphabet" above translates to:

 

SymbolDuty %
"0"32
"1"64

 

The PWM frequency of 20 MHz is quite high, can the signal be done approximated with lower frequency?

 

Reasonable Approximation

The odd thing about the spec for this signal is that it is not symmetric, i. E. the high time for "0" is not equal to the low time for "1" as I had expected. Since the rising edge of the signal is every 1.25 μs this allows the receiver to synchronize. The sampling presumably takes place at exactly the half of the time which explains the asymmetry: It gives a safety margin for the timing or rather does not require steep edges.

The tolerance for the falling edge is quite high. I did not recognize it at first sight, but when I converted the whole timing into nano seconds (ns) It's pretty clear:

 

Signal Name

Time of Falling Edge

Nominal [ns]

Time of Falling Edge

Minimal [ns]

Time of Falling Edge

Maximal [ns]

T0H400350550
T1H800650950

 

This allows a much more reasonable approach:

Divide the 125 ns in three sections ad vary the duty cycle between 1/3 and 2/3 or in decimal:

 

SymbolDuty %
"0"33
"1"66

 

The frequency in this case is only 2.4 MHz. That's much better!

 

Reset

 

The reset symbol is an exception - it does not fit in the above timing. It can be generated by 40 periods with a duty cycle of 0%.

Since we are able to generate the signal there is only one question left: What is this for?

 

Usage of the Signal

 

Did you recognize / guess the signal? What do you think it is for? image

 

(solution in the next blog post)

  • Sign in to reply

Top Comments

  • crjeder
    crjeder over 11 years ago in reply to balearicdynamics +3
    Yes, the quiz with you guys balearicdynamics , mcb1 , clem57 and Workshopshed was a lot of fun! Thank you for participating!
  • Workshopshed
    Workshopshed over 11 years ago +2
    Will there be a small flower dancing along to the music?
  • mcb1
    mcb1 over 11 years ago in reply to crjeder +2
    It's been a very interesting trip back down memory lane... Looking at this sheet for WS2812B it says single NRZ protocol http://www.seeedstudio.com/document/pdf/WS2812B%20Datasheet.pdf There is some interesting…
Parents
  • crjeder
    crjeder over 11 years ago

    And we have a winner to this "Guess the Mysterious Signal" mini-callenge:

     

    Congratulations to clem57!

     

    He mailed me the correct answer 5 hours ago!

    It is a WS2812B RGB LED with integrated controller.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to crjeder

    I had not understood that you was asking for the exact component name ... Then, I am sorry I have delayed (maybe I find a way to kill clem57 with some strange frequency in attach to a mail) but I spent half of the day outside under the sun. Today we decided to posticipate the daily work some hours image So, my compliments to the winner !

     

    Enrico

     

    P.S. By the way crjeder, as mentioned in the datasheet of the WS2812B RGB LED:

    The data transfer protocol use single NZR communication mode. After the pixel power-on reset, the DIN

    port receive data from controller, the first pixel collect initial 24bit data then sent to the internal data latch,

     

    The NZR communication mode (that means Non Zero Return code) is one of the applications of the mentioned Manchester code are you can read on Wikipedia.

     

    Cheers, Enrico.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to crjeder

    I had not understood that you was asking for the exact component name ... Then, I am sorry I have delayed (maybe I find a way to kill clem57 with some strange frequency in attach to a mail) but I spent half of the day outside under the sun. Today we decided to posticipate the daily work some hours image So, my compliments to the winner !

     

    Enrico

     

    P.S. By the way crjeder, as mentioned in the datasheet of the WS2812B RGB LED:

    The data transfer protocol use single NZR communication mode. After the pixel power-on reset, the DIN

    port receive data from controller, the first pixel collect initial 24bit data then sent to the internal data latch,

     

    The NZR communication mode (that means Non Zero Return code) is one of the applications of the mentioned Manchester code are you can read on Wikipedia.

     

    Cheers, Enrico.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • crjeder
    crjeder over 11 years ago in reply to balearicdynamics

    Thank You for pointing this out!

    Yes NZR is mentioned in the datasheet, but Wikipedia calls the class of codes (which Manchester is one example) NRZ and it is wrong in this context, because the signal does return to zero.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to crjeder

    Yep, same mistake I've done reading the article. The point is not if the signal returns to zero or not - as it is impossible that remain always to one.

    The real meaning of the sentence is that while in the traditional  methods there are two state signals, 0 and 1 and the synchronization is done by a separate clock channel, in this case bot zero and one are done with both zero and one physical levels. Just because there is not a "support" signal clock for sync.

     

    a non-return-to-zero (NRZ) line code is a binary code in which 1s are represented by one significant condition (usually a positive voltage) and 0s are represented by some other significant condition

     

    Best. Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to balearicdynamics

    NRZ is an encoding technique used for communications to prevent dropped bits on noisy lines.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to clem57

    Hi Clem,

     

    I see, that's almost the reason that all these protocols communication family has been invented. Anyway it is a great thing I have never used. Not yet image

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago in reply to balearicdynamics

    Encoding and physical representation of signals are two different things. I am no expert here, but from what I understand Manchester goes into the "encoding" category where NRZ falls into the other. The reason for Manchester Code is to ensure a transition in every clock period to facilitate "self-clocking". NRZ on the other hand uses + 2.5 V and - 2.5 V as high and low for example to ensure that there always is an non-zero DC component in the signal which using + 5 V and 0 V would imply. Therefore more power is transmitted via NRZ which facilitates noise immunity among other positive effects.

    Just to show why I do not believe that the Mystery Signal is a Manchester Code I have drawn a image: