Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog oh no - deadline passed
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
  • Author Author: Jan Cumps
  • Date Created: 26 Jun 2015 8:17 PM Date Created
  • Views 1061 views
  • Likes 3 likes
  • Comments 2 comments
  • enchanted_player
  • enchanted_objects
Related
Recommended

oh no - deadline passed

Jan Cumps
Jan Cumps
26 Jun 2015

Just too late to meet the timeline image

 

I've been telling the story of the brothers Christian and Josef Steidinger here on the blog.

Christian is the one who left the family business and started the Perpetuum Ebner manufacture.

But to be honest, he's the one that didn't succeed. Brother George created the DUAL brand, and that company survived in its original form till the 80's.

 

The photos below are turntables that I have from DUAL. Some are brought back to specs. Others are Work In Progress.

I don't have a museum. Regularly I sell the ones that I have and buy new ones to play with.

 

 


 

{gallery} DUALs

image

DUAL 1010 and amp HS 32 (1960's): revised

image

DUAL 1019 (1960's): revised

image

DUAL 1218: donor for spare parts (1970's)

image

DUAL 1214 in console: wip (1970's)

image

DUAL 1218: WIP (1970's)

image

DUAL 510: revised (1970's)

 

 

 

 

The 1010 I've just purchased and fixed a week ago. That one has outside duty during sunny days. The others I pick and choose whenever I want, until I'm tired (or someone buys one).

 

{gallery} DUAL 510

image

DUAL 510: looks

image

DUAL 510: looks

image

DUAL 510: looks

image

DUAL 510: looks

image

DUAL 510: headshell

image

DUAL 510: cartridge and stylus

image

DUAL 510: tracking force and anti-skate

image

DUAL 510: speed control

image

DUAL 510: looks

 

 

If you're interested in turntable maintenance, I've got a Youtube channel dedicated to that subject.

  • Sign in to reply
  • DAB
    DAB over 11 years ago

    Nice link,

     

    I picked up a couple of turn tables at some garage sales locally.

    I might need to do some repairs if they do not work as advertised.

     

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    I have a DUAL 521.

    Absolutely brilliant until I replaced the stylus and it was never as good.

     

    It's just sitting in the bottom of the cupboard and I'm not 100% sure where all the round black things are ever since we moved 12 yrs ago.....

     

     

    Mark