Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Servo and mechanics in action
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
  • Author Author: Workshopshed
  • Date Created: 12 Apr 2015 8:55 PM Date Created
  • Views 2734 views
  • Likes 7 likes
  • Comments 14 comments
  • enchanted_cottage
  • enchanted_objects
Related
Recommended

Servo and mechanics in action

Workshopshed
Workshopshed
12 Apr 2015

A quick video of the servo and mechanism all connected up. I've spotted an interesting issue with these positional servos. When they power up the driving software has no idea where the servo is position so it will send the signal representing the centre position (which is configurable). The servo will move to that position as fast as it can even it it's right at the limits of it's positioning. Only after it reaches that point can the software attempt to control the speed of motion by sending a series of positions with delays between them.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This should be the last of the mechanical based posts and I'll switch onto electronics and software.

Hopefully there will be another installation of Hans and Matilda tomorrow but it might be delayed until slightly later in the week.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago +2
    Great work on all the woodwork. I can barely hammer a nail into a piece of wood without messing it up. Software development, applications and electronics are however no problem for me.
  • clem57
    clem57 over 11 years ago +1
    Seeing these figurines in action makes me marvel how the pieces work. Thanks Workshopshed
  • Workshopshed
    Workshopshed over 11 years ago in reply to gadget.iom +1
    I don't have cats but I do plan to hide the mechanism in an enchanting way. Don't want to say more as that would spoil the fun.
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Great work on all the woodwork.

    I can barely hammer a nail into a piece of wood without messing it up.

     

    Software development, applications and electronics are however no problem for me.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to e14 Contributor

    Cheers Rob, just a simple cut and glue job, although after cutting the 3rd hole for the servo I was getting quite good at it. I'm looking forward to seeing dwinhold's woodwork, that should be impressive although he's probably using a bit more than a knife and saw http://workshopshed.com/2015/04/3mm-plywood/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago in reply to e14 Contributor

    Cheers Rob, just a simple cut and glue job, although after cutting the 3rd hole for the servo I was getting quite good at it. I'm looking forward to seeing dwinhold's woodwork, that should be impressive although he's probably using a bit more than a knife and saw http://workshopshed.com/2015/04/3mm-plywood/