Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog The Genie Gives A Tour Of His House
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
  • Author Author: RParkerE
  • Date Created: 25 Mar 2015 1:15 AM Date Created
  • Views 1110 views
  • Likes 5 likes
  • Comments 5 comments
  • enchanted_objects
  • mini_automator
  • magic_lamp
Related
Recommended

The Genie Gives A Tour Of His House

RParkerE
RParkerE
25 Mar 2015

The genie being proud in nature, wished to show off his sweet new crib. He would like to invite all of you to an informal open house, where you can see his sweet new setup, and all his cool furniture. Arduino Yun was the architect of the genies sweet new living quarters. Mr. Infineon was the electrician. He wired the building to be as bright as the sun, but Mr. Infineon was also a good guy and wanted the energy consumption to be minimized, and allowed this through his setup. The lamp itself looks like it is a normal 60W bulb, shines just as bright too, but it only a 12V/15W bulb! Also the lamp doesn't have to be much larger than the average lamp, since the power required to power both units is minimal. So from the genie, "Welcome to my Magic Lamp!"

                                                    image

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 11 years ago +1
    Hi Parker, Nice presentation. I will look forward to seeing your lamp. John
  • Workshopshed
    Workshopshed over 11 years ago +1
    An energy efficient genie, fantastic!
  • amgalbu
    amgalbu over 11 years ago +1
    Nice presentation! Looks like your project is based on Arduino Yun... It was in the parcel or are still waiting for it?
Parents
  • amgalbu
    amgalbu over 11 years ago

    Nice presentation!

    Looks like your project is based on Arduino Yun... It was in the parcel or are still waiting for it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • amgalbu
    amgalbu over 11 years ago

    Nice presentation!

    Looks like your project is based on Arduino Yun... It was in the parcel or are still waiting for it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • RParkerE
    RParkerE over 11 years ago in reply to amgalbu

    Thank you! I did indeed receive the YUN in my parcel. I am currently waiting on the parts to prototype my lamp and contemplating what to do for the power sources, and then I will be ready to roll! image