Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog The Genie Makes A Grand Exit
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
  • Author Author: RParkerE
  • Date Created: 21 Jun 2015 3:03 AM Date Created
  • Views 3519 views
  • Likes 6 likes
  • Comments 18 comments
  • mini_automator
  • enchanted-objects-design-challenge
  • enchanted-objects
Related
Recommended

The Genie Makes A Grand Exit

RParkerE
RParkerE
21 Jun 2015

Unfortunately, I was unable to create a video to show you guys how beautifully my magic lamp was working. When I asked the genie to come out and play today he instead thought to introduce me to some magic smoke, and like that he was gone (In other words, my Infineon RGB  Shield went BOOM!). But I had a blast working on this project. I have a quick, very pathetic, mock up of what the final thing would look like.

 

image

 

The big box around the shield and Arduino is the 3D printed container. The finished product was very simple for any user to use. You only needed to know very basic things about Arduino to get started, (I tested it on my mother). All you needed to know is how to setup the Yun to connect to your home WiFi and how to upload a sketch onto the board. After that was done, the lamp would run on its own. I started looking into possibly even preloading the sketch to the board, but didn't get too far with that. The case I printed was Ivory, and I thought about taking it further and painting it oak, or different colors that matched the surrounding environment. The LED was placed on an Edison screw in bulb, so it fit in most household lamp sockets, however, you'd have to "plug" the lamp into the shield rather than straight into the wall. It was also relatively cheap, other than the case (but I got to print it for free! image).


 

ProductCost
Arduino Yun$55.01
Infineon RGB Shield$23.90
LED Chip and Bulb$20.00
Edison Screw In$15.00
TOTAL$113.91

 

And a lot of these costs can really be lowered depending on what you have already, and whether or not you really need to use the Yun. But I feel as though this product meets the requirements. I believe that it does as intended, even though I unfortunately have no proof other than this screenshot image.

image

I also believe, as I stated before, and my mother would agree, that it is very easy for a non technical person to use. However, the price is a little steep for a lamp, but as I stated it wouldn't be incredibly hard to adapt it some to make it much more cost effective. Also when you realize that it can also act as an alarm clock with a strobing feature at the designated time you wish to wake up, this price begins to be more realistic. And when properly cased, or placed, this would last a one a very long time, I see it as incredibly durable, well it was image, but also aesthetically pleasing. I wish I had pictures and videos for you all, and I may later, but for now I believe this to be a farewell, hopefully a see you soon. I had a great time and appreciate all of you! Look forward to seeing the out come of these other projects and who is announced the winner!

  • Sign in to reply

Top Comments

  • RParkerE
    RParkerE over 11 years ago in reply to Jan Cumps +4
    It is but a great learning experience!
  • Workshopshed
    Workshopshed over 11 years ago +1
    Yes, the Yún is a costly component for most projects. Hopefully as IOT takes off there will be more competition and cheap / low power options.
  • DAB
    DAB over 11 years ago +1
    Yea, every maker experiences that short moment of triumph before the magic smoke escapes. Still, it was a nice project and now you know that you should make a video of every test, just in case. DAB
  • RParkerE
    RParkerE over 11 years ago in reply to balearicdynamics

    It is actually this Friday, the 26th, which is why there is such a time crunch, and why I am not sure a video will be coming by then, I may continue this past the deadline, just to put everyone's curiosity to res.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to RParkerE

    I see but I was thinking to something temporary, just to give you the option to make some shooting on the finished project. Before next Friday, if I am not wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RParkerE
    RParkerE over 11 years ago in reply to balearicdynamics

    I have looked into possibly make a step down circuit to use with this project in general so it would be useable in all rooms, not just when attached to a computer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to RParkerE

    Maybe that for the other things I can do nothing, but for the 30V it is not so difficult to make if, at least following two possible ways: the first is from the wall AC power and a transformer and the other from a car battery (or the car charger plug without the control for the recharger, using the bare two cables and a simple power elevator like the one that from the car 12V reach 19V for the laptop charger

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RParkerE
    RParkerE over 11 years ago in reply to balearicdynamics

    I'll have to get the parents to ship me my materials(Yun, LED, Case, etc.), I'll have to order a new LED Shield, and then find a power source and I will be ready to present!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>