Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog The Weekend Proved Productive
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
  • Author Author: RParkerE
  • Date Created: 25 May 2015 2:59 AM Date Created
  • Views 1036 views
  • Likes 4 likes
  • Comments 2 comments
  • mini_automator
  • enchanted-objects
Related
Recommended

The Weekend Proved Productive

RParkerE
RParkerE
25 May 2015

So this weekend the genie buckled down, determined to finish the project he had started. His heart was delighted to see that he had finally finished all the wiring to his house! Now all that need to be done was furnishing and some aesthetics!


#include <TimeAlarms.h>
#include <infineonrgb.h>
#include <Wire.h>
#include <Time.h>
#include <stdlib.h>

InfineonRGB LEDS;

void setup() {
     // put your setup code here, to run once:
     LEDS.begin();   
     LEDS.SetDimmingLevel(0x0000);
     setTime(5,41,0,5,24,14); // set time to Saturday 5:41:00am May 24 2015
     Alarm.alarmRepeat(5,41,05, Light);  // 5:41:05am every day

}

void loop() {
     // put your main code here, to run repeatedly:
     Alarm.delay(1000);
}

void Light() {
     LEDS.SetIntensityRGB(0x01FF, 0x0000, 0x0000);
     LEDS.SetDimmingLevel(0x01FF);
     delay(3000);
     LEDS.SetDimmingLevel(0x03FF);
     delay(3000);
     LEDS.SetDimmingLevel(0x07FF);
     delay(3000);
     LEDS.SetDimmingLevel(0x0FFF);
     delay(3000);
     LEDS.SetDimmingLevel(0x07FF);
     delay(3000);
     LEDS.SetDimmingLevel(0x03FF);
     delay(3000);
     LEDS.SetDimmingLevel(0x01FF);
     delay(3000);
     LEDS.SetDimmingLevel(0x0000);
}

 

Above is the code that I used for the video, this will be implemented in the final code, but not using the TimeAlarm library. Also I would like to give Inderpreet Singh a huge thanks. His library infineonrgb.h was very useful. You can find it here.

 

                                                                                                    

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Stay tuned to see what magic the genie preforms next!

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 11 years ago +1
    Congratulations on getting the dimming working.
  • DAB
    DAB over 11 years ago +1
    I can see I need to pick up a couple of these Infineon LED controllers. They appear to be very useful. DAB
  • DAB
    DAB over 11 years ago

    I can see I need to pick up a couple of these Infineon LED controllers.

     

    They appear to be very useful.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    Congratulations on getting the dimming working.