Experimenting with Extreme Environments
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Extreme Environments
  • More
  • Cancel
Experimenting with Extreme Environments
Blog Blog 3 - Wildlife Monitor Project - Enclosure Modifications
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Extreme Environments to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 20 Apr 2024 12:56 AM Date Created
  • Views 1662 views
  • Likes 13 likes
  • Comments 5 comments
  • Pi Camera 3
  • Midas MC42005A6W-SPTLYI-V2
  • Hammond 1554VA2GYCL
  • Pi CM4 IO
  • Experimenting with Extreme Environments
Related
Recommended

Blog 3 - Wildlife Monitor Project - Enclosure Modifications

ralphjy
ralphjy
20 Apr 2024

Enclosure Modifications

Modifications need to be made in the form of additions to the interior and exterior of the enlosure to mount parts into the enclosure and attach the enclosure to its mounting pole.

  • Baseplate to mount the CM4 IO and RS-232 level converter board to the floor of the enclosure
  • Front panel to mount the sensors, Pi Camera, and Midas display at the top of the enclosure near the lid
  • External Pole Mounting Bracket Adapter to attach enclosure to garden pole
  • Rear Plugs to attach Bracket Adapter to rear of enclosure

All of these parts are 3D printed using PLA.  For long term outdoor exposure I'll need to replace the external bracket adapter with something more durable but it will work for the prototype.

 

Baseplate

The required dimensions (226mm x 147mm) of the baseplate exceed the printable area on my Anycubic Kobra 2 so I needed to print the baseplate in two halves and add a plate to join the two halves together.

image

The baseplate is mounted to the floor of the enclosure using the 4 M3 threaded inserts at the outer corners.  The CM4 IO board is attached to the baseplate using 4 M2.5 standoffs.  The position of the CM4 IO board is offset to allow mounting the RS-232 level translator on the left and allowing space for the power barrel plug cable at the bottom right.  The bottom space also allows insertion and removal of the uSD card.  Luckily, I am not using most of the connectors and just need access to the GPIO header on the left above the RTC battery and the CSI connector on the upper left (I'll need to leave these cables attached unless I dismount the board).

image

 

Front Panel

The front panel needs to position the sensors, camera and display at the center of the enclosure near the transparent lid.  I decided to mount a protoboard on the panel to hold the 3 sensors which I will plug into sockets.  The protoboard will allow me to aggregate the I2C wiring between the sensors and display and run a single harness to the GPIO connector on the CM4 IO board below.  The front panel fits into the PCB rails that are on the walls of the enclosure.

image

Here is a view of how the completed assembly will look.

image

 

Pole Mounting Bracket Adapter

I needed an adapter to attach the enclosure to the bracket that screws onto the top of the garden pole assembly.  Here is the adapter piece mounted to the bracket.  The adapter attached to the enclosure using the 2 center lid screws in front and using 2 screws in the back.

image

 

Rear Plugs

In order to attach to the back I needed to create support for the screws.  I printed 2 plugs for the center holes in the rear and press fit threaded inserts into them.

image

Here are the plugs pressed into the enclosure:

image

 

Mounted enclosure

Front view

image

Side view

image

 

Garden Pole

Here is a picture of the garden pole I'll be mounting the enclosure on.  It had been previously used to hold a bird feeder.  It is currently configured at a height of 3 feet, but it has 16" screw-in sections that can adjust the height.  It has a 5 prong base and is very stable even with a load in windy conditions.

image

  • Sign in to reply
Parents
  • javagoza
    javagoza over 2 years ago

    Congratulations ralphjy , great solution! This is the most complicated part of this challenge for me. I still haven't come to a solution that suits me. I have insisted on having batteries inside the box and it is being a nightmare to organize everything inside the enclosure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 2 years ago in reply to javagoza

    Thx javagoza .   Getting projects into enclosures is always a challenge.  I wish that I had the tools that mayermakes has.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 2 years ago in reply to ralphjy

    those tools came slowly one after the other..basically I spent almost all of my income to get those tools over the last 10 years. I still do a lot of modifications by hand as its often just faster/simpler. So I'm sure you get to a remarkable enclosure by hand as well. and you already showed how awesome they can look without fancy tools.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 2 years ago in reply to ralphjy

    those tools came slowly one after the other..basically I spent almost all of my income to get those tools over the last 10 years. I still do a lot of modifications by hand as its often just faster/simpler. So I'm sure you get to a remarkable enclosure by hand as well. and you already showed how awesome they can look without fancy tools.