Experimenting with Flyback Transformers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Flyback Transformers
  • More
  • Cancel
Experimenting with Flyback Transformers
Forum Some Changes in How Blogs are Scored in Experimenting Challenges
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Flyback Transformers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 43 replies
  • Subscribers 44 subscribers
  • Views 6121 views
  • Users 0 members are here
  • Experimenting Challenges
Related

Some Changes in How Blogs are Scored in Experimenting Challenges

rscasny
rscasny over 3 years ago

I am simplifying the requirements and changing the way the extra credit blogs will be scored, starting with the upcoming program, Experimenting with Flyback Transformers.

I'll describe the changes below.

Changes
I am dropping the introductory blog and the forum participation as separate tasks. Why? I just feel I was asking too much of a participant. I am still retaining the 5 extra credit blogs and the final blog.

New Scoring for Extra Credit Blogs
I think I was given some fair criticism on the way the extra credit blogs were scored. I was trying to streamline the judging process, but I feel a change in scoring is in order.

So, this is the system I want to adopt for the extra credit blogs. They will be scored based on the type of blog written, as well as how well all Blogs 1s, 2s, 3s, etc rank to each other.

Scoring for Type of Blog

  • Introduction blog: this type of extra credit blog describes the kit, performs an unboxing, and/or describes what types of experiments the participant will perform. Score: 20 points
  • Component or Technology Overview/Description: this type of extra credit blog describes the kit components, the supplier's product family, and variants in depth: Score: 25 points
  • Experiment Description: this type of extra credit blog describes an experiment, shows data, and/or comes to a conclusion regarding the experiment  Score: 50 points
  • Tutorial - this type of extra credit blog would show the reader how to do something such as coding, circuit building, and/or troubleshooting with regard to the kit components.. Note: this could be an experiment; however, if the full force of the blog is educational or to provide a nice-to-know tip or trick, then it will be scored as a tutorial Score: 55 points
  • Building an application with the kit -- the type of extra credit blog would describe how the participant used the kit's components to build a project that illustrates an application. While this blog isn't a pure experiment, it experiments with the component through an application Score 45 points

Add-on Points to an Extra Credit Blog

  • Including a video will earn you an extra 5 points
  • Including a video that our element14 team promotes on social media earns you an extra 15 points (this would be a high quality video)
  • Including educational images that illustrate the experiment and are highly informative earns you an extra 10 points

Ranking Score

All the Blog 1's, 2's, 3's, 4's and 5's will be scored relative to each other. They will be ranked based on quality. The lowest ranking blog will earn 2 points. Each blog above it will score an additional 2 points. Example: for 5 participants, 5th place = 2 points, 4th place = 4 points, 3rd place = 6 points, 2nd place = 8 points, 1st place = 10 points. 

The total extra credit blog score will be the sum of the type of blog score + the ranking score.

  • Sign in to reply
  • Cancel

Top Replies

  • rscasny
    rscasny over 3 years ago +5
    SCORING SYSTEM UPDATE I appreciate everyone who has offered their ideas. I like the point system and will continue to use it. While no scoring system is perfect, I think that a sweet spot can be found…
  • rscasny
    rscasny over 3 years ago +4
    I would like to thank everyone who participated in this discussion and offered their ideas. I'm going to update the instructions now. I think we have the scoring rules that are fair. Thanks! Randall
  • shabaz
    shabaz over 3 years ago in reply to rscasny +2
    I think this will definitely give contestants a lot of freedom, and pick up deserved points for good photos/experimenting/informative blogs/training content or video etc.. Also, an extra benefit, it…
Parents
  • Gough Lui
    Gough Lui over 3 years ago

    That is a most interesting scoring system.

    I think a potential issue is that a blog may not be a singular type. What if a blog shows an unboxing and an experimental design? Will it score both? Or the higher of the two?

    In theory, all blogs could be of a tutorial for best score, without much regard to quality? (i.e. difference in blog type score outweighs the 10 point rank score, potentially even the 15 point video+images modifier noting we have little control of what staff choose to promote on socials).

    This, in my view, forms a strict disincentive to write any introductions or overviews (20-25pt) category because anything classed as a tutorial or experiment will earn double without any difference in possibility of earning additional bonus points.

    It is also interesting to see there is no "cap" to points - so a single blog could be scored 55 (type) + 30 (bonus) + 10 (rank) = 95 points. This puts a lot more (potential, but variable) voting power back in the hands of element14 which is perhaps not a bad thing.

    There is also the potential for category overlap - when is a technology overview different from a tutorial on how to use a given component, and when is a tutorial about how to use a component different from an application build?

    I feel this is perhaps pushing towards five tutorial-experiment hybrid blogs as the best way forward.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to Gough Lui

    I asked my self some of those questions as well. I had a thought about how to resolve it, but I wanted to see what other people felt. So, let's say that one blog covers an introduction, and overview and an unboxing of a kit. How should it be scored. One way would be to be additive. So it would be worth 20 + 25 = 45 points. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to rscasny

    This opens up the obvious - what if I write a blog that is a tutorial (walks people through the ”how”), experimental design+data+conclusion (shows people the ”what”) but is also done through an application (perhaps explaining the "why")? Wouldn't that become a theoretical 100-point blog score (on top of which, bonuses and ranks would be handed out)?

    As with every contest, knowing the rules is the first step to potentially playing the game, or winning. If this is the golden path, then I will do my best :).

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to Gough Lui

    Interesting scenarios. That is, if someone packed an experiment's results, a tutorial, an application, and an overview in the blog, would they get a ton of points, additive? Obviously, no. Thinking out loud here: I'd probably look at what was the essential purpose of the blog: to teach, to report or to provide back ground information? teach = tutorial; report=experiment; provide general information = overview. So, it seems I need to work on the scoring guidelines for combination blog situations. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rscasny
    rscasny over 3 years ago in reply to Gough Lui

    Interesting scenarios. That is, if someone packed an experiment's results, a tutorial, an application, and an overview in the blog, would they get a ton of points, additive? Obviously, no. Thinking out loud here: I'd probably look at what was the essential purpose of the blog: to teach, to report or to provide back ground information? teach = tutorial; report=experiment; provide general information = overview. So, it seems I need to work on the scoring guidelines for combination blog situations. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • misaz
    misaz over 3 years ago in reply to rscasny

    That packed blog can be considered as final blog, I think.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to rscasny

    I do like the idea of nominating what sort of blog it is, but this also is not problem-free. If you've looked at my recent entries, I prioritised having a consistent posting cadence. As a result, early blogs were introductions/unboxing, but from there-on, blogs were a mixture because it was not possible to achieve everything necessary for a neat bundled posting within each week.

    Now, if one must nominate just one type - I suspect nobody would choose to blog lower value types and instead will choose the higher ones. Because the higher value types generally need more work/time/results, I can foresee blogs being released in a "bunch" toward the end of the time frame because of this. Filming and editing video can take a while, for example, and experiments may require procuring unforeseen parts and building. This may make engagement tricky if all the content arrives at once.

    Furthermore, the later the blog post is provided, the more time one potentially has to polish and improve it. Comparing earlier posts to later posts may not be favourable for the earlier poster.

    But this also opens an interesting conundrum - blogs must also be numbered/ordered for the "blog 1s" to all be compared. If I were to follow traditional rules and go intro/unbox for my blog 1, then it seems likely a double-whammy effect may also occur on the bonus points where someone else's blog 1 is an experiment. Not only is it likely they will score higher on the base type score, the scope also leads to more potential content for which higher bonus points can be allocated. It also means competitors can see other people's already posted "blog 1s" and scale their efforts.

    There may be no perfect scoring system - but I'm just voicing my thoughts out because any policy change (while very welcome as an attempt to improve the program) may have unintended side effects.

    - Gough