Experimenting with Flyback Transformers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Flyback Transformers
  • More
  • Cancel
Experimenting with Flyback Transformers
Forum Some Changes in How Blogs are Scored in Experimenting Challenges
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Flyback Transformers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 43 replies
  • Subscribers 44 subscribers
  • Views 6025 views
  • Users 0 members are here
  • Experimenting Challenges
Related

Some Changes in How Blogs are Scored in Experimenting Challenges

rscasny
rscasny over 2 years ago

I am simplifying the requirements and changing the way the extra credit blogs will be scored, starting with the upcoming program, Experimenting with Flyback Transformers.

I'll describe the changes below.

Changes
I am dropping the introductory blog and the forum participation as separate tasks. Why? I just feel I was asking too much of a participant. I am still retaining the 5 extra credit blogs and the final blog.

New Scoring for Extra Credit Blogs
I think I was given some fair criticism on the way the extra credit blogs were scored. I was trying to streamline the judging process, but I feel a change in scoring is in order.

So, this is the system I want to adopt for the extra credit blogs. They will be scored based on the type of blog written, as well as how well all Blogs 1s, 2s, 3s, etc rank to each other.

Scoring for Type of Blog

  • Introduction blog: this type of extra credit blog describes the kit, performs an unboxing, and/or describes what types of experiments the participant will perform. Score: 20 points
  • Component or Technology Overview/Description: this type of extra credit blog describes the kit components, the supplier's product family, and variants in depth: Score: 25 points
  • Experiment Description: this type of extra credit blog describes an experiment, shows data, and/or comes to a conclusion regarding the experiment  Score: 50 points
  • Tutorial - this type of extra credit blog would show the reader how to do something such as coding, circuit building, and/or troubleshooting with regard to the kit components.. Note: this could be an experiment; however, if the full force of the blog is educational or to provide a nice-to-know tip or trick, then it will be scored as a tutorial Score: 55 points
  • Building an application with the kit -- the type of extra credit blog would describe how the participant used the kit's components to build a project that illustrates an application. While this blog isn't a pure experiment, it experiments with the component through an application Score 45 points

Add-on Points to an Extra Credit Blog

  • Including a video will earn you an extra 5 points
  • Including a video that our element14 team promotes on social media earns you an extra 15 points (this would be a high quality video)
  • Including educational images that illustrate the experiment and are highly informative earns you an extra 10 points

Ranking Score

All the Blog 1's, 2's, 3's, 4's and 5's will be scored relative to each other. They will be ranked based on quality. The lowest ranking blog will earn 2 points. Each blog above it will score an additional 2 points. Example: for 5 participants, 5th place = 2 points, 4th place = 4 points, 3rd place = 6 points, 2nd place = 8 points, 1st place = 10 points. 

The total extra credit blog score will be the sum of the type of blog score + the ranking score.

  • Sign in to reply
  • Cancel

Top Replies

  • rscasny
    rscasny over 2 years ago +5
    SCORING SYSTEM UPDATE I appreciate everyone who has offered their ideas. I like the point system and will continue to use it. While no scoring system is perfect, I think that a sweet spot can be found…
  • rscasny
    rscasny over 2 years ago +4
    I would like to thank everyone who participated in this discussion and offered their ideas. I'm going to update the instructions now. I think we have the scoring rules that are fair. Thanks! Randall
  • shabaz
    shabaz over 2 years ago in reply to rscasny +2
    I think this will definitely give contestants a lot of freedom, and pick up deserved points for good photos/experimenting/informative blogs/training content or video etc.. Also, an extra benefit, it…
Parents
  • JWx
    JWx over 2 years ago

    Interesting modification... I only wonder if it doesn't prevent people from publishing traditional unboxing/kit content information? I can imagine the series of experiment/tutorial type blogs with very limited information about kit components. That could of course be compensated by final blog judging guidelines (e.g. kit content information needs to be included to get good final score)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to JWx

    And another thing - does it means that final blog will not be a sum of extra credit blogs? I think that writing - for example - a tutorial could require extra effort not always advancing the main story of final blog (and in some cases not easily integrated into final blog)... [EDIT] I think that it could be a better approach from reader's perspective to get more different reading material during the contest

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • JWx
    JWx over 2 years ago in reply to JWx

    And another thing - does it means that final blog will not be a sum of extra credit blogs? I think that writing - for example - a tutorial could require extra effort not always advancing the main story of final blog (and in some cases not easily integrated into final blog)... [EDIT] I think that it could be a better approach from reader's perspective to get more different reading material during the contest

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • JWx
    JWx over 2 years ago in reply to JWx

    BTW - from my perspective - some sort of judging results summary would be very nice (something like anniel747 have published - but maybe anonymized/aggregated between all judges). I understand that judges are very busy, time for scoring is short and maybe detailed scoring is not always present or generated using different criteria sets  (thus not easy to summarize), but I think that it would be very interesting to the challenger in the long-term perspective (what was considered ok and - especially - what aspects were below expectations)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to JWx

    I definitely would not volunteer to judge in that case. It's difficult enough, let alone having to then inevitably justify to the world.

    Besides, comments are provided, and they are used in the summaries of all the project for all the competitions as far as I'm aware. 

    People often ask for advice about competitions (and applications) and as far as I can tell, it is always given by plenty of people. 

    Some publicly ask for 1:1 help offline, which too is fine, but few of those make the effort to follow up on it. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to JWx

    "time for scoring is short"

    This is not the case at all. Sorry, but if you try judging, you'll realize a ton of effort goes into it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to shabaz

    maybe "deadlines are short" would be better... I was meaning: there is short (calendar) time to judge all the blogs...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to JWx

    Ok, but I think language is important. On the one hand everyone says the judging is fair, but on the other hand, there are plenty of subtle implications (I'm being general, only commenting here since it was mentioned) that point to people being unhappy with the scoring. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to shabaz

    I understand that it would put additional burden on judges - but from challenger perspective it is sometimes difficult to tell what was wrong/what needs to be improved... But I understand different aspects - people could get upset and discouraged, so maybe it wouldn't be positive change after all

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to shabaz

    sorry - I was thinking that it was clear (I think my English skill is worse than I have thought). BTW - I have volunteered to judge one of Project14 projects so I can imagine what it takes to judge something much bigger ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to JWx

    I mainly currently just care about readers perspective because there is a lot of support for challengers, including help pages to ask questions. We all seem to agree the final rankings are pretty accurate, and there's lots of opportunities to self-improve in any aspect. It would be nice to get back to the fun aspect of challenges, with people writing what they want to (passionately) because it feels unpleasant having to concentrate on points when it would be more fun to concentrate on the technology. I understand that the points are necessary for ranking and awards of course. But feel something is lost if it is too much focus on that.

    Also, there doesn't have to be anything wrong with contest blogs. Contestants have naturally focussed on their "baby" throughout the challenge, they naturally have not got to know all the other babies and a few might simply have the edge in comparison. That's not a negative thing for contestants, and people genuinely are congratulating everyone who makes an effort at the end of the day.

    The contestants I hope also afterwards look at the other contestants and be honest about how they would vote after having spent some time reading the others' blogs. Has anyone seen a genuinely unfair award? If not, then the answers simply have to be in those babies they just have to get to know them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to shabaz

    From the reader's perspective I think that aggregating (mayor parts of) extra blogs into final blog could be discouraging - reader can either skip all the extra blogs and read only the final or read intermediate blogs and then get bogged down by looking what was changed in the summary blog.

    And in this aspect the new scoring would be an improvement - one cannot simply  aggregate 5 different tutorials (and - given the experience from previous scoring system - when maximum number of points from intermediate blogs was essential to the final score - tutorials will be created) into one coherent summary blog....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to JWx

    People successfully write blogs without making their final blog discouraging to read. Here's an example that Ralph did, I can't recall it in detail but I recall being impressed at the organization and the avoidance of all the "ancillary" stuff that really should be in a separate blog, neatly linked where necessary:

     Panda Enclosure - Final Summary Blog 

    From the reader's perspective, that was far better than either:

    (a) having to read five blogs, 

    (b) having to read an unorganized amalgamation of five blogs.

    And let's be honest. While a writer may think all five of their blogs are full of interesting content, a reader wants the readers digest version, comfortable in the knowledge that if they want the code, they simply click a link, and if they want to drill down into the detail about how something was prepared or installed, that's a link away. None of it is hidden, it's simply that URLs are embraced, but it's still entirely readable standalone. Its too much to expect a reader will follow all five blog posts let alone the final one.