Experimenting with Flyback Transformers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Flyback Transformers
  • More
  • Cancel
Experimenting with Flyback Transformers
Forum Some Changes in How Blogs are Scored in Experimenting Challenges
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Flyback Transformers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 43 replies
  • Subscribers 44 subscribers
  • Views 6134 views
  • Users 0 members are here
  • Experimenting Challenges
Related

Some Changes in How Blogs are Scored in Experimenting Challenges

rscasny
rscasny over 3 years ago

I am simplifying the requirements and changing the way the extra credit blogs will be scored, starting with the upcoming program, Experimenting with Flyback Transformers.

I'll describe the changes below.

Changes
I am dropping the introductory blog and the forum participation as separate tasks. Why? I just feel I was asking too much of a participant. I am still retaining the 5 extra credit blogs and the final blog.

New Scoring for Extra Credit Blogs
I think I was given some fair criticism on the way the extra credit blogs were scored. I was trying to streamline the judging process, but I feel a change in scoring is in order.

So, this is the system I want to adopt for the extra credit blogs. They will be scored based on the type of blog written, as well as how well all Blogs 1s, 2s, 3s, etc rank to each other.

Scoring for Type of Blog

  • Introduction blog: this type of extra credit blog describes the kit, performs an unboxing, and/or describes what types of experiments the participant will perform. Score: 20 points
  • Component or Technology Overview/Description: this type of extra credit blog describes the kit components, the supplier's product family, and variants in depth: Score: 25 points
  • Experiment Description: this type of extra credit blog describes an experiment, shows data, and/or comes to a conclusion regarding the experiment  Score: 50 points
  • Tutorial - this type of extra credit blog would show the reader how to do something such as coding, circuit building, and/or troubleshooting with regard to the kit components.. Note: this could be an experiment; however, if the full force of the blog is educational or to provide a nice-to-know tip or trick, then it will be scored as a tutorial Score: 55 points
  • Building an application with the kit -- the type of extra credit blog would describe how the participant used the kit's components to build a project that illustrates an application. While this blog isn't a pure experiment, it experiments with the component through an application Score 45 points

Add-on Points to an Extra Credit Blog

  • Including a video will earn you an extra 5 points
  • Including a video that our element14 team promotes on social media earns you an extra 15 points (this would be a high quality video)
  • Including educational images that illustrate the experiment and are highly informative earns you an extra 10 points

Ranking Score

All the Blog 1's, 2's, 3's, 4's and 5's will be scored relative to each other. They will be ranked based on quality. The lowest ranking blog will earn 2 points. Each blog above it will score an additional 2 points. Example: for 5 participants, 5th place = 2 points, 4th place = 4 points, 3rd place = 6 points, 2nd place = 8 points, 1st place = 10 points. 

The total extra credit blog score will be the sum of the type of blog score + the ranking score.

  • Sign in to reply
  • Cancel

Top Replies

  • rscasny
    rscasny over 3 years ago +5
    SCORING SYSTEM UPDATE I appreciate everyone who has offered their ideas. I like the point system and will continue to use it. While no scoring system is perfect, I think that a sweet spot can be found…
  • rscasny
    rscasny over 3 years ago +4
    I would like to thank everyone who participated in this discussion and offered their ideas. I'm going to update the instructions now. I think we have the scoring rules that are fair. Thanks! Randall
  • shabaz
    shabaz over 3 years ago in reply to rscasny +2
    I think this will definitely give contestants a lot of freedom, and pick up deserved points for good photos/experimenting/informative blogs/training content or video etc.. Also, an extra benefit, it…
Parents
  • rscasny
    rscasny over 3 years ago

    SCORING SYSTEM UPDATE


    I appreciate everyone who has offered their ideas. I like the point system and will continue to use it. While no scoring system is perfect, I think that a sweet spot can be found where it has a consensus for its fairness.

    Before I posted this update to my discussion, I went back and read through every blog in Experimenting with Supercapacitors. I saw the blogs covered the following things:

    • An introduction, which often was a combination of an unboxing and kit overview
    • Unboxing
    • Kit Overview 
    • Deep dive into the kit and components
    • Background technical information related to the components
    • A report on a specific experiment that answered a question: How does high temperature affect a supercapacitor?
    • A blog that tests a component through an application or prototype
    • A tutorial--the blog is meant to teach the reader something

    My feeling after reading all the blogs was that this is a component experimenting challenge, so blogs with a report on a experiment should score higher. A tutorial should also score high because it should be teaching something specific. An experiment using the component in a device or application should also score high. The others would have less points.

    BUT ONCE I READ THROUGH ALL YOUR IDEAS, as a group, you want the scoring to reflect the quality as well.

    I was attracted to Shabaz's suggestion (he has been a judge for a number of my experimenting challenges). I modified the ASSIGNED points to reflect quality.

    • A blog that contains a decent unboxing or detailed photographs will get up to 20 points.
    • A blog that contains a deep-dive into the components will get up to 20 points.
    • A blog that contain a fair amount of information towards an actual experiment will get up to 20 points.
    • A blog that significantly helps newcomers to work with the technology will get up to 20 points.
    • A blog that contains a good quality video will get up to 20 points.
    • A blog that uses components in an application or prototype to test or experiment with them will get up to 20 points.

    The actual scoring will be judged based on quality, with a 20-point perfect score based on a very high level of quality and thoroughness. A blog with more than one of the above characteristics would get an additive score, based on quality.

    By dropping the Introduction blog and forum participation, gives more time to judge the 5 blogs.

    The final project blog will stay the same, up to 300 points.

    I'm leaning towards this scoring system. I'll let it "age" for a day or so before finalizing it. Your feedback is always appreciated.

    Randall

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to rscasny

    Personally, I don't mind this - I think the added freedom to allocate points where necessary is good, as it's less prescriptive and constraining.

    But at the same point in time, I don't want to see the same thing happen as before, where full marks are awarded to nearly everything, thus the score "saturates" at 100%. As long as your 20 points are sensibly allocated in such a way that an excellent blog scores 20, and a satisfactory blog scores less - something like 10-15, then it makes sense. It has to be a scale ...

    If everything is 20 points or 0 points ... then I feel that we're back to square one ...

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago in reply to rscasny

    Personally, I don't mind this - I think the added freedom to allocate points where necessary is good, as it's less prescriptive and constraining.

    But at the same point in time, I don't want to see the same thing happen as before, where full marks are awarded to nearly everything, thus the score "saturates" at 100%. As long as your 20 points are sensibly allocated in such a way that an excellent blog scores 20, and a satisfactory blog scores less - something like 10-15, then it makes sense. It has to be a scale ...

    If everything is 20 points or 0 points ... then I feel that we're back to square one ...

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Andrew J
    Andrew J over 3 years ago in reply to Gough Lui

    Agreed.  I also refer back to an earlier point: entries shouldn’t even make it to scoring if it’s obvious the effort and quality is poor (I.e. lip service is being paid).  I don’t think Randall should worry about disqualifying entries.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to Gough Lui

    I think that was the problem last time. They were scored sort of in a pass fail approach. If you did it, you got all points. I realize that each blog needs individual scoring based on its inherent value. 

    Randall