Experimenting with Flyback Transformers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Flyback Transformers
  • More
  • Cancel
Experimenting with Flyback Transformers
Forum A 2 parter: does anyone know of a pwm controller that can work with 1.5v? and! Does this section of the element14 community remain active for like general flyback discussion?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Flyback Transformers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 42 subscribers
  • Views 2841 views
  • Users 0 members are here
Related

A 2 parter: does anyone know of a pwm controller that can work with 1.5v? and! Does this section of the element14 community remain active for like general flyback discussion?

Anthocyanina
Anthocyanina over 2 years ago

Now that the time constraints have been removed, I want to keep working on my portable chaos toy. I started by taking apart the tiny transformer (the hot air station made this super easy) to rewind it with two symmetrical secondaries.

image

image

Now my goal is to power the converter with a rechargeable AAA battery, or if getting a low enough voltage pwm controller is not possible, a single 18650. So, does anyone know of a controller that can do that? 

And well, my second question is if this section remains active in the community, or if this should be used only for the challenge and I should take my questions elsewhere? 

Thank you!

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 2 years ago in reply to Anthocyanina +3
    If you are doing the winding yourself, you can still add an auxiliary winding to have a higher voltage, enough to power a common pwm regulator you can even use that auxiliary winding for regulator feedback…
  • cstanton
    cstanton over 2 years ago +2
    Anthocyanina said: And well, my second question is if this section remains active in the community, or if this should be used only for the challenge and I should take my questions elsewhere? We typically…
  • jc2048
    jc2048 over 2 years ago +2
    https://www.analog.com/en/products/lt1073.html
Parents
  • dougw
    dougw over 2 years ago

    DRV8837CDSGR

    Is this what you are looking for? It can output any voltage although you would need to boost the input logic to 1.8V.

    There are small MCUs that will run down to 0.7V by using an internal voltage booster. Such as ATtiny43U, which could drive the H-bridge above with PWM.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 2 years ago

    DRV8837CDSGR

    Is this what you are looking for? It can output any voltage although you would need to boost the input logic to 1.8V.

    There are small MCUs that will run down to 0.7V by using an internal voltage booster. Such as ATtiny43U, which could drive the H-bridge above with PWM.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to dougw

    No, that's an H bridge, not a pwm controller, but thank you! Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to Anthocyanina

    The MCU can do PWM. What functionality do you need with the PWM? - What controls it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to dougw

    i want this toy to be fully analog. the pwm controller is to drive the flyback converter, this time with feedback from the output to keep the output voltage from drifting as the battery discharges. Thank you!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to Anthocyanina

    If you are doing the winding yourself, you can still add an auxiliary winding to have a higher voltage, enough to power a common pwm regulator you can even use that auxiliary winding for regulator feedback and not have to complicate measuring in the secondary.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to javagoza

    Thanks! I looked into this when i saw your response, it seems most controllers won't start with low vin, so now i'm looking into either designing a controller myself, or adding in a charge pump boost converter that kickstarts the whole thing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to Anthocyanina

    Maybe you can experiment with Blocking oscillators . 

    imageimage

    Source: wikipedia

    Joule thief - Wikipedia