Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Power amplifier using flyback converter
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 332 subscribers
  • Views 3870 views
  • Users 0 members are here
  • Experimenting Challenges
  • EXPERIMENTING WITH FLYBACK TRANSFORMERS
  • flyback transformers
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Power amplifier using flyback converter

Maxbiggair
Maxbiggair over 2 years ago

 There is a kind of converter I need help on. It is a buck-boost converter but the inductor is replaced by a steel toroid core transformer with a core power of 2025W max, it has a primary input and two secondary output 250 turns 1:1:1 each. 

The transistor is changed to a MOSFET and is driven by a 555 timer pwm circuit. Powered by a 12V, 75AH Battery 

Flyback voltage is tapped out from the primary coil and the high current is tapped from the first secondary coil through the use of diode and capacitors. 

The high voltage and high current is combined and fed to the inverter converting it to 50Hz AC. The output of the inverter is connected to the first secondary coil. Which is the same coil that the high current capacitor is drawing current from.

The second secondary coil will be the output whereby a band pass filter will be used to extract the 50Hz frequency from the transformer.

The goal is to provide good efficiency while reducing the cost.

  • Sign in to reply
  • Cancel

Top Replies

  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Maxbiggair +2
    if not familiar with component symbols, please draw the components as they are physically connected and mark the toroid windings with colors to see which winding connects to what. i would again recommend…
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Maxbiggair +2
    do you think we have time to try to decipher your drawing and engineer a solution for you for free? especially after that response? good luck in your endeavours!
  • shabaz
    shabaz over 2 years ago in reply to Maxbiggair +2
    That's very rude considering people are trying to help you. Your diagram doesn't use standard symbols, and it's impossible for anyone to get inside your mind to understand precisely what was meant by…
  • dougw
    dougw over 2 years ago

    It sounds strange to me to connect the AC output to the input transformer. Could you post the schematic?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Maxbiggair
    Maxbiggair over 2 years ago in reply to dougw

    Well am not good at schematics but I hope you understand this.  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Maxbiggair

    are you using a distributed air gap toroidal core? 

    aslo, the MOSFET placement isn't correct. I'll do a bit of self-promotion here with this guide of flyback converters which might help you /search?q=Experimenting%20with%20Flyback%20Transformers%20#serpauthor=438987&serpcategory=blog&serpgroup=445 

    that blog series covers everything you need to know to get a flyback converter up and running and is very beginner-friendly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Maxbiggair
    Maxbiggair over 2 years ago in reply to Anthocyanina

    Am not good at schematics.

    But you should know that the PWM is connected to the gate 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Maxbiggair

    yeah, that's not the problem, if you're using an N channel fet, you connect the positive of the DC source to the first pin of the transformer primary, and the other pin goes to drain, and you connect source to ground. the connection shown in your drawing doesn't seem to be doing that

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Maxbiggair
    Maxbiggair over 2 years ago in reply to Anthocyanina

    Let say am using a reference node 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Maxbiggair

    if not familiar with component symbols, please draw the components as they are physically connected and mark the toroid windings with colors to see which winding connects to what. 

    i would again recommend you read the flyback blogs i shared. flyback converters are one of the simplest dc to dc converter topologies to learn, even if you only have a basic understanding of electronics.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Maxbiggair
    Maxbiggair over 2 years ago in reply to Anthocyanina

    Do you think I have time 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Maxbiggair

    do you think we have time to try to decipher your drawing and engineer a solution for you for free? especially after that response? good luck in your endeavours! Slight smile

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to Maxbiggair

    That's very rude considering people are trying to help you.

    Your diagram doesn't use standard symbols, and it's impossible for anyone to get inside your mind to understand precisely what was meant by each part of your diagram.

    You would need to put into standard symbols that everyone can understand, or try the approach of sketching the actual connections, rather than that pseudo-"diagram" you have currently.

    It's like language; if you're speaking a different language, how can anyone help without it being translated? Your diagram needs to be translated, and there's no translator in the world that can do that if you're using your own unique terminology that is only known to you.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
>