Experimenting with Gesture Sensors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Gesture Sensors
  • More
  • Cancel
Experimenting with Gesture Sensors
Forum Establishing serial communication over UART instead of USB in MAX25405 EVKIT
  • Challenge Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Gesture Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 89 replies
  • Subscribers 40 subscribers
  • Views 15730 views
  • Users 0 members are here
  • MAX25405
  • gesture sensors
  • maxim integrated
  • uart
  • max32620fthr
Related

Establishing serial communication over UART instead of USB in MAX25405 EVKIT

rsjawale24
rsjawale24 over 4 years ago

The MAX25405EVKIT comes with a MAX32620FTHR board which is preprogrammed with custom binary file for the gesture recognition. The application note at Maxim Gesture Sensor EVKit Serial API (maximintegrated.com)

mentions "The serial interface can be implemented over the Universal Serial Bus (USB) virtual serial port or over a Universal Asynchronous Receiver-Transmitter (UART). The EV kit is shipped configured to use the USB serial port to work with the EV kit PC Graphical user Interface (GUI). If a UART serial interface is desired, custom firmware in binary format is available."

Upon researching more, I found the firmware_framework code that contains the code for gesture recognition compiled using mbed compiler.

The readme file says that a file called interface.h and interface.c define the communication protocol. When I open the interface.c file, I can see a comment in the code that says Option to implement serial API over UART instead of USB but there is only a MACRO set as #define macro_name 0 

I tried to change the 0 to 1 and compile the code, however, it does not compile successfully. The USBDevice library shows some error while compiling. 

Did anyone try to change the serial API over UART instead of USB? Was it successful?  

EDIT: I have successfully compiled the code for UART. However, I'll do some experiments and write introductory blogs before I re-program the MAX32620FTHR board with my firmware. 

  • Sign in to reply
  • Cancel

Top Replies

  • misaz
    misaz over 4 years ago in reply to misaz +4
    Today I found root cause of the issue. Issue is caused by invalid assembly code generated by modern ARM compiler. With older GCC compiler it works because it handle undefined behaviour used in code differently…
  • misaz
    misaz over 4 years ago +3
    I am curious how did you successfully compiled non-changed code? I started working with latest mbed-os but I was unable to compile it (missing toolchain) no matter of USE_UART_INTERFACE setting. Later…
  • BigG
    BigG over 4 years ago in reply to rsjawale24 +3
    I've create a very basic stripped down library based on the firmware framework using the latest MbedOS 6.16. github.com/.../Max25x05_MbedOS6 All it is doing is getting the raw pixel data. It is doing…
  • rsjawale24
    rsjawale24 over 4 years ago in reply to BigG

    For the past one hour, I have been trying mbed CLI which is quite difficult to run in windows. I tried mbed studio but I get two errors - 

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 4 years ago in reply to rsjawale24

    I recommend using Linux. I have issues even when downloading Python requirements on WIndows. I have no idea about first error but I also faced second error and after searching on internet I found that this is not error but rather warning indicating that MBED OS was tested with GCC 6 to 7. You most probably use newer version but this is not problem. Compilation should continue after this error (warning).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 4 years ago in reply to misaz

    Thanks, I guess I'll just switch to linux

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 4 years ago in reply to rsjawale24

    Please note that the default compiler for Mbed Studio is ARMC6, which is different to what is used to compile the default firmware according to the firmware framework readme.txt instruction (i.e. uses GCC_ARM)... and I see from the above that you tried to compile using ARMC6, which will fail.

    As such CLI is recommended.

    However, you can still use Mbed Studio using ARMC6 but it just requires some code modification or you can also change the default compiler... but this may introduce other issues (not tested).

    https://os.mbed.com/docs/mbed-studio/current/installing/switching-to-gcc.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 4 years ago in reply to BigG

    Yes I changed the default compiler to GCC using the mbed commands. 
    I got it working finally using mbed cli on windows. Thanks to both of you for helping me with this. 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 4 years ago

    So I'm facing another problem now.

    As long as I send commands like ver and ping, it works fine. But as soon as I send poll command, I get results and then it gets stuck there. It does not respond to any commands. Not sure why this is happening.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 4 years ago in reply to rsjawale24

    I also noticed this behaviour. I had not very much time, so following information about source code and my theory may be inaccurate. After brief look to code I did not find anything which should cause crash of firmware. Executing poll command only printf some data from global variables if I understand it correctly. But I remember that readme.txt contained some notices of extending main stack nad poll printf is quite a complicated (memory usage extensive). Maybe our firmware was not compiled and configured properly and printf with many format strings make some memory overflow which destroys stack and causes firmware to crash. I will try to debug it this week and find some fix.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 4 years ago in reply to misaz

    Thanks! I looked into it. The poll command is giving only 0's as output so maybe something is wrong. I will try looking into in tonight. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 4 years ago in reply to rsjawale24

    I've create a very basic stripped down library based on the firmware framework using the latest MbedOS 6.16.

    github.com/.../Max25x05_MbedOS6

    All it is doing is getting the raw pixel data. It is doing none of the manipulation routines as yet.

    It seems to provide data and does not lock up using USBserial - well OK, I only let the program run for about 20 seconds. You should be able to change USBSerial and use RX/TX pins.

    Please let me know if you spot any errors, or have any problems, and you are free to recommend changes.

    At the moment, the only thing that is puzzling me is the configuration setting used in the Firmware Framework for MAIN CONFIGURATION 2 (0x2). Here the value is set to 0x02 and this does not correspond with the documentation.

    Maybe someone has an answer.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 4 years ago in reply to BigG

    Thanks, I'll check this. But the gesture algorithm is quite complex, I guess. Here from the raw pixel data it would be difficult to identify the gestures, or maybe a simple gesture sensing algorithm can be devised by reading the raw sensor data. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>